全 2903 件が検索されました。(761 - 780件を表示)
- マニュアル
... connection This product has four RS-485 communications ports for RS-485-connected measurement devices. Up to 31 devices can be connected o one port.t Power Monitor Up to 14 RS-485-connected measurement devices Power Monitor Wiring must be conducted ...
- マニュアル
... manual describes the functions, performance, and application methods needed for optimum use of the product. Please observe the following items when using the product. • Before using the product, thoroughly read and understand this manual to ensure correct use. • Keep this manual in a safe location ...
- マニュアル
...L-N. • ES1-L-N or ES1-LL-N are designed for use by qualified personnel with a knowledge of electrical systems. • Before using the product, thoroughly read and understand this manual to ensure correct use. • Keep this manual in a safe location ...
- マニュアル
...Please observe the following items when using the product. • This product is designed for use by qualified personnel with a knowledge of electrical systems. • Before using the product, thoroughly read and understand this manual to ensure correct use. • Keep this manual in a safe location ...
- マニュアル
... in death or serious injury Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury, or property damage. Warnings and Cautions WARNING Do not attempt to take any Unit apart while the power is being supplied. Doing ...
- マニュアル
... in death or serious injury Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury, or property damage. Warnings and Cautions WARNING Do not attempt to take any Unit apart while the power is being supplied. Doing ...
- マニュアル
... User’s Manual NX1P2- NJ501- NJ301- NJ101- NX-SL NX-SI NX-series Safety Control Unit NX-SO User's Manual W504 SYSMAC-SE2 Sysmac Studio Version 1 Operation Manual W570 NX-ILM GX-ILM IO-Link System User’s Manual Z405 F3SG-SR F3SG-PG Safety Light Curtain F3SG-SR Series Z930 Multi-Beam Safety Sensor F3SG-...
- マニュアル
... switches. We started to develop switches over half a century ago. In order to do everything possible to meet the needs of our customers, we have been committed to various types of switch development and quality improvement. We summarized preventive measures against failures in this guide ...
- マニュアル
... 5 0 9 - 3 C * Thank you very much for purchasing an OMRON product. To ensure safe and proper use of this product, please read and thoroughly understand this sheet before use. When finished reading the sheet, keep it in a convenient location ...
- マニュアル
... mounter bracket (F39-LMAF1) > 1. Loosen the Bolt (1) of the Muting sensor arm mounter bracket. (Fig. 1) Bolt (1) Loosen R12.6 2 3. 4. Securely tighten Install the Muting sensor arm mounter bracket so that there is enough space to install the dedicated brackets to F3SG-SR/PG. 1. Remove End cap Fig. 2 L 4.4 2- - 6.2 2 3.2 40 13.5 3. Securely tighten 45 15.1 3. Securely tighten the included Bolt (2) (hexagon socket head bolt (M4 x 8) ) to fix the Muting sensor arm mounter (Right) and the Muting ...
- マニュアル
... out of the specified range - Areas submerged in water or subject to rain water • Properly perform the wiring after confirming the signal names of all the terminals. • Do not connect the F39-JGR3K-- Conversion Cable to the F39-GCN5. Failure to do ...
- マニュアル
...and proper use of this product, please thoroughly read and understand this instruction sheet before using it. Please also thoroughly read and understand the User’s Manual on the included CD-ROM. When you finish reading the manuals, keep them in a convenient location ...
- マニュアル
...0720 0800 0880 Fig. 1 (2) When using the product subjected to vibration or mechanical shock, attach the included Fixing Stickers. Model F39-HSG A Precautions for Safe Use Attach the Spatter Protection Cover ...
- マニュアル
... verify that the F3SG-SR/PG operates as intended. Make sure to stop the machine until the test is complete. Unintended settings may cause a person to go undetected, resulting in serious injury. Do not try to disassemble, repair, or modify the product. Doing ...
- マニュアル
... brouillage, et (2) l'utilisateur de l'appareil doit accepter tout brouillage radioélectrique subi, même si le brouillage est susceptible d'en compromettre le fonctionnement. ■ IC CAUTION To reduce potential radio interference to other users, the antenna type and its gain should be ...
- マニュアル
...function settings may cause a person to go undetected, resulting in serious injury. Do not connect each line of the F3SG-SR to a DC power supply of higher than 24 VDC+20%. Also, do not connect it to an AC power supply. Failure to do ...
- マニュアル
... be able to perform these operations properly, which may cause a person to go undetected, resulting in serious injury. Make sure to perform wiring while the power supply is OFF. Do not use the product in environments where flammable or explosive gases are present. Doing ...
- マニュアル
... exposed to vibration or shock levels higher than in the specification provisions - Areas where the pollution degree is harsher than 3, such as outdoor environment • When carrying and installing the product, make sure that two people work together according to the weight of the product ...
- マニュアル
...- Areas exposed to vibration or shock levels higher than in the specification provisions - Areas where the pollution degree is harsher than 3, such as outdoor environment • When carrying and installing the product, make sure that two people work together according to the weight of the product ...
- マニュアル
... cables are connected with the polarity reversed, the load will not operate, or the operation indicator will not light. ・Make sure that signal lines are always connected through a load. ・Use Sensors that meet the specifications. ・Do not pull on the connectors and cables. Doing ...