全 2903 件が検索されました。(861 - 880件を表示)
- マニュアル
... (safety extra low-voltage circuits on the secondary side). ■Installation environment ・ Do not use the product in environments where it may be exposed to inflammable/explosive/corrosive gas. ・ Do not use the product outdoors or in environments exposed to direct sunlight. ・ Install the unit ...
- マニュアル
... 2022 - 2023 All Rights Reserved. PRECAUTIONS FOR SAFE USE · Keep foreign matter away from the connector. Otherwise a failure may occur. · Do not touch the terminal portion (connecting portion) of this product directly or allow it to come in contact with metals. Doing ...
- マニュアル
.... For your convenience, keep the sheet at your disposal. · Keep foreign matter away from the connector. Otherwise a failure may occur. · Do not touch the terminal portion (connecting portion) of this product directly or allow it to come in contact with metals. Doing ...
- マニュアル
... Headquarters OMRON EUROPE B.V. Sensor Business Unit Carl-Benz-Str. 4, D-71154 Nufringen, Germany Tel: (49) 7032-811-0/Fax: (49) 7032-811-199 Camera cable connector Camera FZ-SC2M FZ-S2M *The camera cable is polarized, ...
- マニュアル
...: (49) 7032-811-0/Fax: (49) 7032-811-199 OMRON ELECTRONICS LLC 2895 Greenspoint Parkway, Suite 200 Hoffman Estates, IL 60169 U.S.A. Tel: (1) 847-843-7900/Fax: (1) 847-843-7787 Approx. 85g (including base) *The camera cable is polarized, ...
- マニュアル
... the Controller immediately, turn OFF the power supply, and consult your OMRON representative. ・Dispose of FZ-SC components as industrial waste. Camera Name plate Camera cable FZ-SC/S connector *The camera cable (FZ-VS,FZ-VSL,FZ-VSB) is polarized, ...
- マニュアル
... 4 年 7月 TRACEABILITY INFORMATION: Importer in EU: Manufacturer: Omron Europe B.V. OMRON Corporation, Wegalaan 67-69, Shiokoji Horikawa, Shimogyo-ku, NL-2132 JD Hoofddorp Kyoto. 600-8530 JAPAN The Netherlands *The camera cable is polarized, ...
- マニュアル
...immediately, turn OFF the power supply, and consult your OMRON representative. ・ Dispose of FZ-SHC/SC components as industrial waste. Camera cable connector Name plate Camera FZ-SHC FZ-SH *The camera cable (FZ-VS,FZ-VSL,FZ-VSB) is polarized, ...
- マニュアル
...Weight Approx. 70 g Dimensions 12 35.5 (Unit: mm) Item FZ-SLC100-DL Transmittance 87% (typical value) 78 Performance Specifications Removal 1. Loosen the screws of the mounting brackets and turn the brackets ...
- マニュアル
... on the back of the camera and the camera connector on Controller FZ-3□□. Extension Camera cable Camera cable connector connector FZ-VS□ Nameplate Intelligent camera FZ-SLC100 *The camera cable (FZ-VS,FZ-VSL,FZ-VSB) is polarized, ...
- マニュアル
...-DL Transmittance 87% (typical value) Mounting brackets 73 93 38 39 40.5 36 20 11.5 Item 1. Loosen the screws of the mounting brackets with the provided hexagonal wrench and turn the brackets so that they will not catch on the illumination part of the FZ-SLC15. 1.5 Performance Specifications (Unit: mm) Diffusion Board φ28 73 92.5 Operating: 0 to 50°C (with no icing or condensation) Storage: −25 to 60°C (with no icing or condensation) 12.5 Thank you for selecting this OMRON product. This Instruction Sheet primarily describes precautions required ...
- マニュアル
...OMRON ELECTRONICS LLC One Commerce Drive Schaumburg,IL 60173-5302 U.S.A Phone:1-847-843-7900 Telephone Consultation 1-800-55-OMRON Fax : 1-847-843-7787 Intelligent camera FZ-SLC15 *The camera cable (FZ-VS,FZ-VSL,FZ-VSB) is polarized, ...
- マニュアル
... on the back of the camera and the camera connector on Controller FZseries. Illumination connection Camera cable Camera cable connector FZ-VS□ connector Nameplate Automatic focus camera FZ-SZC100 ※ The camera cable (FZ-VS,FZ-VSL,FZ-VSB) is polarized, ...
- マニュアル
... on the back of the camera and the camera connector on Controller FZseries. Illumination connection Camera cable Camera cable connector FZ-VS□ connector Nameplate Automatic focus camera FZ-SZC15 ※ The camera cable (FZ-VS,FZ-VSL,FZ-VSB) is polarized, ...
- マニュアル
... length and kind is selected. 3. Connect the controller with “CONTROLLER” display side. Vibration resistance 10 to 150 Hz, 0.35-mm single amplitude, 10 times each in X, Y, and Z directions for 8 min ※The camera cable FZ-VS□□□ series is polarized, ...
- マニュアル
... to inform you that our connectors are used in device and equipment applications in a wide range of fields, and we have been able to achieve a track record in the industrial equipment industry up to the present. We summarized preventive measures against failures in this guide ...
- マニュアル
...制御の使用。 特に安全性が要求される用途への使用。 ⃝人命や財産に大きな影響が予測され、 3 SSR uses electronics parts mounting on PCB, so that any dropping and vibration, physical shock beyond the standard level should be prevented, otherwise the initial characteristics will be not insured. It should be prevented to overhaul the product in order to repair and modify at where it is used because it is not expected to work correctly and there is a ...
- マニュアル
... heat sink either while the power supply is ON, or immediately after the power is turned OFF. The SSR and the heat sink will be hot. Precautions for Safe Use ●Transpporting Do not use or store the G32A-P in the following transporting. Doing ...
- マニュアル
... in the built-in snubber circuit. Must need an air convection for SSR or the heatsink. Less convection air produces a heating on SSR abnormal and causes a short-circuit failure and burning. Do not apply short-circuit current to load side of SSR. If ...
- マニュアル
...認図は貴社のお取引先、 または貴社担当オムロン営業員に ご相談ください。 (5) Using Do not operate the G3PF in any of the following locations.Doing so may result in damage to the G3PF or cause the G3PF to malfunction. 1.Supply a high voltage or high current to the input and output terminals. 2.Select a load outside the rated range. 3.Select the power supply outside the rated frequency range. English Model (6) Failure DetectionUsing G3PF - CTB/STB...