全 2903 件が検索されました。(641 - 660件を表示)
- マニュアル
...Control output *5 OFF Flashing Communication indicato( r Green) (1sec cycles) ON Operation indicato( r Orange) OFF NO *3 Precautions for Correct Use (1) Do not install the product in the following locations. Doing ...
- マニュアル
...0 0 0 0 0 D 6 11 18 25 9 11 21 40 200 110 (100) (60) 0 NC (1) Do not install the product in the following locations. Doing so may result in product failure or malfunction. ①Outdoor locations directly subject to sunlight, rain, snow, water droplets, or oil. ②Locations subject to atmospheres with chemical vapors, in particular solvents and acids. ③Locations subject to corrosive gases. (2) The Sensor may malfunction if used near ultrasonic cleaning equipment, high-frequency equipment, transceivers, cellular phones, inverters, or other devices that generate a high-frequency electric field. Please refer to the...
- マニュアル
...0 0 0 3 2 2 2 L 10 16 31 50 12 21 46 60 ■Dimension 0 NO (1) Do not install the product in the following locations. Doing so may result in product failure or malfunction. ①Outdoor locations directly subject to sunlight, rain, snow, water droplets, or oil. ②Locations subject to atmospheres with chemical vapors, in particular solvents and acids. ③Locations subject to corrosive gases. (2) The Sensor may malfunction if used near ultrasonic cleaning equipment, high-frequency equipment, transceivers, cellular phones, inverters, or other devices that generate a high-frequency electric field. Please refer to the Precautions ...
- マニュアル
... determine the Setting distance (Sa) ・Please use it after confirming the installation distance by following (a) and (b) with an actual detection object when you install (a)The detection distance receives the influence by the material of the detection object, thickness, shape, and the size. ...
- マニュアル
... enter the product, resulting in a risk of corruption or burning. (7) Dispose of this product as industrial waste. ■Protective Structure E2ER-X3D -M1TGJ E2ERZ-X2D -M1TGJ 48.3 WARNING (1) Do not install the product in the following locations. Doing ...
- マニュアル
... to 30 VDC (Including 10% ripple (p-p)),Class2 Non-sensing zone 3 Note. About connector types NO type:①④③ NC type:①②③ 0V Load E2EW-(Q)X1R5C□8 (1) Do not install the product in the following locations. Doing ...
- マニュアル
... relay as shown on the figure. Load Detectable object NC OPERATING INDICATOR(ORANGE), OPERATING SET INDICATOR(GREEN) Proximity switch Dispose in accordance with applicable regulations. (1) Do not install the product in the following locations. Doing ...
- マニュアル
... burn. Be sure to insert a load when connecting the power supply. Main Circuit C/Q④ White/② Blue/③ 0V③ C/Q④ DI② M12 (Q)X2□12 (1) Do not install the product in the following locations. Doing so may result in product failure or malfunction. ①Outdoor locations directly subject to sunlight, rain, snow, water droplets, or oil. ②Locations subject to atmospheres with chemical vapors, in particular solvents and acids. ③Locations subject to corrosive gases. (2) The Sensor may malfunction if used near ultrasonic cleaning equipment, high-frequency equipment, transceivers, cellular phones, inverters, or other devices that generate a high-...
- マニュアル
... damage. ●Alert statements ■EFFECTS OF SURROUNDING METAL ■EXTERNAL DIMENSIONS When mounting the proximity switch in a metal panel, maintain the clearances given in table 2. When installing it with the nut, the value is different depending on the kind of the nut used, ...
- マニュアル
...) Size Model M12 X3□12 M18 X7□18 M30 X12□30 A B 40 35 65 60 110 100 X2 Vs Load (1) Do not install the product in the following locations. Doing so may result in product failure or malfunction. ①Outdoor locations directly subject to sunlight, rain, snow, water droplets, or oil. ②Locations subject to atmospheres with chemical vapors, in particular solvents and acids. ③Locations subject to corrosive gases. (2) The Sensor may malfunction if used near ultrasonic cleaning equipment, high-frequency equipment, transceivers, cellular phones, inverters, or other devices that generate a high-frequency electric field. Please ...
- マニュアル
...,replace the sensor. Not Blinking Inconsistency has occurred on Lighting the settings (service data) written in by the IO-Link communications. Rated sensing distance (%) Precautions for Correct Use (1) Do not install the product in the following locations. Doing ...
- マニュアル
... of at least 0.3 mm2 for extension. · Do not apply the forces on the cord exceeding the following limits: Pull: 29.4N; torque: 0.1N·m; pressure: 20N; bending: 29.4N · Always keep the protective cover in place when using the product. Not doing ...
- マニュアル
... the power supply. (6) Dispose of this product as industrial waste. The Sensor can be used by only switching the sensing direction in five ways without changing the mounting hole of the Sensor. (1) Do not install the product in the following locations. Doing ...
- マニュアル
.... (6) When turning on the power by influence of temperature environment,an output mis-pulse sometimes occurs. After the sensor has passed for 300 msec after turning on, please use in the stable state. (7) The sensor is adjusted with a high degree of accuracy, ...
- マニュアル
... polarity of the power is correct, and do not connect to an AC power supply. • Do not short-circuit the load for the open collector output. • Do not lay the power supply cable for the Smart Sensor together with high-voltage lines or power lines. Doing ...
- マニュアル
..., Y and Z directions Operating pressure range 0 to 0.6 MPa Material ZDC2 Ni plating Applicable sensor E3AS-F, E3AS-L, E3AS-HL, E3Z, E3ZR, E3ZM Contents Material Air discharge The length of the sensor mounting screw is limited ...
- マニュアル
...sheet at your disposal. 2.Hold and screw the protective cover against the E3AS-HL reference plane. Reference plane * 5 6 3 0 5 4 7 - 0 A * © OMRON Corporation 2020 All Rights Reserved. The length of the sensor mounting screw is limited ...
- マニュアル
... pas directement dans la lumière sortante. Attention-L utilisation des commandes ou réglages ou l exécution des procédures autres que celles spécifiées dans les présentes exigences peuvent étre la cause d une exposition à un rayonnement dangereux. Do not disassemble this product. Doing ...
- マニュアル
.... Ne regardez pas directement dans la lumière sortante. Attention-L’utilisation des commandes ou réglages ou l’exécution des procédures autres que celles spécifiées dans les présentes exigences peuvent étre la cause d’une exposition à un rayonnement dangereux. Do not disassemble this product.Doing ...
- マニュアル
... regardez pas directement dans la lumière sortante. Attention-L utilisation des commandes ou réglages ou l exécution des procédures autres que celles spécifiées dans les présentes exigences peuvent étre la cause d une exposition à un rayonnement dangereux. Do not disassemble this product.Doing ...