全 1073 件が検索されました。(361 - 380件を表示)

  • マニュアル

    ... × hour or count × minute) Time Division width (See note.) Note The following table shows the divisions for the cumulative counter. 132 Section 5-4 Analog Input Units DRT2-AD2 Unit Hour Minute Divisions 3.6 ...

  • マニュアル

    ... Bit Input Slave Units, whichever is greater) × 0.5 μs] M Calculation Example Conditions Baud rate --- Word outputs Word inputs Bit outputs 8 nodes 16 nodes 16 nodes Bit inputs 8 nodes M = (16 × 0.625 µ...

  • マニュアル

    ... to Bit Slaves using e-CON connectors, clamp terminals, or compact connectors are supplied power from the CompoNet communications power supply. No separate wiring is required for I/O power supply. Industry Standard Sensor e-CON Connectors (CRT1-V@D08S(-1)/ CRT1-@D@...

  • マニュアル

    ...A-4 A-5 A-6 Channel/Relay Numbers ......................................................................................... 104 Instructions .............................................................................................................. 109 Inner Workings of CP1L/CP1E .................................................................................113 CP1L Programming Examples ................................................................................ 123 Comparison between CP1L and CP1E ................................................................... 174 Difference between CP1E E/N/NA……-type and E/N……...

  • マニュアル

    ... within specified time When operation is started in hot start mode (ITEM018 = 0), a hot start is performed after recovering from a power interruption if the time that power is interrupted is a within the time specified in ITEM037 (Hot start enabled time: 0 to 3,600 ...

  • マニュアル

    ... within the range of 1 condition. You cannot write the data of multiple sequences or multiple conditions with 1 instruction. S: Rightmost Word Number of Transfer Source Prepare the transfer data as follows in the word which you specified in S. Words S ...

  • マニュアル

    ... Units ................................................................................................................................. 2-4 2-2-1 2-2-2 2-2-3 2-3 General Specifications ................................................................................................................ 1-9 Characteristics .......................................................................................................................... 1-10 Functional Specifications .......................................................................................................... 1-12 Difference between E/N/NA-type and E/N...

  • マニュアル

    ...Related Manuals ...................................................................................................... 25 Section 1 1-1 Overview CP1E Overview ........................................................................................................................ 1-2 1-1-1 1-2 Basic Operating Procedure .................................................................................................... 1-4 1-3 Difference between E/N/NA-type and E/N...

  • マニュアル

    ...TIM 0002 (1.5 seconds) LD TIM 100.05 2 #0015 #0015 T0001 2.05 LD T0001 OUT 100.05 0.00 100.05 1.0 s 2-70 1.5 s 1.0 s 1.5 s CP1E/CP2E CPU Unit Instructions Reference Manual(W483) 2 Instructions 2) Clock Pulse 0.00 P. 1s (1-s clock pulse) 100.06 0.00 Instruction Operands LD 0.00 AND 1s OUT 100.06 • The internal clock pulse (0.1 s, 0.2 ...

  • マニュアル

    ...control Time IFEED executed 8-4-4 INTERRUPT FEEDING Instruction: IFEED(892) Execution condition @IFEED #0100 P: Port specifier, Example: Interrupt input 0 and pulse output 0 #0000 C: Control data, CW/CCW outputs and CW direction D0 ...

  • マニュアル

    ... rate 4.0 Mbps Word outputs 16 Units Word inputs 32 Units Bit outputs 64 Units Bit inputs 32 Units G = (16 × 5.31 µs) + (32 × 15.55 µs) + (64 × 0.66 µs) + (32 × 14.49 µs) ≅ 1.088 ms • 0.1 ms: Interval for inputting input data CJ-series CompoNet Master Unit Operation Manual for NJ-series CPU Unit (Cat. No. W493) 5-53 5-5-1 I/O Response Time The figures in parentheses are when message communications are not used. *1 Communications Mode 8 G = (Number of Word Output Slave Units × ...

  • マニュアル

    ... specified for each device: One for storing received data and the other for storing sent data. Writes the receive data to memory used for CJ-series Units during CPU Unit I/O refresh. Setting range: 0.01 to 0.99 s, 0.1 to 9.9 ...

  • マニュアル

    ... size: 5 bytes Node address 1: OUT size: 4 byte, IN size: 3 bytes Node address 2: OUT size: 1 byte, IN size: 2 bytes Allocation size setup table 15 I 1 5 s I+1 4 3 s+1 I+2 1 2 s+2 : : s+3 OUT block 1 IN block 1 15 00 00 k 00 00 01 01 k+1 00 00 01 01 k+2 02 k+3 Not usable Not usable : 00 : k+4 Not usable 01 01 Not usable 01 02 k+5 l: First word in allocation size setup table s: ...

  • マニュアル

    ... Power is Turned ON A-1 Supplementary Explanation of Functions A-1-8 Isolated-type Direct Current Input Unit Appendices A-1-9 Integral Value Calculation Integral Value Unit: Hour The process value is calculated using an integral width of 3.6 ...

  • マニュアル

    ... exceed the values in the table below. 4-34 NX-series System Units User's Manual (W523) 4 Installation and Wiring Connecting destination of Additional I/O Power Supply Unit NX-PF0730 Peak value 20 A*1 Pulse width 1 ...

  • マニュアル

    ...Communications Coupler Unit 6 Incremental Encoder Input Units Refresh Cycle The following table lists the refresh cycles for Free-Run refreshing, synchronous I/O refreshing, and task period prioritized refreshing. I/O refreshing method Refresh cycle Free-Run refreshing Always 125 µ...

  • マニュアル

    ...that is allocated to the STRING variable. • Upper and lower bytes are reversed. Example: The outputs will be as follows for a STRING array named s that has two elements (with the data quantity around elements is set to 4 bytes) when s[0] is “ab” and ...

  • マニュアル

    ...LREAL 0 Depends on data type. LREAL 0 Positive number or 0 LREAL 0 Positive number or 0 LREAL --- --- _eMC_BUFFER _MODE _mcAb orting _mcAborting Unit Command units/s*1 Command units/s2 Command units/s2 Description The velocity set value. The acceleration rate set value. The deceleration rate set value. --- The jerk set value.*2 --- Operation for multi-execution of motion control instructions _mcAborting: Aborting *1. Refer to Unit Conversion Settings in the motion control user's manual for information on command units. *2. This is a reserved variable. The user cannot assign a value to it. Sysmac Library ...

  • マニュアル

    ... unit is [command unit].*1 Set the measurement start position. The unit is [command unit].*1 Set the measurement end position. The unit is [command unit].*1 Set the velocity for the X-axis movement to the preparation position. The unit is [command unit/...

  • マニュアル

    ... Comparison Table Depending on the number of target values in the table, the target-value comparison table requires a continuous block of 4 to 19 words. 15 S 0 0001 to 0006 hex (1 to 6 target values) Number of target values ...