全 1073 件が検索されました。(341 - 360件を表示)
- マニュアル
... Operation Manual or Programming Manual. Example Conditions Master node address: 63 Slave network address: 1 Slave node address: 2 Example: Using the CMND Instruction Command Words (S: First Command Word) Word Contents (Hex) Meaning S 28 01 ...
- マニュアル
... 03: 0 to 3 hex 0 (0 hex) Decimal point position (from right) for instantaneous value when 100% input --- Bit 04 to 07: 0 to 4 hex 0 (0 hex) Instantaneous value time unit (matching conversion period) 0: 1 ...
- マニュアル
... at the local node) to remote node N. In return, “m” bytes of response data are stored at the local node beginning with D (the beginning word for storing response data). 15 Remote (source) node N Local node 0 S ••• (...
- マニュアル
... to 3-5-4 Editing User Link Tables. Refresh period The refresh cycle for CPU Unit data. The cycle can be set to the system common operating cycle, 0.01 s, 0.02 s, 0.05 s, 0.10 s, 0.20 s, 0.50 s, 1.00 s, or 2.00 s (If the user link table is pasted in a block diagram to make software connections and the function block data is downloaded to the Loop Control Board with the Update User Link Table Refresh Cycle selection selected in the CX-Process Tool, the setting made here ...
- マニュアル
...Process Tool or FINS command. block Function block Standard: Operation of all function blocks is executed at the same operation cycle preset operation cycle to ITEM 004 in the System Common block. Settable operation cycles: 0.1 s, 0.2 s, 0.5 ...
- マニュアル
....00 Yes r/w R – – S 2 output +115.00% Parameter 030*2 TMU SP rate-of-change limit 0 to 2 0 – R/W (S) – – – – 1 time unit 0: s, 1: min, 2: hr Parameter 032 Bumpless output between 0, 1 0 – R/W(S) – – – – 1...
- マニュアル
...128 Master’s node number: 63 Slave’s network address: 1 Slave’s node number: 2 Section 6-3 Explicit Message Communications CMND(194) Operand Details [CMND S D C] • Command Words Word S S+1 S+2 S+3 S+4 S+5 Contents Function (Hex) 28 01 EXPLICIT MESSAGE SEND command code = 2801 (Hex) 02 1C Slave node number = 02 (Hex) READ BYTE DATA command service code = 1C (Hex) 00 2F Class ID = 002F (Hex) 00 01 Instance ID = 0001 (Hex) specifies data area 0A 00 Starting read address = 000A (Hex) specifies IR 010 Address L = 0A (Hex); ...
- マニュアル
... 15 DM 6611 00 to 15 DM 6612 00 to 15 DM6645 00 to 15 DM6646 00 to 15 Function ABS resolution Rightmost 4 digits (the No. of input pulses for Leftmost 4 digits encoder's 1 revolution) Note: HCA12V1 Only Details 0000 0001 to 0000 8000 Hex Note: Set the resolution considering servo driver's "encoder dividing rate" and unit's "pulse input multiplication setting". Ex: “Driver: 1000, unit: with multiplication of 4”: FA0 (4000) Maximum ring counter value for high-speed counter 2 Note: HCP22V1/HCA22-V1 Only ABS offset value Note: HCA12V1 only As above. Rightmost ...
- マニュアル
... Unit CPU Unit Interpretation1 Interpretation2 Command data Response No. of command bytes Response Response monitoring time ...... S+2 S+3 S+4 Command Destination node Local Master Unit CPU Unit S+1 Operands C: Control code S: 1st source word D: Destination information Execution L Execution ... Response data 1: For commands addressed to Master Unit 2: For commands addressed to CPU Unit Description IOWR transfers data from the words beginning at S to the specified Special I/ O Unit. The control code (C) specified parameters for the instruction as shown in the following illustration. C: Destination unit address (see ...
- マニュアル
... size: 5 bytes Node address 1: OUT size: 4 byte, IN size: 3 bytes Node address 2: OUT size: 1 byte, IN size: 2 bytes 15 Allocation size setup table I 1 5 s I+1 4 3 s+1 I+2 1 2 s+2 : : s+3 OUT block 1 15 k 00 00 01 01 k+1 00 00 01 01 k+2 02 k+3 Not usable : k+4 00 Not usable 01 01 Not usable 01 02 k+5 l: First word of the allocation size setup table s: First word of OUT block 1...
- マニュアル
...Ladder Symbols IR, SR, AR, DM, EM, TIM/CNT, LR, # MOVL(––) @MOVL(––) S S D D 000 000 D: Starting destination word Limitations IR, SR, AR, DM, EM, LR, # 000: Always “000” 000 S and S+1 must be in the same data area, as must D and D+1. DM 6144 to DM 6655 cannot be used for D. Note When using this instruction from the CX-Programmer, set bits 08 to 11 of DM 6600 in the Unit Setup Area to 1 to enable user-specified expansion instruction settings before uploading and downloading the program. On the CX-...
- マニュアル
...Setting time (unit: 0.1 s) 0 to 999.9 s Binary mode TTIMX &0 to &65535 (decimal) or #0000 to #FFFF (hexadecimal) 0 to 6,553.5 s LONG TIMER (100 ms) Instruction name BCD mode Mnemonic S, S+1 (timer set values) TIML #00000000 to #99999999 (BCD) Setting time (unit: 0.1 s) 0 to 999.9 s Binary mode TIMLX &0 to &4294967295 (decimal) or #0000 to #FFFFFFFF (hexadecimal) 0 to 6,553.5 s MULTI-OUTPUT TIMER (100 ms) Instruction name Mnemonic S to S-7 (each timer set value) BCD mode MTIM #0000 to #9999 (...
- マニュアル
... intend to use two CV’s (e.g. CV 0 and CV 15) then you still have to define the number of CV’s (M) to be 16. In order to prevent configuration errors from happening you should make sure that the data of CV’...
- マニュアル
... Status Flags turns ON. Analog input value Cumulated value (count x hour or count x minute) Time Division width Note The following table shows the divisions for the cumulative counter. DRT2-AD04 Unit Hour Minute Divisions 3.6 ...
- マニュアル
... is continued before operation is started) is possible CX-Process Tool or FINS command. Standard: Operation of all function blocks is executed at the same operation cycle preset to ITEM 004 in the System Common block. Settable operation cycles: 0.1 s, 0.2 s, 0.5 ...
- マニュアル
... number of words, starting from the beginning word S at the remote node (node address M) is received at the words starting from the beginning word D at the local node. 15 Local node 0 Destination node number N S Command (...
- マニュアル
.... 98 Section 4-10 Batch Trend Screens • The trend data collection cycle and maximum save time in a Batch Trend Screen are shown in the following table. Item Collection cycle (See note.) Maximum save time Note Details 1 ...
- マニュアル
... number of words, starting from the beginning word S at the remote node (node address M) is received at the words starting from the beginning word D at the local node. 15 Local node 0 Destination node number N S Command (...
- マニュアル
...1 N = 1 kg·m·s−2 Pressure, stress pascal Pa Energy, work, quantity of heat Power, radiant flux joule J 1 Pa = 1 N·m−2 1 J = 1 N·m watt W 1 W = 1 J·s−1 Electric charge, coulomh quantity of electricity Electric potential, volt electromotive force Electric capacitance farad C 1 C = 1 A·s V 1 V = 1 W·A−1 F 1 F = 1 C·V−1 Electrical resistance Ω 1 Ω = 1 V·A−1 Electric conductance siemens S Magnetic flux weber Magnetic flux density tesla wb T 1 ...
- マニュアル
...PLC model CJ2M CPU Unit model CPU68/67/66/65/64/68-EIP/67-EIP/66-EIP/65-EIP/ 64-EIP CPU35/34/33/32/31/15/14/13/12/11 CS1G-H*1 CS1H-H*1 CS1D-H*1 CS1D-S*1 CJ1G-H*1 CJ1H-H*1 CJ1M*1 CPU45/44/43/42 CPU67/66/65/64/63 CPU68A/67A CPU67A/44A CPU45/44/43/42 CPU67/66/65/67-R/66-R/65-R/64-R CPU23/22/21/13/12/11 CJ2H *1.with unit version 4.0 or later 4-2-2 Specifications Item Specification...