全 5560 件が検索されました。(3681 - 3700件を表示)

  • マニュアル

    ...x 1001 9 HT EM ) 9 I Y i y 1010 A LF SUB * : J Z j z 1011 B VT ESC + ; K [ k { 1100 C FF FS , < L \ l | 1101 D CR GS Ć = M ] m } 1110 E S0 RS . > N ^ n ~ 1111 F S1 US / ? O _ o 63 Revision History A manual revision code appears as a suffix to the catalog number on the front cover of the manual. Cat. No. Z043–E1–01A Revision code The following table outlines the changes made to the manual during each revision. Revision code Date 1 June 1990 01A December 2004...

  • マニュアル

    .... Memory Backup Characteristics Ambient temperature (°C) 10 Section V600-CAjA-Vj ID Controller 2-1 2-1-3 External Input/Output Specifications Input Specifications (RESET) Input voltage 24 VDC: +10% (including ripple component), –15% Input impedance 2.2 ...

  • マニュアル

    ...Keyboard Some keys cannot be used. 2 Coiled modular phone cable Connected to Keyboard Adaptor Keyboard Adaptor No. Name Remarks 1 Visual Controller connector Attached to Visual Controller RS-232C connector 2 Selector Set to ...

  • マニュアル

    ... (for 1 minute) (see note) Interface Video output In accordance with RS-170 Composite video signal, Amplitude 1.0 Vp-p/75 W RS-232C 1 port Parallel I/O 11 inputs (photocoupler) 29 outputs (open collector) User program capacity 16 ...

  • マニュアル

    ... the program is to branch. Comments ––– Reference GOSUB, ON...GOTO Sample Program When you press one of the cursor control keys, the system will display on the screen the name of the key you pressed and end execution of the program. 100 ...

  • マニュアル

    ...Connection Diagram The following diagram shows how the E5AX is connected to the host computer using RS-485. VDD SN751177N or equivalent E5AX: SW601 of Controllers other than the terminator must be turned off. Host computer RS-485 Abbreviation 51 ...

  • マニュアル

    ... provides information on how the RS-485 Intelligent Signal Processor is to be connected to the host computer. Intelligent Signal Processor side: Turn OFF all terminal block switches except at the end-station. Host computer RS-485 Abbreviation 5V 47 ...

  • マニュアル

    .... . . . . . . . . . . 4-4-9 Command Processing Terminating Command (AA) . . . . . . . . . . . . . . . . . . . . . . . 4-4-10 Data Check Command (MD C/K) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-11 Data Management Command (MDS/MDL) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-12 Write Processing Repeat Command (RP) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-13 Controller Control Command (CC) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-14 Error Information Read Command (CF) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-15 Test Command (TS) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-16 Abort Command (XZ) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-17 Command Undefined Response (IC) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-18 Error Response . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-19 End Code List . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Example of Communications Program . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 24 28 28 28 29 32 36 36 37 37 38 39 40 40 41 42 42...

  • マニュアル

    ...The following Strobes can be connected to the Strobe Unit. F300-L100EV2 OVL Unit The F300 can be operated using the OMRON Visual Language (OVL). Commands and data are input from a special keyboard connected to an OVL Unit. F300-L100EV2 OVL Unit F300-...

  • マニュアル

    ...” those that you do not wish to be displayed. (see note 1) W. Set by window W. Window W. Drawing window P. Parameters Selection of window number Window drawing (editing, deletion) See note 2 K. Camera I. Parameters display See note 3 O. Conditions Binary level S. Settings X. Clear M. Shading Master Position W. Window Position 1. Setting: 1 Window 2. Setting: 2 Windows R. Reference Image P. Parameters Note 1. “Display window no.” under the “D. Display” menu is only a function for selecting the numbers of those windows that are not normally to be displayed. It ...

  • マニュアル

    ...95 GOSUB Branches to a specified subroutine. General Command 95 GOTO/GO TO Unconditionally jumps to a specified line. General Command 96 Section 1-1 OVL Alphabetical List Command/Function H I J K Operation Instruction Type Page HELP Displays help messages. Program editing Command 96 HELP ON/OFF/STOP Disables, enables, or stops interrupts from the HELP Key. Key control Command 96 HEX$ Converts a numeric expression to hexadecimal. 1-byte character string operation Function 97 HISTGRAM Reads a density histogram. Image processing Command 97 IF. . . GOTO ~ ELSE Evaluates a condition. General Command 98 IF. . . THEN ~ ELSE Evaluates a ...

  • マニュアル

    ...1-2 Models The thermocouples and platinum resistance thermometers listed in the following table can be connected to any Thermac E5jJ Temperature Controller. Input Selectable internally. Platinum resistance thermometer JPt100 Temperature range (°C) INPUT Factory-set to 2 (...

  • マニュアル

    ...C P 2 $ D Q 3 % E R 4 & F S 5 ’ G T 6 ( H U 7 ) I V 8 ^ J K L M WX Y Z 9 . – _ ‘ 17 Section 1-4 Menu Configuration In addition to these characters, the following functions are available. Display 1, 2, 3... Operation DEL Deletes the character at the cursor position. BS Deletes the character just to the left of the cursor position. INS Toggles between insert and overwrite mode. (The default is overwrite mode.) ← Moves the cursor to the left. → Moves the cursor to the right. END Ends the character input operation....

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K.Environment . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . B.Backup . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . M.Memory Card . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . E.End . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 6 Maintenance . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6-1 6-2 Maintenance Parts and Replacement Parts . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Inspection . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 7 Troubleshooting . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7-1 7-2 Errors . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Error Messages . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 8 Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 8-1 8-2 8-3 Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Dimensions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Lens Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . vii TABLE OF CONTENTS Appendix A Comparison of New and Old Models . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . B RS-232C Data Transmission Program Examples . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Glossary . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Index . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . viii About this Manual: This manual describes the installation and operation of the Setup Menu of the F350 Visual Inspection System and includes the sections described below. Please read this manual ...

  • マニュアル

    ... be sure that the Units shown in the basic system configuration are included, as well as any peripheral devices that may be required. Basic System Configuration (Must be used.) KF350-C12E F350-C41E IMP Unit Processes images. F300-P2 (100 to 120 VAC) ...

  • マニュアル

    ... Carrier was soaked in hot water (100_C for 16 hours), and extracted ions were analyzed. The results are shown below. • Extracted Ions (Concentration) Na+ . . . . 10 p.p.m. Cl– . . . . 0.5 p.p.m. + K+ . . . . . 1.0 p.p.m. NH4 . . 11 p.p.m. • Results of ICP Emission Spectral Analysis The V600-D23P66SP Data Carrier was soaked in concentrated hydrochloric acid (which can easily penetrate through PFA) at 80_C for 300 hours, then extracted substances were analyzed. • Extracted Substances (Concentration) Si . . . . . 700 ng/ml S . . . . . 1000 ng/ml Ca . . . . . 30 ng/ml 116 Appendix Optional Accessories...

  • マニュアル

    ... command (MD). A CRC (Cyclic Redundancy Check) code calculation, overwrite, and comparison are made, using the check block units specified by the user. The CRC code is calculated from the polynomial expression created; x16 + x12 + x5 + 1. Command Format M D C/...

  • マニュアル

    ... Carrier. Results of Ion-exchange Chromatography A built-in Data Carrier was soaked in hot water (100°C for 16 hours), and extracted ions were analyzed. The results are shown below. Extracted Ions (Concentration) Cȏ: 0.5 ppm, Na+: 10 ppm, NH4+: 11 ppm, ...

  • マニュアル

    ... Carrier was soaked in hot water (100_C for 16 hours), and extracted ions were analyzed. The results are shown below. • Extracted Ions (Concentration) Na+ . . . . 10 p.p.m. Cl– . . . . 0.5 p.p.m. + K+ . . . . . 1.0 p.p.m. NH4 . . 11 p.p.m. • Results of ICP Emission Spectral Analysis The V600-D23P66SP Data Carrier was soaked in concentrated hydrochloric acid (which can easily penetrate through PFA) at 80_C for 300 hours, then extracted substances were analyzed. • Extracted Substances (Concentration) Si . . . . . 700 ng/ml S . . . . . 1000 ng/ml Ca . . . . . 30 ng/ml 78 Appendix A Accessories (...

  • マニュアル

    ... Input Terminals Wired to external devices, such as synchronous sensors or inputs from a Programmable Controller. I Output Terminals Wired to external devices, such as synchronous sensors or outputs to a Programmable Controller. J Monitor Connector Connects to the monitor. ...