全 5560 件が検索されました。(3741 - 3760件を表示)

  • マニュアル

    ...V - C A 1 0 1 . 0 0 0 CR Version •Other commands Either OK or ER is returned according to the result of the command. The command was executed successfully: O K CR The command was not executed successfully or the setting was NG: E R CR The delimiter can be selected from the following three types: CR/LF/CR+LF ZFV-C Non-procedural Communication Command Reference 3 1feature.fm 4 ページ 2006年6月6日 火曜日 午後6時30分 List of Non-procedural Commands List of Non-procedural ...

  • マニュアル

    ... used for calculation. The calculation setting is enabled only in the EXP mode. Icon Description Set any equation to perform addition/subtraction on the measurement result. The equation can be substituted with measurement results obtained by other tasks. Calc Allowable equation: ...

  • マニュアル

    ...111 Position 59 Position correction 98, 106, 109 Power connector 18 Pre-processing 86 Profile 130 J Judge 100 Judgment indicator 17 Judgment output destination 120 Judgments list 106, 109 K Key Lock 125 R L Language Lenses Light Control Loading Data 127 23 91 129 Recipe Function 91 Registering Images 97 RS-232C/422 connector 18 RUN Mode 31, 42, 106 S M Measurement Condition Adjusting 112 Setting 38 measurement display settings 123 Measurement items Selecting 39 Measurement items and banks 33 Measurement regions Setting 40 Measurement values/judgment 100 Memory capacity 132 Menu Button ADJ Mode 110 RUN ...

  • マニュアル

    ... a PLC, refer to the Instruction Manual for the PLC. ZFX-C Serial Communication Command Reference Connection 5 About Communication Commands Command/Response Format < Command > Command data Delimiter < Response > When processing ends successfully Response data O ...

  • マニュアル

    .... Menu sheet Section 4 Menu Sheet/Command List 80 Command Menu sheet Command "A" is set. 0A "I" is set. 0I "B" is set. 0B "J" is set. 0J "C" is set. 0C "K" is set. 0K "D" is set. 0D "L" is set. 0L "E" is set. 0E "M" is set. 0M "F" is set. 0F "N" is set. 0N "G" is set. 0G "O" is set. 0O "H" is set. 0H "P" is set. 0P V500-R521B2/C2 User’s Manual V500-R521.book 81 ページ 2008年7月18日 金曜日 ...

  • マニュアル

    ...input Number of channels section A/D resolution Photo MOS relay scanning system; all channels isolated 10 ch 16-bit Measurement Voltage ranges Temperature Humidity (*1) Measurement Voltage accuracy Thermo(*2) (*3) couple Thermocouples: ...

  • マニュアル

    ...) – ............................................. Low-voltage terminal (terminal for low-voltage input signals) Item 18 Description Input configuration Isolated input, scanning Analog voltage 20, 50, 100, 200, 500 mV/F.S.; 1, 2, 5, 10, 20, 50 V/F.S.; 1-5V Thermocouples ...

  • マニュアル

    ... max. A/D resolution 16-bit Measurement Voltage ranges Temperature 20, 50, 100, 200, 500 mV; 1, 2, 5, 10, 20, 50 V; 1-5 V F.S. Humidity (*1) Measurement Voltage accuracy Thermocouple Type (*2) (*3) Thermocouples: ...

  • マニュアル

    ... isolated within each channel. Terminal b is shorted within all channels. Item Description Input configuration Isolated input, scanning Analog voltage 20, 50, 100, 200, 500 mV/F.S.; 1, 2, 5, 10, 20, 50 V/F.S.; 1-5V Thermocouples ...

  • マニュアル

    ...Camera only Camera with lighting Optional lighting Overall judgment result P J Judge Judgment Judgment indicator Judgment output destination Judgments list 126, 117 117 17 142 129 Key Lock 148 K L Labeling Lenses Light Control Loading Data Logging monitor 129 122, 126, 67 23 108 153 128, 222 INDEX Panel output dimensions Parallel Connector Specifications Parallel I/O cable Connecting Pin assignment Parallel port Parameter Setup Partial Function Settings Password Pattern Search Perform Re-measurement Position Position correction 115, 126, Power connector Pre-processing Profile 208 160 Recipe Function Registering Images Revision History RS-232C/422 connector RUN Mode...

  • マニュアル

    ... a PLC, refer to the Instruction Manual for the PLC. 6 Connection ZFX-C Serial Communication Command Reference About Communication Commands Command/Response Format < Command > Command data Delimiter < Response > When processing ends successfully Response data O ...

  • マニュアル

    ..._X*H_ One-shot duration: 30 ms [X*I _X*I_ 76 V400-R1CF/R1CS User’s Manual Section 4 Setting Method Menu sheet One-shot duration: 40 ms Command [X*J _X*J_ [X*K One-shot duration: 50 ms _X*K_ One-shot duration: 60 ms [X*L _X*L_ One-shot duration: 70 ms [X*M Section 4 Menu Sheet/Command List _X*M_ [X*N One-shot duration: 80 ms _X*N_ One-shot duration: 90 ms [X*O _X*O_ One-shot duration: 100 ms [X*P _X*P_ V400-R1CF/R1CS User’s ...

  • マニュアル

    ...) – ........................... Low-voltage terminal (terminal for low-voltage input signals) Item Description Input configuration Isolated input, scanning Analog voltage 20, 50, 100, 200, 500 mV/F.S.; 1, 2, 5, 10, 20, 50, 100, 200, 500V/F.S.; 1-5V Thermocouples ...

  • マニュアル

    ... are output when the command is processed normally, and the command execution result is OK. A delimiter is inserted at the end of the response. The delimiter is always CR. Command Execution Result Parameter 1 0 CR Delimiter O ...

  • マニュアル

    ...-voltage input signals) –....................................Low-voltage terminal (terminal for low-voltage input signals) Item Description Input configuration Isolated input, scanning Analog voltage 20, 50, 100, 200, 500 mV/F.S.; 1, 2, 5, 10, 20, 50 V/F.S.; 1-5V Thermocouples ...

  • マニュアル

    ... all channels. 28 Connecting the Signal Input Cables ZR-RX45 User’s Manual Item Description Isolated input, scanning Analog voltage 20, 50, 100, 200, 500 mV/F.S.; 1, 2, 5, 10, 20, 50 V/F.S.; 1-5V Thermocouples ...

  • マニュアル

    ... execution result is OK. A delimiter is inserted at the end of the response. The delimiter is always CR. 304 No-protocol Connections FQ-M User’s Manual Command Execution Result Parameter 1 0 CR Delimiter O ...

  • マニュアル

    ...GetSystemData G GetUnitData G GetUnitFigure G gosub G goto H hex$ I If I ImageFormat I input # I input$ I int I isfile J JudgeOut K kill L left$ L len L line input # L list L load L log L Loop While L lsqumeth M MeasureDispG 164 Using Custom Command FZ4 User's Manual MeasureId$ M MeasureProc M mid$ M mkdir M mod N new N Next N not O on O open O or P ParallelExecute P piece$ P print P print # P PutAll P PutPort R ReceiveData R rem R RenumUnitNo R RGB R right$ R rmdir...

  • マニュアル

    ... Controller. Measuring the Thickness p.232 • For the operation of the thickness scaling, refer to p.88. ZW User's Manual Setting Measurement Items 81 Performing Calculations Perform calculations using the results calculated by the tasks. The calculation formula is mX+nY+...

  • マニュアル

    ... mode. Surface for measurement1,2 Sets a plane to gain measured values within a selected area. * When "Thickness" of the measurement mode(TASK*) is selected, Measurement surface 2 is also set and its thickness is calculated. Operation parameter X,Y,...