全 5560 件が検索されました。(3701 - 3720件を表示)

  • マニュアル

    ...CompoBus/D, 81 terminal blocks, 64 keys, RS-232C, 92 using STEP terminal, 64 input terminals, 64 non-measurement commands, 69 with handshaking, 70 without handshaking for continuous measurement, 67, 68 using STEP signal, 66 installation, overview, 4 ...

  • マニュアル

    ... Camera. F Wired to the power supply. G Wired to a ground. H Wired to external devices, such as synchronous sensors or inputs from a Programmable Controller. I Wired to external devices, outputs to a Programmable Controller. J Connects to the video monitor. ...

  • マニュアル

    ... the Camera. F Wired to the power supply. G Wired to a ground. H Wired to external devices, such as synchronous sensors or inputs from a Programmable Controller. I Wired to external devices, outputs to a Programmable Controller. J Connects to the monitor. ...

  • マニュアル

    ... Indicator Lit in RUN mode. C ERROR Indicator Lit when an error occurs. I D RS-232C Connector Connects the F150 to a computer, Programmable Controller, or other external device. J E Camera Connector Connects to the Camera. ...

  • マニュアル

    ...See also input format; output format I/O monitor 148 images adjusting 47 for position compensation 64 changing 166 overview 3 storing 162, 207 types displayed 24 JG 127 judgement output 304 output expressions 122, 129, 209 ...

  • マニュアル

    ...c d q r 2 3 % DEL E F GH I J S T U VWX e f g h i j s t u v w x 4 5 6 7 8 9 ( ) ^ ` BS INS ← → 1. K Y k y . L MN Z l m n z - - ! These characters can be input. SPC DEL BS INS ← → END END Inserts a space. Deletes 1character to the right of the I cursor. Deletes 1character to the left of the I cursor. Switches between insert (default)/overwrite. Moves the I cursor to the left. Moves the I cursor to the right. Ends ...

  • マニュアル

    ...CTRL + Z ($1A) F1 Key CTRL + C ($03) F2 Key CTRL + V ($16) F3 Key CTRL + B ($02) F4 Key CTRL + N ($0E) F5 Key CTRL + J ($0A) F6 Key CTRL + K ($0B) F7 Key CTRL + L ($0C) F8 Key CTRL + O ($0F) F9 Key CTRL + P ($10) --- (See note.) CTRL + Q ($11) Note Changes the serial interface input to normal (no-protocol) mode. This input is valid only in Monitor Mode and Run Mode. 15 Setting Communications Specifications 2-1-2 Section 2-1 Inputting Characters from the Computer The computer can be used to input filenames and comments ...

  • マニュアル

    ...c d q r 2 3 % DEL E F GH I J S T U VWX e f g h i j s t u v w x 4 5 6 7 8 9 ( ) ^ ` BS INS 1. K Y k y . L MN Z l m n z - - ! These characters can be input. Inserts a space. Deletes 1character to the right of the I cursor. Deletes 1character to the left of the I cursor. Switches between insert (default)/overwrite. Moves the I cursor to the left. Moves the I cursor to the right. END Ends character input. SPC DEL BS...

  • マニュアル

    ...) * This can be set by a dip switch of the controller. For how to set, refer to Chapter 3. 2-1-5 I/O Specifications • Input Specifications (RST/IN) Specifications Input voltage 24 VDC ±10% (including ripple) Input impedance 2.2 ...

  • マニュアル

    ...+P C -P D RS-422A RD (Receiving) RD+ E RD- F RS-422A SD (Sending) SD+ SD- G H RS-232C Receiving Rx J RS-232C Sending Tx K RS-232C Signal 0 V SG L Frame ground GR M Setting Usage Pin Layout Supply 24 VDC. Short-circuit for setting mode. Refer to Section 6-1. This pin is not connected in operation mode. Use for RS-422A communications. (Terminating resistance 220 Ω is connected to both RD and SD in the Antenna.) Do not connect when RS-232C is used. Use for RS-232C communications. Do not...

  • マニュアル

    ...-C300E will send “READY” to the external device when it is ready to load. Transfer the system data after receiving “READY”. Send Load System Data via XModem Command @ Y

    L Receive Data Loaded Correctly
    O ...

  • マニュアル

    ... the Camera. F Wired to the power supply. G Wired to a ground. H Wired to external devices, such as synchronous sensors or inputs from a Programmable Controller. I Wired to external devices, outputs to a Programmable Controller. J Connects to the monitor. ...

  • マニュアル

    ...4 to 20 mA LOW output GND (0 V) Pink Laser OFF input Purple Timing input Orange Zero reset input Red Reset input Black Linear output Voltage output 4V Current output: 300 max. 10 k min. Load Voltage output: Shield Linear output GND 6 Z157-E1-01C.book Page 7 Thursday, August 31, 2006 5:13 PM Section 1-3 I/O Circuit Diagrams 1-3-2 PNP Amplifier Unit: ZX-LDA41 Brown 12 to 24 VDC White HIGH output Green PASS output Gray Load 12 to 24 VDC LOW output Load Internal circuits Load Blue GND (0 V) Pink...

  • マニュアル

    ... ka o 4 od ufa E F ma 530 wa rati 0.1 uc ctu acto nu JA , Sh on 0 a t co nd m re ry, fac PAN imo d OM tu gy 10 plie in R re o-k 40 s O : u, N .1 wit C 1. h orp DANGER Certification and Identification Label . Laser radiation is emitted from this aperture AVOID EXPOSURE Certification and Identification Label Laser Safety CAUTION Caution Label Aperture Label PEAK POWER 15000 µw PULSE DURATION 25000 µs WAVE LENGTH 658 This laser product complies with 21 CFR 1040.10 and ...

  • マニュアル

    ...is emitted from this aperture PEAK POWER 1000 µw PULSE DURATION 10000 µs WAVE LENGTH 650 ith w . es 1 pli 0.1 m 04 co 1 ct nd du 0 a u, o-k pro 0.1 y r g 4 n se 0 tio imo . la 1 ra h N : orp is FR o a, S PA C Th 1 C orpkaw JA ture ON 2 C ori 530 fac MR N O H -8 u O R oji 00 an ry, M iok 6 m to in O Sh yoto of Fac red ...

  • マニュアル

    ...1. 2. Move the cursor to the item for which a value is to be changed. Press the ENT Key. The cursor will change to a cursor the size of a single digit. Scn0 SET Equation A= B= K= Zero Upper Lower K A Sensor0.Avg .Frnt Sensor0.Avg .Frnt [ 0.0000]mm [ 0.0000]mm [ 5.0000]mm [ -5.0000]mm End 10 Section 1-1 Menu Operation 3. Move the cursor to the digit to be changed. Use the Left and Right Keys to move the cursor. 4. Change the value. Use the Up Key to increase the...

  • マニュアル

    ...

    SECTION 8 Communication with the Host Function 2 • • • Changes the currently displayed scene. Send @ S N
    Set the desired scene number (0 to 9). Receive Command executed correctly:
    O ...

  • マニュアル

    ...QR c d q r 2 3 % DEL E F GH I J S T U VWX e f g h i j s t u v w x 4 5 6 7 8 9 ( ) ^ ` BS INS K Y k y . L MN Z l m n z - - ! ¨ 1. These characters can be input. Inserts a space. Deletes 1character to the right of the I cursor. Deletes 1character to the left of the I cursor. Switches between insert (default)/overwrite. Moves the I cursor to the left. Moves the I cursor to the right. END Ends character input. SPC DEL...

  • マニュアル

    ...CTRL + Z ($1A) F1 Key CTRL + C ($03) F2 Key CTRL + V ($16) F3 Key CTRL + B ($02) F4 Key CTRL + N ($0E) F5 Key CTRL + J ($0A) F6 Key CTRL + K ($0B) F7 Key CTRL + L ($0C) F8 Key CTRL + O ($0F) F9 Key CTRL + P ($10) --- (See note.) CTRL + Q ($11) Note Changes the serial interface input to normal (no-protocol) mode. This input is valid only in Monitor Mode and Run Mode. 15 Z172-E1-02A.book Page 16 Friday, June 16, 2006 1:42 PM Setting Communications Specifications 2-1-2 Section 2-1 Inputting Characters ...

  • マニュアル

    ...c d q r 2 3 % DEL E F GH I J S T U VWX e f g h i j s t u v w x 4 5 6 7 8 9 ( ) ^ ` BS INS 1. K Y k y . L MN Z l m n z - - ! These characters can be input. Inserts a space. Deletes 1character to the right of the I cursor. Deletes 1character to the left of the I cursor. Switches between insert (default)/overwrite. Moves the I cursor to the left. Moves the I cursor to the right. END Ends character input. SPC DEL BS...