全 5560 件が検索されました。(3761 - 3780件を表示)

  • マニュアル

    ... Controller. Measuring the Thickness p.306 • For the operation of the thickness scaling, refer to p.92. ZW User's Manual Setting Measurement Items 85 Performing Calculations Perform calculations using the results calculated by the tasks. The calculation formula is mX+nY+...

  • マニュアル

    ... actual system. Also, periodically check that the response time of the machine has not changed. 4 Detection Zone Orthogonal to Direction of Approach Installation Considerations Chapter 4-1-2-1. Safety Distance Formulas according to ISO 13855/EN ISO 13855 S = ...

  • マニュアル

    ... status .................................................... 4-20 Information ............................................................ 9-7, 9-12 Input terminal block ........................................2-9, 2-27, 4-3 Installation environment ............................................... 2-10 Installation space .......................................................... 2-10 Installing the marking data ............................................. 7-2 IO ERROR ........................................................... 4-15, 4-24 ...

  • マニュアル

    ...0 1 2 3 4 5 6 7 8 9 : ; < = > ? Input @@ A B C D E F G H I J K L M N O Code A @ A B C D E F G H I J K L M N O Code B @ A B C D E F G H I J K L M N O Input P Q R S T U V W X Y Z [ Code A P Q R S T U V W X Y Z [ Code B P Q R S T U V W X Y Z [ ] ^ _ ] ^ _ ] ^ _ Input ` a...

  • マニュアル

    .... Therefore they must not be included as an active sensing surface in safety distance calculation. According to EN ISO 13855, the minimum distance, S, in millimeters, from the detection zone to the harzard zone shall not be less than that calculated using the following equation: S = (...

  • マニュアル

    ...informacije i upute o instalaciji, rukovanju, upotrebi i sukladnosti/sigurnosti. A-8 Fiber Laser Marker MX-Z2000H series Setup Manual (Z376) Appendix TENTO PRODUKT JE PRŮMYSLOVÝM PRODUKTEM URČENÝM pro zabudování A POUŽití V PRŮMYSLOVÝCH ZAŘÍZENÍCH, přístrojích NEBO INSTALACÍCH. NENÍ URČEN ...

  • マニュアル

    ...0 1 2 3 4 5 6 7 8 9 : ; < = > ? Input @@ A B C D E F G H I J K L M N O Code A @ A B C D E F G H I J K L M N O Code B @ A B C D E F G H I J K L M N O Input P Q R S T U V W X Y Z [ Code A P Q R S T U V W X Y Z [ Code B P Q R S T U V W X Y Z [ ] ^ _ ] ^ _ ] ^ _ Input ` a...

  • マニュアル

    ... actual system. Also, periodically check that the response time of the machine has not changed. 4 Detection Zone Orthogonal to Direction of Approach Installation Considerations Chapter 4-1-2-1. Safety Distance Formulas according to ISO 13855/EN ISO 13855 S = ...

  • マニュアル

    ... actual system. Also, periodically check that the response time of the machine has not changed. 4 Detection Zone Orthogonal to Direction of Approach Installation Considerations Chapter 4-1-2-1. Safety Distance Formulas according to ISO 13855/EN ISO 13855 S = ...

  • マニュアル

    ...5 VDC 4 to 6 VDC G3RZ-201SLN 12 VDC 9.6 to 14.4 VDC 24 VDC 19.2 to 28.8 VDC * This varies depending on the ambient temperature. Model Input Impedance 400 Ω ± 20% 1.1 kΩ ± 20% 2.2 kΩ ± 20% Voltage level Operating voltage Release voltage 4 VDC max. 9.6 VDC max. 1 VDC min. 19.2 VDC max. Rated load voltage 5 to 240 VAC 5 to 100 VDC Output Load voltage Load current* range 3 to 264 VAC 3 to 125 VDC 100 μA to 1.0 A Inrush current injection amount 10 ...

  • マニュアル

    ... actual system. Also, periodically check that the response time of the machine has not changed. 4 Detection Zone Orthogonal to Direction of Approach Installation Considerations Chapter 4-1-2-1. Safety Distance Formulas according to ISO 13855/EN ISO 13855 S = ...

  • マニュアル

    ... ! S D 2 B R b X 2 ” E D C S c X 3 # 3 E D D T d T 4 $ 4 E N E U e Q K % 5 A S F V f K N & 6 B E L B B C S H N E T L M S F H B E M C C ↑ R ↓ S O → S I ← L C 7 8 ) 9 * : + ; , < - = . > / ? ’ ( Character Code Table G H I J ...

  • マニュアル

    ...) is inserted in the reception character string delimiter section. The size of the reception data includes the final 0x00. Example: Getting the Number (0) of the Current Scene Send data (2 bytes): 0x53('S') 0x00 ↓ Receive data (5 bytes): 0x30('0') 0x00 0x4f('O') 0x4b('...

  • マニュアル

    ... Cables length: 0.2 m, 0.3 m, 0.5 m, 1 m, 1.5 m, 2 m, 3 m, 5 m, 7.5 m, 10 m, 15 m, 20 m Rugged type Cable with Connectors on Both Ends (RJ45/RJ45) XS5W-T421-MD-K • Wire Gauge and Number of Pairs: AWG22, 2-pair Cable • Cables length: 0.3 m, 0.5 m, 1 m, 2 m, 3 m, 5 m, 10 m, 15 m Rugged type Cable with Connectors on Both Ends (M12/RJ45) XS5W-T421-MC-...

  • マニュアル

    ...Int IOIDENT$ IsFile ItemCount ItemIdent$ ItemInfo ItemTitle$ JGINDEX& JUDGE& JUDGE_ERROR JUDGE_IMAGEERROR JUDGE_MEMORYERROR JUDGE_MODELERROR JUDGE_NC JUDGE_NG JUDGE_OK JUDGELOWER# JUDGEMACROFLAG& JudgeOut J JUDGEUPPER# ...

  • マニュアル

    ...4 ghi 3 4 d→e→f→D→E→F g→h→i→G→H→I 9 Section 1-3 Control Keys 1-3-4 Key 5 jkl 5 Number mode Alphabet and symbol mode j→k→l→J→K→L 6 mno 7 pqrs 6 7 m→n→o→M→N→O p→q→r→s→P→Q→R→S 8 tuv 9 wxyz 8 9 t→u→v→T→U→V w→x→y→z→W→X→Y→Z 0 .,: * +/- 0 * .→,→:→;→"→'→`→_ +→/→-→=→^→~ # (< # (→)→[→]→<→>→{→} Function Keys Key Function ESC F1 Escape Not used. F2 NUM/CHARA Not used. Changes the input ...

  • マニュアル

    ...トを表示する際は下表となります A b c d E F G h I J H P L LD ON ABL E K L m n o P q r S t (1)CF パワー LED メモリカード(コンパクトフラッシュ)への電源供給状態を表します。 電源 ON 時に点灯、OFF 時に消灯します。 ZER O EN (2)CF アクセ...

  • マニュアル

    ...す。 点灯・・・測定範囲内消灯・・・測定範囲外 ○ゼロリセット表示灯【ZERO(緑)】 ゼロリセット機能が有効の場合に点灯します。 K L m n o P q r S t 【解除方法】 U v w X Y ゼロリセットが実行されている状態で、ENTキーとRIGHTキーを同時に約 3秒押します。...

  • ...リレー逆相欠相温度モータ・リレー ・電圧不平衡検出・温度異常検出・モータ内部温度監視 形K2CM 反限時動作 形SE-K/-KP 形SE-KQ モータ・リレー 高さ: 96mm 形SE-K/-KP モータ保護用 モータ保護用 形SAO-Q 形SAO-RS 高さ: 96mm 形SAO-QS 形SAO-SS 反相 逆転防止リレー...

  • ...,700∼ 12,200 *1. 2017年9月現在、当社調べ。 *2. センサ取付け時の距離調整にかかる時間。 当社調べ。 *3.・対象油種:JIS K 2241:2000規定の切削油剤耐油実力値2年とは、商品設計、および、耐油性能評価結果の中央値 (=Typ値) を表したものです。 出荷する製品は、2...