全 5560 件が検索されました。(3721 - 3740件を表示)
- マニュアル
...1001 9 FE1(HT) EM ) 9 I Y i y 1010 10 FE2(LF) SUB * : J Z j z 1011 11 FE3(VT) ESC + ; K [ k { 1100 12 FE4(FF) IS4(FS) , < L \ l | 1101 13 FE5(CR) IS3(GS) − = M ] m 1110 14 S0 IS2(RS) . > N ^ n } - 1111 15 S1 IS1(US) / ? O _ o 126 TC7(DLE) (SP) DEL Revision History A manual revision code appears as a suffix to the catalog number on the front cover of the manual. Cat. No. Z174-E1-02A Revision code The following table outlines the changes made to the manual during ...
- マニュアル
... be equal to 0.01 m. ● Notation used for settings Letters, numbers and abbreviations in settings that appear in the E5AR/ER display are as follows. a b c d e f g h i j k l m A B C D E F G H I J K L M n o p q r s t u v w x y z N O P Q R S T U V W X Y Z 0 1 2 3 4 5 6 7 8 9 -1 0 1 2 3 4 5 6 7 8 9 -...
- マニュアル
... with DC power supplies. 2. With V1 CPU Units, both PNP and NPN sensors can be connected to DC input circuits. Connecting PNP Sensors PNP output + (power supply) 750 Ω 2,200 pF I0 to I3 (I0 to I9) 4.1 ...
- マニュアル
... to 100 Ω or less Input Specifications Input ID-RESET Input type Input current Two-wire Sensor 6.0 mA typical Line driver inputs 13 mA typical Input voltage 24 V DC + 10%, −15% Input impedance 3.6 kΩ RS-422A line driver AM26LS31 standards (See note.) --- Number of circuits ON voltage/current 1 circuit 17.4 V DC min./3 mA min. --- OFF voltage/current Delay 5 V DC max/1 mA max. 200 ms max. 24 V LD+ 3.6 Ω 100 Ω 750 Ω 1,000pF 0V/LD− Note 100 Ω Internal circuits Circuit configuration --- (1) The power supply voltage on ...
- マニュアル
... mA) Negative logic (H = 0, L = 1) Accuracy Within ± 1° Rotation direction Clockwise (viewed from the shaft) for output code increment Rise and fall times of output 1.0 µs max. (control output voltage: 16 V; load resistance: 1 ...
- マニュアル
...No. of check block bytes 4 2 1 * CR 2 Specifies the method for communicating with a Tag. Refer to Communications Designations for details. p.43 SECTION 4 Process designation Specifies the check process. “...
- マニュアル
...ᣣᦐᧁޓᣣޓඦ೨㧥ᤨ㧟㧤ಽ Section 4 INDEX Gang mounting Panel Installation distance 27 25 39 Key Operations 47 Continuous measurement Output time Synchronous measurement Operating modes OUTPUT OUTPUT TIME K...
- マニュアル
... LCD screen.The details displayed on these differ according to the operating mode. Display LCD screen Alphabet characters that appear on the digital displays A B C D E F G H I J K L M N O P Q R S T U V W X Y Z Section 3 SETUP Control keys ● FUN Mode The LCD screen displays the setup menus. The No. at the top of each menu corresponds to a function key. “← →" displayed at the top right of the LCD screen indicates that the setup menu is made p of two or more pages....
- マニュアル
...string position to the right. Use the Left Button to move the character string to the left. ( ) Table of Display Characters ! " # $ % & ' ( ) * + , - . / 0 1 2 3 4 5 6 7 8 9 : ; < = > ? @ A B C D E F G H I J ...
- マニュアル
...9 I Y i y 1 0 1 0 A LF SUB * : J Z j z 1 0 1 1 B VT ESC + ; K [ k { 1 1 0 0 C FF FS , < L \ l | 1 1 0 1 D CR GS - = M ] m } 1 1 1 0 E SO RS . > N ^ n ~ 1 1 1 1 F SI US / ? O _ o DEL R INDEX INDEX A O addresses ................................................................... 14 analog comparator .................................................... 18 ASCII list .................................................................. 42 operation command ...................................................32 B BCC .......................................................................... 10 BCC calculation example ......................................... 11 bit position .......................................................... 16, 21 C calendar timer ........................................................... 25 changing from RUN Mode to STOP Mode ...................
- マニュアル
...Command name COMMAND PROCESSING TERMINATE Function Page Forcedly ends communications with the Data Carrier. p.94 •Host Commands These commands are used to test communications between the Hand-held Reader Writer and host Section 3l Command and Response Format MDC/...
- マニュアル
...A CRC (Cyclic Redundancy Check) code calculation, write, and comparison are made using the check block units specified by the user. The CRC code is calculated from the generated polynomial expression x16 + x12 + x5 + 1. Command @ × × M D C/...
- マニュアル
... determined according to the communication condition settings, is attached at Seciton 4 CONNECTION TO EXTERNAL DEVICE the end of a command. ● Response Format The non-procedural command response format is shown as below: •In the event that a command is correctly executed: O ...
- マニュアル
...: 50% 5: 62.5% 6: 75% 7: 87.5% 0: OFF 1: ON 0: Timing A 1: Timing B 1 to 5 0: OFF 1: Average 2: Peak 3: Bottom 4: Thickness 5: Gap 6: K+mX;+nY ZS Series CompoWay/F Communication Command Reference When the measurement object is changed, the settings are initialized according to the selected object. TASK1 settings. The settings in Unit Number 28h are valid only for multi-task mode. Section 3 Setting Value Obtaining and Changing Command Parameter Parameter X 28h 4h Parameter Y 5h Parameter ...
- マニュアル
... is output in the following format: Z S - L D C 2 CR Version •Other commands Either OK or ER is returned according to the result of the command. The command was executed properly: O K CR The command was not executed properly or the setting was NG: E R CR The delimiter can be selected from the following three types. CR/LF/CR+LF ZS-Series Non-procedural Communication Command Reference 3 zs_normal_E.fm 4 ページ 2006年1月12日 木曜日 午後6時0分 List of Non-...
- マニュアル
... A. The minimum current when the Sensor’s OFF residual voltage is 25 V max. is 0.005 A. R1 (Ω) ≤ 25 V AC/0.0017 A = 14,706 Ω R2 (Ω) ≤ 85 V AC /0.005 A = 17,000 Ω The bleeder resistor must thus be 14 kΩ. The Sensor output current in this case would be 100 VAC/14 ...
- マニュアル
..., OUT2, OUT3, OUT4) Specifications Item Specifications Output method Open collector output (Sync type: NPN) Input voltage 10.2 to 26.4 VDC (including ripple) Output maximum level 26.4 VDC (including ripple) Input impedance 2.35 ...
- マニュアル
... number of bytes 0001 excluding the last two bytes. The last two bytes are the check code area. When check code write is specified (transaction code: Area start address Check code calculation area (Number of check block bytes - 2) ...
- マニュアル
...Output cable OUTPUT TIME 67 82 79 85 71 63 76 32 36 34 P Part Names Amplifier Unit Sensor Head Partial function Pattern Inspection Position check Power Supply K Key Operations MENU/ADJ mode RUN Mode 60 60 57 LANGUAGE LIGHT TEACH Lighting Unit (Option) Lock Function 103 66 134 107 L 109 110 109 27 61 113 39 110 24 25 95 63 76 21 R ROTATION RS-232C Cable external dimensions Cable wiring Communication Setting RUN Mode M 88 99 S SEARCH AREA 65, 91 Sensor Head Connecting the Sensor Head 51 Focus adjustment 49 Installing the ...
- マニュアル
... has failed G ?N Error Code Reading is repeated until it is successful. SO Function... Stops the level trigger. This command is effective only when a level trigger is being executed. 64 Input S O Output O ...