全 5560 件が検索されました。(3621 - 3640件を表示)

  • マニュアル

    ... mA, Resolution of 1/6,000 A Temperature Sensor Unit can be connected to provide up to 6 inputs for temperature input from sensors, such as thermocouples or platinum resistance thermometers. Temperature Sensor Unit Functions Thermocouple input (CPM1A-TS001/002; 2/4 input points): ...

  • マニュアル

    ...-V1 Expansion Memory Unit Uploads the ladder program and DM 6144 to DM 6655 from the PC to the EEPROM and downloads the ladder program and DM 6144 to DM 6655 from the EEPROM to the PC. EEROM-JD EEPROM 256 ...

  • マニュアル

    ...1.SelecttheStartpush-buttonfromthetaskbarandchooseSettings._ 2.SelecttheWindowsControlPanel. 3.SelecttheAddlRemoveProgramssetting. 4.TheAdd!RemoveProgramsPropertiesdlalogisdisplayed. tns憾∼u幽stal}・wt噛鴎9杖碗Sta醐コD敏1 1丁口無t威迫酬・口口9槌;pff{加音恥pPP・di§...

  • マニュアル

    ... to the same Rack does not exceed the maximum current provided for the Rack. Limitations Due to Unit Current Consumption Rack type Number of Analog I/O Units that can be mounted on the same Rack Rack model C200HX/HG/HE CPU R ...

  • マニュアル

    ...information. Note Indicates information of particular interest for efficient and convenient operation of the product. 1, 2, 3... 1. Indicates lists of one sort or another, such as procedures, checklists, etc. Trademarks and Copyrights COMBICON is a registered trademark of Phoenix Contact ...

  • マニュアル

    ...information. Note Indicates information of particular interest for efficient and convenient operation of the product. 1, 2, 3... 1. Indicates lists of one sort or another, such as procedures, checklists, etc. Trademarks and Copyrights COMBICON is a registered trademark of Phoenix Contact ...

  • マニュアル

    .... TheSelectProgramManagerGroupdialogappears. こぐ り 、ミc=n・``,4;`-II 聡肇饗讐三二ご/治…緬岨・郷「抗=≡ご 三 1'∵' lii蹴ご瑠/ 《 、 電曲1涌uば ぷ錨'脳" 、 、 口a繧k 詣雌必1奮酎Upノ ベシ シ 、 _ 一一 Figure1・3SelectProgramManagerGroupDialog 6 ---------------------[End of Page 3843]--------------------- TopiclinstallingandStartingCPT } 6.SelectwheretheCPTiconsshouldbeinstalledbyclickingonCreatenew grouporUseexistinggroup・ 7.ClickonContinue. TheSYSMAC-CPTUserInformationdialogappears. ごび戊㌣ 一 '二│一・一一 ㍉ 曙│ / 'r 鐵羅糟灘整怠;;盛 「1 「・ー │ ∵ ■ . ノ Figure1・4UserInformationDialog 8.Typeyournameandyourorganization'snameinthefieldsprovided・ 9.ClickontheContinuebutton....

  • マニュアル

    ...,however,youmustsaveallchangestodisk. ■Tosaveanewproject: 1.ClickontheFilemenuandselectSaveAsorclickontheSavetoolbar button. TheSaveAsdialogappears. 28 ---------------------[End of Page 3971]--------------------- Chapter2WorkingwithProjectFiles ノ荊扉、 一四 ∵㌘∵ ∴∴ Figure2・4SaveAsDiabg 234 く」rO Selectadriveanddirectoryfortheprojectfile. TypeanamefortheprojectintheFileNamebox. ClickonOK. TheSummaryInformationdialogappears(seeFiguresonpage30). Typethedesiredsummaryinfbrmation. ClickonO〕...

  • マニュアル

    ... max. 19 Section Specifications Output Specifications Item 2-1 Specification Maximum switching capacity Minimum switching capacity Leakage current 30 mA at 4.75 to 26.4 VDC (NPN open collector) (16 mA: Terminals with 1.6-...

  • マニュアル

    ...CQM1H-PRO01-E LCD display Mode switch FUN SFT A ST OR H AA LD AC OUT N M 7 0 . −IR TR J *EM WR/LR K AR HR EM DM P CH *DM Q CONT # R 6 T DEL MON 2 3 Y TEXT ! CLR VRFY NOT B C CHG W INS TN AND G H AC OUT N M 7 E F 4 6 0 6 D 2 DR IR . −IR TR J *EM WR/LR ...

  • マニュアル

    ... increasing the number of retries for applications using UDP. b) Insert a noise filter right next to the Unit’s power supply terminals. 24 VDC 24-VDC power supply Noise filter As close as possible Recommended filter: MAS-1206-33 by Nemic-Rambda ...

  • マニュアル

    ... input terminal and G) OFF voltage OFF current Input current 88 Specification Model Internal I/O common Input impedance 6.0 mA max./point at 24 V DC 3.0 mA min./point at 17 V DC 4.4 kΩ ON delay time OFF delay time 1.5 ms max. 1.5 ms max. Section 4-5 Transistor Remote I/O Terminals with Connectors Item Max. simultaneously ON input points 32 points (See note.) Specification Number of circuits 32 points with one common Note All 32 inputs can be ON simultaneously if the Remote I/O Terminal is mounted...

  • マニュアル

    ... the information contained in this publication. Trademarks • Microsoft, and Windows are either registered trademarks or trademarks of Microsoft Corporation in the United States and other countries. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • COMBICON is a registered trademark of Phoenix Contact ...

  • マニュアル

    ... in CPU Unit ↔ Host computer Devices Ethernet Unit FTP server function PC ↔ Nodes with socket service (such as Unix-based computers) Socket service function Controller Link PC ↔ Computer directly y connected d to the h network ...

  • マニュアル

    ... of the transmitted data is used to prevent more data from being transferred until the transmitted data is copied to another section of Data Memory for storage. The code is erased from the original block of data after it is copied. SEND S L ...

  • マニュアル

    ... a Transit Voltage Suppressor (TVS) diode between the 24-V and 0-V DC power supply wiring. The polarity of the TVS diode is bidirectional, i.e., it has no set polarity. Recommended TVS: 1.5KE33CA Manufacturer: Vishay Semiconductors (formerly General Semiconductors) ST Microelectronics ...

  • マニュアル

    ... be mounted to the CPM2C. There are 2 models of Temperature Sensor Unit: One for input from a thermocouple sensor and one for input from a platinum resistance thermometer sensor. There are 2 input points on each Temperature Sensor Unit. • Thermocouple inputs (and measurement ranges): ...

  • マニュアル

    ...CQM1HCPU11 Number of I/O points (see note) 512 256 Program capacity (words) CPU Unit external input points DM capacity (words) DC: 16 6K 6K 7.2 K 6K None 3.2 K 3K 15.2 K EM capacity (words) Built-in serial communications ports Peripheral port RS-232C port With With Inner Boards Communications Units Supported Supported Not supported Not supported Without 9 Section 1-2 System Configuration Note Number of I/O points = Number of input points (≤ 256) + Number of output points (≤ 256). Maximum Number of Units CPU Block Only CPU Unit Maximum number of Units connectable CQM1H-...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 139 C E5@K Digital Controller Read Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 155 D E5@...

  • マニュアル

    ..., CJ1W-PDC15 and CJ1W-PH41U Analog I/O Units. • Standard accuracy: ±5% The following conditions were used in the immunity test of the CS1W-PTS51/ PTS52/PTS55/PTS56, PDC55 and CJ1W-PTS51/PTS52. CS1W-PTS51 R or S thermocouple CS1W-PTS55 CJ1W-PTS51 ...