全 5560 件が検索されました。(3601 - 3620件を表示)
- マニュアル
... Device is connected when the C200HS power is already on, the mode status prior to connecting the Peripheral Device will be retained. PC Setup (DM 6600) status Mode according g to status of P Programming i Console C l keys ...
- マニュアル
... each Master and Expansion Master Unit number are fixed. Word n n+1 Input m m+1 Expansion Mas- Input ter, Unit 1 (Output) j j+1 Expansion Mas- Input ter, Unit 2 (Output) k k+1 Note 4-point Slave Address Bit 8-point Slave Address Bit #0 #1 00 to 03 04 to 07 #0 00 to 07 #2 #3 08 to 11 12 to 15 #2 08 to 15 #4 #5 00 to 03 04 to 07 #4 00 to 07 #6 #7 08 to 11 12 to 15 #6 08 to 15 #8 #9 00 ...
- マニュアル
... inputs to models that run on DC power. Doing so can cause counters and shift registers to be reset and bits programmed with KEEP(12) to reverse status during power interruptions. Input Specifications Specifications 24 VDC +10%/–15% Input impedance 3.9 ...
- マニュアル
...◎nductor 一一一 BX-G 一一一 G旬eraトpurp◎se,standardclass Copper C◎pper B R ●工■ RX-G,SX・G ●●一 AlbywRhcoppgromickglasmak)r◎◎nstRuθnt S ●●一 RX・H,SX・H ●●■ Heat-rgsistant,standardclass K CA KX-G WCA・G Gθ随raトpurpos9,standaζdclass Albywithnickθlorchromeasmajorconstituent Alloyw口hnickθlasmalorcons慌uent KX・GS WCA唱S KX・H WCA-H Heat-resistant,standardclass KX・HS WCA-HS Heat・resistant,precisionclass WX-G WCA{i General・purP◎se,standardclass lron A‖oywロhcoppgrornickθlasmajorcons世U白nt WX・H WCA・H Heat・resistant,...
- マニュアル
...N T E T CV–series N PC E S T N CV–series N T PC PC SYSMAC NET network IBM PC/AT or compatible SLK-NSB S S L N K T PC S N T PC SYSMAC LINK network S L K 2 PC S L K PC S L K PC ETN: SNT: SLK: SLK-NSB: Ethernet Unit SYSMAC NET Link Unit SYSMAC LINK Unit SYSMAC LINK Support Board Ethernet Unit Features 1-2 Section 1-2 Ethernet Unit Features A CV500-ETN01 Ethernet Unit provides the following features to the PC to which it is ...
- マニュアル
...-9P DE-Cl-J6 JAE NoteThreeXM2A-0901ConnectorsandthreeXM2S-0911Housingsareprovidedwiththe3G2A9-ALOO1-E LinkAdapter. 65 ---------------------[End of Page 1500]--------------------: L加鳶AdOpter A endixD 3G2A9-ALOO4図E(・PE) Dimensl◎ns § ‥、謡」 L ▼ OI プ...
- マニュアル
...醒◎Board 国 [=コロ〔=コロ____ C=コロ【=コロ tnPUtLED (orange) ㊥ 2・2.1LEDlndicators The32・POintS/OBoardindicatorsaredescribedinthefOllowjngtabie hdicabr Fundion OUTPUT AnoutputLEDislitwhen龍soo惰spondingoutput{OUTOOtoOUT15)isON. INPUT AninputLεDislitwhenitscorresp◎ndinginput{INOOtoIN15)isON. 懸 ....
- マニュアル
... inputs. System Configuration and Installation Section 2-2 If the leakage current exceeds 1.3 mA, insert a bleeder resistor in the circuit to reduce the input impedance, as shown in the following diagram. Input power supply R = 7.2/(2.4I–3) ...
- マニュアル
...A/Bphasedifference90。 ±45。 (%±拓丁) Outputrise/falltime 1.0μsmax.(Controloutputvoltage5V,10adresis-tancefKΩ,cordl旬gth50cm) Clockwise(CW)Rotation PhaseAisadvanced万±殆TphaseaheadofphaseB. ON PhaseA OFF ON PhaseB OFF /、 →CWdirection T 、/(360。 ) ...
- マニュアル
...・日c. →口 TeachingBox MCUnit CPU Usedtoset dataorfor G-language P「ogrammlng・・EditingGlanguageprograms ・Monitoringstatus ・Filecontrol ・Etc. SYSMAC C∨-seriesPC 口口 [1 Use「must ㌫ぽthese PowerSupplyUnit Periheralbus HostLi「)...
- マニュアル
...SECTIONl ComponentsandSwitchSettings.。 。 。 。 .。 .。 。 。 .。 e.e。 ..。 1-1 1-2 1-3 14 1-5 Components Indicators. SettingtheUnitNumber SettingtheDIPSwirch InstallingtheMCUnit ●●●●◆● 2-11!OConn㏄tor 2-2DRVCo皿㏄...
- マニュアル
...+Voltage input Input point 1 – Input Shield +Voltage input – Input Input point 2 Shield Shielded twisted-pair cable 2. Connect resistors from the shield to the positive and negative terminals. Input device +V R: 15 ...
- マニュアル
...PHC R D C SA R C: 0.1 µF min. R: Limiting resistor SA: Varistor D: Back-electromotive force protection diode PHS: Photo coupler V: DC power supply Recommended circuit example: R1: 2.7 kΩ; 1/2 W R2: 390 Ω; 1/4 W C: 50 V; 0.1 µF min. (However, these are only examples and are not guaranteed values. Construct the circuit in accordance with the characteristics of the input device to be connected.) Note 1. Mounting and PCB Cleaning: • If a soldering iron is used to solder the circuit, make sure that the circuit is soldered within ...
- マニュアル
... Sensor Unit models and available temperature sensors. Only one kind of temperature sensor can be connected to the C200H-TS001 or C200H-TS002. Each Temperature Sensor Unit connects to a maximum of four temperature sensor inputs. Model Connectable temperature sensor C200H-TS001 ...
- マニュアル
...xii xiii xiii 1 2 14 16 19 23 24 34 38 55 Appendices: System Protocols A B C D E F G H I J K L E5K Digital Controller Read Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . E5K Digital Controller Write Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . E5ZE Temperature Controller Read Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . E5ZE Temperature Controller Write Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . E5J Temperature Controller Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . ES100 Digital Controller Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K3T Intelligent Signal Processor Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . V500/V520 Bar Code Reader Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3Z4L Laser Micrometer Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Visual Inspection System Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . V600/V620 ID Controller Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Hayes Modem AT Command Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Index . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 59 77 93 115 135 149 191 213 225 257 275 311...
- マニュアル
...External device Details LPRT When not outputting Chinesederived characters (Kanji) No conversion from Shift JIS code to JIS code. NKPRT When outputting Chinese-derived Shift JIS code is converted to JIS code and characters, the printer control code KI (Kanji In): [ESC]...
- マニュアル
... rate for all nodes on the same network. • Be sure to set routing tables for CVM1 and CV-series PLCs. When a CVM1 or CV-series PLC is connected to the network, set routing tables at all the nodes. C C L P ...
- マニュアル
... current is 20 mA) Clockwise (CW) Rotation Max. response frequency 30 KHz Output phase difference A/B phase difference 90°±45° (1⁄4±1⁄8T) Output rise/fall time 1.0 µs max. (Control output voltage 5 V, load resistance 1 ...
- マニュアル
... axes that are to be edited. It is assumed here that the MCSS has already been installed. 8-8-1 Selection of MC Model 1, 2, 3... 1. Turn on the power supply to the computer, and start up the MCSS. 2. Select “...
- マニュアル
...4.3 mA ON voltage 17.4 V min. OFF voltage 3.0 V max. ON response time 1 ms max. OFF response time 2.5 ms max. Circuit Configuration +24 V 24 VDC 680 Ω 5 6 kΩ 5.6 Photocoupler The circuit in the table below is used to interface outputs RUN (X and Y) and ALMRS (X and Y). Item Specification Max. switching capacity 50 mA/24 VDC Circuit Configuration +24 V Leakage current 0.1 mA max. Output Residual voltage 1.0 V max. External supply voltage 24 VDC ± 10% Photocoupler The circuit in the table below ...