全 5560 件が検索されました。(3581 - 3600件を表示)

  • マニュアル

    ... the power supply can be connected to the common (COM) terminals, enabling connection of both PNP (negative common) and NPN (positive common) inputs. Input voltage 24 VDC +10%/ –15% Input current 7 mA Typ. (24 VDC) Circuit configuration IN 3.3 ...

  • マニュアル

    ...CPUBusUnitSetuρ UsedtosetparametersforSYSMACNEτSYSMACUNK,andSYSMACBUS/2・・communlcatlons. 105 NetworkSupρortTables UsedtototransferdatalinktablesandroutingtablesbetweenLinkUnits,thePC,andtheCVSSandtocomparethesetables.Alsousedtostartandstartdatalinks. 113 NetworkDiagnosis Usedtoruntestsbetweennodes,toreadnodestatus,andtoreaderrorbgsfromUnitsfortheSYSMACNETandSYSMACUNKSystems.AlsousedforSYSMACLINKSystemstorunbroadcasttestsandsetnetworkparametgrs. SYSMACBUS/2 UsedtomanipulateSYSMACBUS/2RemoteI!OMasterUnits. 141 MemoryCards UsedtodisplayfileslistsfromMemoryCardsinthePCandtomanipulatethesef‖es.WritingisnotpossibleforEEPROMandεPROMcards. 152 ReadError Usedtoreadthecurrenterroranderrorlogs.AlsousedtoforcereleaseoftheaccessrighttoaPC. 148 Cl㏄...

  • マニュアル

    ...MIN㈹ 166 FINDMIMMUM MLB㈹ 082 BINARYMUじ『IPLY MLBL㈹ 086 DOU8LEBINARYMULTIPLY MLPX㈹ 110 4・TO・16DECODER MOV㈹ 030 MOVE MOVB㈹ 042 MOVEBIT MOVD㈹ 043 ,MOVEDIGIT MOVL㈹ 032 DOUBLEMOVE MOVQ 037 MOVEQU℃...

  • マニュアル

    ...,no responsibilityisassumedforclerical,typographical,orproofreadingerrors,oromissions. 3 ---------------------[End of Page 9319]--------------------- ---------------------[End of Page 9320]--------------------- ---------------------[End of Page 9321]--------------------- ` iJ] 」 メ ] 目㌔ : 、 ↓ { / ---------------------[End of Page 9322]--------------------- TheCVSeries Ge師ngStarted Guideb◎◎...

  • マニュアル

    ... bit in the CIO Area or a Completion Flag in the Timer, or Counter Area. Bits/flags forced ON with FORCED SET will remain ON until the FORCED SET/RESET CANCEL command is executed. Command Format @ x 101 x 100 Unit no. ...

  • マニュアル

    ... used to display status information, thus not allowing them to be used for user data. Example This example shows reading the contents of 10 words from DM 12001 to DM 12009 in the CPU Unit to the BASIC Unit and storing in the variables H, I, J, ...

  • マニュアル

    ...DELETE D肌ETE[sraπ一〃ηθ一ηo,]【一【eηd-〃ηe−ηo.】] Deletesprogramlines. 42 EDIT EDIT["ne−ηα1 Editsonelineofprogram, 44 FILES/LF工LES FILES{drルθ一ησ1 Displaysnamesandsizeolfilesindrive. 50 LFILES[drルθ一ηO,】 Printsnamesandsizesoffilesindrive, ...

  • マニュアル

    ..., example, error codes, input range, of rules, Error Flag, output, inputs data format, setting the number, error indications, error messages, error processing, examples, application, installation acceptable locations, PC mounting slots, precautions, 57 Index ...

  • マニュアル

    ... is calculated as follows: Number of bytes required by each item Number of items Memory Areas The following data can be read (refer to 7-6 Memory Area Designations for PC word/bit address designations): Memory area CIO,, TR,, CPU Bus Li ...

  • マニュアル

    ...・ほ m S n a ア T t n e m e g a n a M e F e m a N 9 m K a m ヒ O F 獣 .U 』 日 』 日拍 』 e D 』 日 e m a n e R 9 n .H口 n .n P e m a N m 旧 9 b D e d d a L セ・恰 L ヒ n O m e n M 舗 U M E O M D S n O .U a r e P O M D e m a N 鉗...

  • マニュアル

    ...4 6 E F DM 0013 4 7 4 8 G H DM 0014 4 9 4 A I J DM 0015 4 B 4 C K L DM 0016 4 D 4 E M N DM 0017 4 F 5 0 O P MSG ABCDEFGHIJKLMNOP 199 Section 5-23 Special Instructions 5-23-4 LONG MESSAGE – LMSG(47) Operand Data Areas S: First source word (ASCII) Ladder Symbols IR, AR, DM, HR, TC, LR LMSG(47) @LMSG(47) S S D D --- --- D: Destination # (000) ---: Not used. Limitations S through S+15 must be in the same data area ...

  • マニュアル

    ... individual current ratings for the voltage supplied by any single Unit, nor should you exceed the total maximum power output. 41 Section 4-3 Maximum Current and Power Supplied Current Supplied Name CPU Rack Expansion I/O Rack R ...

  • マニュアル

    ... keys, “CONT” stands for “Bit” and “CH” stands for “Word.” Also, the “SFT” Key is used to input the SHIFT instruction only. The “SHIFT” Key is used to toggle in and out of the shift input mode (see below). 8 7 ...

  • マニュアル

    ..., 15 operating procedures, 14 display functions BK, 16 CAM, 16 DATA, 16 MODE, 16 STEP, 16 E error codes, 30 errors causes and corrections, 46 clearing, 48 data setting console display, 48 indicators, 48 F–...

  • マニュアル

    ... type setting 8 7 9 01 2 3 6 5 4 C200H-TC00@ Setting 0 1 2 3 4 5 6 7 8 9 Sensor type R S K J T E B N L U The switch is factory-set to 2. The selected position is shown by the arrow. Turn the switch with a small flatblade screwdriver. Selected position 11 Section 2-2 Switch Settings C200H-TC10@ OFF ON Setting OFF ON Sensor type JPt Pt The switch is factory-set to OFF. See Appendix B Sensor Temperature Measurement Range for the measurable temperature range. Operation and ...

  • マニュアル

    ... on 24 VDC. If the leakage current exceeds 1.3 mA, insert a bleeder resistor in the circuit to reduce the input impedance, as shown in the following diagram. Input power supply 2-wire method sensor, etc. R = 7.2/(2.4I–3) ...

  • マニュアル

    ... via a Host Link System, however, is not counted as a network and thus PC (a) and host computer (d) can also communicate with each other. S N T S N T PC (3) S S L N K T (1) PC S L K PC (a) 2 S S L N K T PC PC (b) (2) S S L L ...

  • マニュアル

    ...DM 0014 4 4 7 9 4 4 8 A G I H J DM 0015 DM 0016 4 4 B D 4 4 C E K M L N DM 0017 4 F 5 0 O P 00000 0010 00001 00 MSG ABCDEFGHIJKLMNOP 5-26-3 I/O REFRESH – IORF(97) Ladder Symbol Operand Data Areas St: Starting word IORF(97) St E IR 000 to IR 115 E: End word IR 000 to IR 115 Note This instruction is not supported by SRM1 PCs. Limitations St must be less than or equal to E. Description To refresh I/...

  • マニュアル

    ... shorted within the Unit. Wire each input’s shield wire to any of these terminals. Section 2-1 Before Operation Input Wiring Diagram Voltage input C200H-AD002 1 MΩ V 0V 1 MΩ COM Shield 10 kΩ 0V Current input 1 MΩ V/I 250 Ω I 0V 1 MΩ COM Shield 10 ...

  • マニュアル

    ... Cassettes Two types of Memory Cassettes are available for storage of data such as the program. The PC can be set to transfer data from the Memory Cassette to UM automatically when the PC is turned on. Model Specifications C200HS-ME16K 16-...