全 7847 件が検索されました。(3441 - 3460件を表示)

  • マニュアル

    ..._ 0R R _0R_ 0S S _0S_ 0T T _0T_ 0U U _0U_ 0V V _0V_ 104 V400-R2 series User’s Manual Section 4 Setting Method Menu sheet W Command 0W _0W_ 0X X _0X_ 0Y Y _0Y_ 0Z Z Section 4 Menu Sheet/Command List _0Z_ $A a _$A_ $B b _$B_ $C c _$C_ $D d _$D_ $E e _$E_ $F f _$F_ $G g _$G_ V400-R2 series User’s Manual 105 Section 4 Setting Method Menu sheet h Command $H _$H_ $I i _$I_ $J j _$J_ $K k Section 4 Menu Sheet/Command List _$...

  • マニュアル

    ...) ±60°(However, exclude from 10° upper side to 7° lower side) Tilt angle (γ) ±25° Reading of bar codes on curved surfaces (R) R20mm (UPC 12 digit) Light source Red laser diode (Wave length: 650 nm) Light output 1.0m ...

  • マニュアル

    ...text string 2: No judgement (not measured) 0: Judgement is OK 1: Judgement is NG 13: Teaching not performed error 14: Figure not registered error 15: Out of range error JG Judgement W Edge width 0 to 99999.9999 Edge width Ref. edge width (reference edge width) 0 to 99999.9999 This is the reference edge width from when the model was registered. SW DF D. edge width 0 to 99999.9999 (difference in edge width) This is the judgment result. This is the difference between the reference edge width and ...

  • マニュアル

    ...First, define a BOOL array data type to access the control signals and status signals. Here, a data type called “U_EIPFlag” is defined. Name of data type: U_EIPFlag Type of derivative data type: Union Name of data type U_EIPFlag F ...

  • マニュアル

    .............3-9 Troubleshooting............................................................... 10-1 Type.................................................................................2-15 U Update Standard Position Tool........................................ 8-17 User Data Setting Tool.......................................................8-7 Using the File Save Tool....................................................8-5 V Variable Assignment List................................................. 8-21 Version.............................................................................2-15 ...

  • マニュアル

    ...(NEQ) TC8(NAK) % 5 E U e u 0110 6 TC6(ACK) TC9(SYN) & 6 F V f v 0111 7 BEL TC10(ETB) ' 7 G W g w 1000 5 FE0(BS) CAN ( 8 H X h x 1001 9 FE1(HT) EM ) 9 I Y i y 1010 10 FE2(LF) SUB * : J Z j z 1011 11 FE3(VT) ESC + ; K [ k { 1100 12 FE4(FF) IS4(FS) , < L \ l | 1101 13 FE5(CR) IS3(GS) - = M ] m } 1110 14 S0 IS2(RS) . > N ^ n − 1111 15 S1 IS1(US) / ? O _ o DEL CIDRW System User’...

  • マニュアル

    ... Window The Status Window displays the model number, firmware version, MAC address, and other information on the Amplifier Unit so that you can check it. Click the Refresh Button at the top of the window to update the displayed information (latest communication, communication history, and H/...

  • マニュアル

    ... a power supply with an overcurrent detector, because this sensor uses DC-DC converter for its power supply circuit and inrush current may activate the protective circuit for a power supply with an overcurrent detector. Recommended power supply: S8VS-06024 (Omron, 24 VDC 2.5 A 60 ...

  • マニュアル

    ... the variables. Refer to the Sysmac Studio Version 1 Operation Manual (Cat. No. W504) for Sysmac Studio operating procedures. 1 (1) Defining the Data Types of the Variables Define data types for variables that match the structures of the communications areas. ...

  • マニュアル

    ... ver2.00, or later ◼ Acquisition of Sensor Controller name Format (Windows) Format (MacOS) int GetSensorName(out string sensorName) func GetSensorName(sensorName: inout String) -> Int32 sensorName (out) Parameters Name of the displacement sensor (up to 32bytes) “ Z ...

  • マニュアル

    ... vision and installation distance Ambient temperature range Operating: 0 to +40°C, Storage: -30 to +65°C (with no icing or condensation) Ambient humidity range Operating and Storage: 35 to 85% (with no condensation) Weight Approx. 52g Approx. 85g (...

  • マニュアル

    ... other devices in the circuit causes the diode to generate an abnormal amount of heat, which may lead to damage. This damage can occur easily when a surge current flows through the diode due to it being connected to an inductive load of 10 ...

  • マニュアル

    ... other devices in the circuit causes the diode to generate an abnormal amount of heat, which may lead to damage. This damage can occur easily when a surge current flows through the diode due to it being connected to an inductive load of 10 ...

  • マニュアル

    ... reactance current limiting elements types can be used. Recommended values for the SSR load current and protective resistance during single-phase motor forward/reverse operation Single-phase motor forward/reverse operation Motor Load power supply 100 V single-phase motor 25 ...

  • マニュアル

    ...Supply voltage Power consumption Ambient operating temperature Ambient operating humidity Ambient storage temperature Ambient storage humidity Insulation resistance Dielectric strength Vibration resistance V780-HMD68-ETN- V780-HMD68-ETN--S 250 × 250 × 70 mm (...

  • マニュアル

    ... in wiring? • The recommended power supply for V430 is the S8VS-24 (manufactured by OMRON) or S8VK-G-24 (manufactured by OMRON). Ground • Check wiring again before turning on the V430 reader. Other • Use only the cables (V430-...

  • マニュアル

    ... of maximum load current for test output of this safety I/O terminal. Residual voltage at test output ON of this safety I/O terminal. Leakage current at test output OFF of this safety I/O terminal. External dimensions of this safety I/O terminal, indicated as ...

  • マニュアル

    ... connector. • Do not attach or remove the connector when the Unit is ON. Otherwise, Unit failure may occur. • You cannot directly connect the antenna cable. Connect it with the amplifier (V680-HA63), extension cable (V700-A4), or a dedicated cable (V700-A40-...

  • マニュアル

    ...Supply voltage Power consumption Ambient operating temperature Ambient operating humidity Ambient storage temperature Ambient storage humidity Insulation resistance Dielectric strength Vibration resistance V780-HMD68-EIP- V780-HMD68-ETN--S 250 × 250 × 70 mm (...

  • マニュアル

    .../000000010> Clears the Trigger Input Count. None Gets the Match Count when the Matchcode function is used. The Response data output is V/ followed by a 9 digit value for the number of Matched strings. <...