全 7847 件が検索されました。(3481 - 3500件を表示)

  • マニュアル

    .../PoE, Serial, Digital IO, Ethernet. VHV5-F££££££££-£££-£ 3 456 7 1 2 No. Classification Code Meaning 1 Focus Distance (mm) 000 Autofocus ### Focus Distance in mm 2 Lens / Field of View W Wide M Medium N Narrow L Long Range 023M 2.3 Megapixel, Monochrome, Global Shutter 3 Sensor Type 050M 5 Megapixel, Monochrome, Global Shutter 4 Front Window S Clear Front Window Filter Type*1 D Light-Diffusing Front Window P Polarizing Window to Eliminate Glare H Half-Polarizing Window (Gives the user the option to use either polarized or standard lighting in the same unit) N None...

  • マニュアル

    ...0 Direct Parameter Page 1 --- RecordT R 16 bytes --- --- --- 1 0 Direct Parameter Page 2 --- RecordT --- 16 bytes --- --- --- 2 0 System-Command --- UIntT W 1 byte --- 0x01: Param Upload Start 0x02: Param Upload End 0x03: Param Download Start 0x04: Param Download End 0x05: Param Download Store 0x06: Param Download Break --- Selectable range Smart Verification flag Format Access Backup (¡ = target) Subindex Index 0 Item 0x7E: Locator Start*5 0x7F: Locator Stop*5 0x81: Application Reset*1 0x82: Restore Factory Settings*1 0x83: Back-to-box*1 3 0 Data Storage --- RecordT R/...

  • マニュアル

    ...an Ta mm o C 5 Additional Communication Unit Functions ZP-series Communication Unit External device Command • Measured value retrieval • Communications setting Response • OK, etc. 5-4-2 Command category Amplifier setting data R/...

  • マニュアル

    ... (TCP/IP Settings) ..............................................................................6-9 Network Settings Window (Port Setting) ...................................................................................6-10 Network Settings Window (IP Filtering Settings)....................................................................... 6-11 Network Settings Window (Permission Settings) ......................................................................6-12 Network Settings Window (Web Password Settings)................................................................6-13 Command Window ....................................................................................................................6-14 Command Window (CID R/...

  • マニュアル

    ...Read External Output Status External Input Control Initialize Threshold Teaching Rewrite/Read Settings Key Lock Communication Unit (Main Unit) Communications Setup Set Current Time Get Event Log Information 3-2-2 Command category Amplifier setting data R/...

  • マニュアル

    ... used for tag data links to communicate with the counterpart device. Defining a data type for signal access (Union) Data type to access control signals and status signals Data type name Data type EIP_Flg UNION F BOOL[16] ...

  • マニュアル

    ... of the Common Edition. A A-2-1 User settings GD Series IO-Link Master Unit (Multi-Network Compatible) User’s Manual EtherNet/IP Edition (Z514) A-9 Appendices RW UINT 1 Value Length in bytes Format R/W...

  • マニュアル

    ... frame, the Holding register number is specified in hexadecimal. Operation Of This Product Character string displayed on the display Category Data name 1st line 2nd line Button operation Holding register (decimal) 00000 ··· 00031 Bit R/...

  • マニュアル

    ...Device name Points Start End RX 64 00000 003F ←→ Designated device X 32 01000 01077 RY 64 00000 003F ←→ Designated device Y 32 01000 01077 RWr 32 00000 001F ←→ Designated device W 32 00100 0011F RWw 32 00000 001F ←→ Designated device ...

  • マニュアル

    ... for setting input terminals will be displayed. 2. In the window above, specify the type of device to be connected to each terminal. The following types can be specified. Type 2 Safety Relays with welding check (See note.) 2 Safety Relays ...

  • マニュアル

    ... setting input terminals will be displayed. 2. In the window above, specify the type of device to be connected to each terminal. The following types can be specified. Type 2 Safety Relays with welding check (See note 1.) 2 Safety Relays ...

  • マニュアル

    ... master, 88 USB communications status, 26 safety network controller, 2 user mode switch, 149, 186 safety output terminals, 32 safety precautions, xx safety signature, 90 safety slave, 88, 95 safety slave I/O, 116 selecting the I/O type, 96 ...

  • マニュアル

    ... requirements, 4 T Timing Chart - Execute 1 Pulse, 47 Timing Chart - OFF, 45 Timing Chart - ON, 45 67 Index Timing Chart - Reverse, 45 timing chart options, 51 Timing Chart Window, 43 tool bars, 11 V versions, 27 ...

  • マニュアル

    ...system combining configuration files, 131 system configuration, 5 system parameters, 128 T test output errors, 144 test output terminals, 15 failures, 140 status, 111 test pulses, 24 test source, 25 Threshold Maintenance Counter, 122 196 V ...

  • マニュアル

    ... filters, 32 test source, 29 J Jump tag, 79 U Unit Conduction Time, 144 unit configuration, 75 M Memory Cassette operations, 154 user testing, 152 user-defined function blocks, 79 199 Index V verification, 128 ...

  • マニュアル

    ... Developer. PLC parameter settings Set RS-232C communication adapter CH2 as given below in the PLC parameter by selecting[Project data list]-[Parameter]-[PLC parameter]-[PLC System(2)]. Parameter Protocol Data length Parity Stop bit Transmission Speed Header H/...

  • マニュアル

    ...SF_Equivalent ............................................................. 4-36 SF_ESPE .................................................................... 4-42 SF_F_TRIG ................................................................. 3-10 SF_GuardLocking ....................................................... 4-49 SF_GuardMonitoring ................................................... 4-55 U Up Trigger ....................................................................3-11 Up-counter .....................................................................3-5 Up-down Counter ...........................................................3-7 ...

  • マニュアル

    ...オムロン 携帯電話・PHS・IP電話などではご利用いただけませんので、 下記の電話番号へおかけください。 U v w X Y Z 電話 055-982-5015(通話料がかかります) ■営業時間:8:00∼21:00 ■営業日:365日 ●FAXやWebページでもお問い合わせいただけます。 FAX (3) エラ...

  • マニュアル

    ...ください。 項目 条件 OS Windows 10 (32 ビット版 /64 ビット版 ) Windows 7(32 ビット版 /64 ビット版 ) センサコントローラ形 ZG2-Wシリ−ズの詳細な機能および操作に関しては別冊(別売り)のユーザーズマニュアル(カタログ番号 SCHE-757)を用意していますので、 お取...

  • マニュアル

    ...、 レーザー製品のクラスに応じて使用者が行わなければならない安全予防対策が規定されています。 形 Z G 2 - W D S 2 2は本 規 格に定めるクラス2に分 類されます。 形 ZG2-WDS22はセンサ部側面に以下の警告ラベルを貼っています。 レー...