全 7847 件が検索されました。(2601 - 2620件を表示)

  • マニュアル

    ...k l m A B C D E F G H I J K L M n o p q r s t u V w x y z N O P Q R S T U V W X Y Z How This Manual is Organized Goal Learning about the appearance, features, functions, and model numbers Setting up the E5@C Related sections Section 1 Introduction Learning the basic procedures from turning ON the power supply to starting actual operation Learning the basic operating methods Learning advanced operating methods Section 3 Part Names and Basic Procedures Calibrating the E5@...

  • マニュアル

    ...0 to 3000 °F 17 B 100 to 1800 °C 300 to 3200 °F 18 0 to 3200 °F 19 0 to 2300 °F 20 W 0 to 2300 °C PLII 0 to 1300 °C Any value can be set for any model. JPt100 * When using the ES1B Infrared Temperature Sensor and an analog input, refer to the E5CC/E5EC Digital Temperature Controllers User's Manual (Cat. No. H174). ←If the setting of the Input Type parameter does not agree with the connected sensor, s.err (S.ERR: Input Error) will flash on the display as shown at the left ...

  • マニュアル

    ...k l m A B C D E F G H I J K L M n o p q r s t u V w x y z N O P Q R S T U V W X Y Z How This Manual is Organized Goal Learning about the appearance, features, functions, and model numbers Setting up the E5@C-T Related sections Section 1 Introduction Learning the basic procedures from turning ON the power supply to starting actual operation Learning the basic operating methods Learning advanced operating methods Section 3 Part Names and Basic Procedures Calibrating the ...

  • マニュアル

    ...: "1" Mark A > B: "0" Space Shield Specify both ends of the transmission path including the host as the end node (that is, connect terminators to both ends). Use a terminating resistance of at least 54 Ω. Terminator 120 Ω (1/2 ...

  • マニュアル

    ... resistance Shock resistance Dielectric strength Insulation resistance Enclosure rating Memory protection EJ1 internal bus communications conditions Weight 2-1-2 Specification End Unit power supply: 24 VDC End Unit power supply: 20.4 to 26.4 VDC 2 ...

  • マニュアル

    ...k l m A B C D E F G H I J K L M n o p q r s t u V w x y z N O P Q R S T U V W X Y Z How This Manual is Organized Goal Learning about the appearance, features, functions, and model numbers Setting up the E5@D Related sections Section 1 Introduction Learning the basic procedures from turning ON the power supply to starting actual operation Learning the basic operating methods Learning advanced operating methods Section 3 Part Names and Basic Procedures Calibrating the E5@...

  • マニュアル

    ...Abbreviation FG TX Abbreviation − Pin 14 + 13 B (+) A (−) RX SG 6.8 V A < B: "1" Mark A > B: "0" Space Shield Terminating resistance 120 Ω (1/2 W) E5CD/ED End node RS-485 Pin Specify both ends of the transmission path including the host as the end node (that is, connect terminating resistance to both ends). Use a terminating resistance of at least 54 Ω. 1-4 Shield Abbreviation 14 A (−) 13 B (+) Use 120 Ω (1/2 ...

  • マニュアル

    ... to 1300°C/-300 to 2300°F 16 R 0 to 1700°C/0 to 3000°F 17 S 0 to 1700°C/0 to 3000°F 18 B 0 to 1800°C/0 to 3200°F 19 C/W 0 to 2300°C/0 to 3200°F 20 PL II 0 to 1300°C/0 to 2300°F 21 Pt1000 - 200 to 850°C/-300 to 1500°F 22 Pt1000 - 199.9 to 500.0°C/-199.9 to 900.0°F 23 Pt1000 0.0 to 100.0°C/0.0 to 210.0°F NX-series ...

  • マニュアル

    ... from TR3 output mode parameter. (default: Error existence)  Configuration via Modbus TCP communications Address A024 hex Parameter name TR3 output mode Description 0: Error existence (default) Initial value 0000 hex Number of bytes 2 R/...

  • マニュアル

    ... 7-8 Feature Visualization on page 7-101. 1-1-6 Universal Input Supported The input sensor can be set to any of the followings: thermocouple, resistance thermometer, current, and voltage. Thermocouple input: K, J, T, E, L, U, N, R, S, B, C/...

  • マニュアル

    ...k l m A B C D E F G H I J K L M n o p q r s t u V w x y z N O P Q R S T U V W X Y Z How This Manual is Organized Goal Learning about the appearance, features, functions, and model numbers Setting up the E5D-H Related sections Section 1 Introduction Learning the basic procedures from turning ON the power supply to starting actual operation Learning the basic operating methods Learning advanced operating methods Section 3 Part Names and Basic Procedures Calibrating ...

  • マニュアル

    ...6.8 V A < B: "1" Mark A > B: "0" Space Shield Specify both ends of the transmission path including the host as the end node (that is, connect terminating resistance to both ends). Use a terminating resistance of at least 54 ...

  • マニュアル

    ... aufgeführten verwenden wollen, dann stellen Sie bitte sicher, dass Sie sich dabei in den Grenzen der Produktklasse und dessen Funktionen bewegen. Diese Sensoren sind nicht für Sicherheits-oder EndabschaltungsAufgaben geeignet. q Für Anwendungen in jeglicher Umgebung oder Zustand, der nicht im Handbuch beschrieben wird. ...

  • マニュアル

    ... rated supply voltage (90% to 110% at 12 VDC) Power reset Minimum : power-opening time 0.1 s Power consumption H3CR-A8 • 100 to 240 VAC/100 to 125 VDC(When at 240 VAC, 60 Hz) Relay ON: approx. 2.0 VA (1.6 ...

  • マニュアル

    ...(90% à 110% à 12 Vc.c.) RAZ de l'alimentation minimum : temps de coupure 0,1 s Consommation H3CR-A8 • 100 à 240 Vc.a./100 à 125 Vc.c.(À 240 Vc.a., 60 Hz) Relais ON : environ 2,0 VA (1,6 W) Relais OFF : environ 1,3 VA (1,1 ...

  • マニュアル

    ... applications such as those listed below, please be sure to maintain strict adherence to the limits of product ratings and functions. These controllers are not intended for use as safety and limiting devices. q For use at any condition or environment not described in the manual. ...

  • マニュアル

    ... range 85% to 110% of rated supply voltage Power reset Minimum : power-opening time 0.1 s Power consumption • 100 to 240 VAC/100 to 125 VDC(When at 240 VAC, 60 Hz) Relay ON and OFF: approx. 2.0 VA (0.9 ...

  • マニュアル

    ... voltage range 85% to 110% of rated supply voltage Power reset Minimum : power-opening time 0.1 s Power consumption • 100 to 240 VAC/100 to 125 VDC(When at 240 VAC, 60 Hz) Relay ON and OFF: approx. 2.0 VA (0.9 ...

  • マニュアル

    ...) Connections D Anschlußanordnung * 1:Voyant de sortie * 2:Voyant d'alimentation * 3:clignotant Brochage F G : Gate input Temporarily stops timing operation. Open terminal t when not used. S : Start input (Always connect) Short-circuit terminal y―...

  • マニュアル

    ... (90% bis 110% bei 12 VDC) Stromrücksetzzeit Minimum: Stromöffnungszeit 0,1 s Min. Impulsbreite: 0,05 s Leistungsaufnahme H3CR-A • 100 bis 240 VAC/100 bis 125 VDC (Bei 240 VAC, 60 Hz) Relais EIN: ca. 2,0 VA (1,6 ...