全 5560 件が検索されました。(2181 - 2200件を表示)

  • マニュアル

    ... 15 in C+9) will turn OFF. The proportional band (C+1), integral constant (C+2), and derivative constant (C+3) calculated by autotuning will be stored and PID control will be started with those PID constants. 16-1-3 Application Example System Configuration ...

  • マニュアル

    ... data can be indicated as odd or even, and if the number of 1s in the received data is not similarly odd or even, it is assumed that an error has occurred. Precaution • When multiple digits are specified in the number of digits to be converted (...

  • マニュアル

    ... Unit to time out the communications. The Master Board notifies the Slave Unit when a Slave Unit participates. Settable range: 0 to 65535 ms (Setting it to 0 will select the default.) Default: 50 ms (163 ms at the data rate of 93.75 ...

  • マニュアル

    ... μm (5) Cable Connection Direction (M12 Connector) 1: Straight 2: Right-angle (6) Cable Length A: 0.3 m B: 0.5 m C: 1 m D: 2 m E: 3 m G: 5 m J: 10 m K: 15 m (7) Connectors 0: M12 plug on one end 1: M12 socket on one end and M12 plug on the other end 2: M12 plugs on both ends C: M12 plug on one end and RJ45 plug on the other end D: RJ45 plugs on both ends E: M12 socket on one end and RJ45 plug on the other ...

  • マニュアル

    ... connecting terminals are as shown in the following diagram. 2-13 2 CJ-series Analog Input Units (CJ1W-AD041-V1/081-V1) 2-4-2 Internal Circuit The following diagrams show the internal circuit of the analog input section. z Input Circuit 15 ...

  • マニュアル

    ...-1 Introduction and Features 1-1-1 Introduction This Unit receives inputs directly from thermocouple or platinum resistance thermometers, performs PID control with two degrees of freedom, and outputs results through open collector outputs. This Unit has two types of inputs: thermocouples (R, S, ...

  • マニュアル

    ...D D II Counter Input Z * I I Counter Input Z * On On 50% 0V Off Off Z E Z J * M aximum a llowed f requency of Z-pulses is 1 k Hz Filter Selection 10 kHz 50 kHz 500 kHz A <3 <3 <3 B >50 >10 >2 C >100 >20 >4 D >23 >4.5 >1 * Maximum allowed frequency of Z-pulses is 1 ...

  • マニュアル

    ...0.110 ms outputs + 128 bit inputs, 128 bit outputs 0.146 ms 0.291 ms 4.674 ms Communications mode 8 1,024 word inputs, 1,024 0.013 ms + 0.018 ms + 0.035 ms + 0.567 ms + K (*1) K (*1) K (*1) word outputs + 256 bit inputs, ...

  • マニュアル

    ... parameters. Set Reset When status is read After busy status is released When status is read When status is read TRUE: Local Unit busy (Reception is disabled because the reception buffer is more than 4/5 (= 2 ...

  • マニュアル

    ...15 I 1 5 s I+1 4 3 s+1 I+2 1 2 s+2 : : s+3 OUT block 1 IN block 1 15 00 00 k 00 00 01 01 k+1 00 00 01 01 k+2 02 k+3 Not usable Not usable : 00 : k+4 Not usable 01 01 Not usable 01 02 k+5 l: First word in allocation size setup table s: First word in OUT block 1 ...

  • マニュアル

    ...Zero/span adjustment Integral value calculation External 24-VDC power supply 1-3 1 Overview and Features Name Model I/O type Isolatedtype Universal Input Unit CJ1WAD04U • Resistance thermometer: Pt100, Pt1000, JPt100 • Thermocouple: ...

  • マニュアル

    ... name Model numbers Manual name NJ-series CPU Unit NJ501-1500 (unit version 1.00) NJ-series CPU Unit Hardware User’s Manual (Cat. No. W500) NJ-series Power Supply Unit NJ-PA3001 EtherCAT Communications Cables XS5W-T421-CMD-...

  • マニュアル

    ... and System Configuration of NJ/NX-series Controllers and 1S-series AC Servo 1-2 1-2-1 System Configuration and Configuration Devices Devices Used in This Guide NX1P Machine Automation Controller NX1P2-1140DT EtherCAT Communications Cable XS5W-T421-MD-...

  • マニュアル

    ... wires. (H) Terminal block lever This lever is used to fix the terminal block on the NX Unit. (I) Unit specifications The specifications of the Unit are given. (J) Terminal block The terminal block is used to connect external devices. (...

  • マニュアル

    ... master that supports Free-Run Mode only. NX-PG0112 and NX-PG0122 The following figure shows the system configuration of NX-PG0112 and NX-PG0122. (C) (A) (B) (D) (F) (G) (E) (M) (H) (I) (J) (K) (L) Letter 8-4 Description (A) Support Software (Sysmac Studio) (B) Connection to the peripheral USB port or built-in EtherNet I/P port on an NJ/NX-series CPU Unit (C) EtherCAT master (NJ/NX-series CPU Unit) (D) EtherCAT communications cable (E) EtherCAT Coupler Unit (F) Pulse Output Unit (NX-PG0112 or NX-PG0122) (G) Digital Input Unit NX-series ...

  • マニュアル

    ...Errors and status of the DB Connection Service Data 1 Data 2 Data 3 Data 4 Relational Database DB Connection Service 1-2-2 DB Connection System DB Connection Instruction Field4 Data 4 Operation Logs (k...

  • マニュアル

    ... Controller and NJ301-□□□□ NJ101-□□□□ NY-series W564 Troubleshooting Manual AC Servomotors/Servo I576 Drives G5-series with Manual 8 I577 in an NY-series Industrial PC. information on individual errors are described. R88M-...

  • マニュアル

    ...EtherCAT CAT NETRUN NET RUN NET NETERR ERR LINK LINK/ACT /ACT PORT2 EtherNet/IP PORT3 EtherCAT (P) (O) Letter 3-2 (N) Name (M) (L) (I) (K) Function A DIP switch Used in Safe Mode or when backing up data. Normally, turn OFF all of the pins. B Push switch Unused. For future expansion, leave it unoperated. C Power supply connector Connects to the Power Supply Unit. D DIN Track mounting hooks These hooks are used to mount the Unit to a DIN Track. E Fan Unit Cools the CPU Unit internally. Refer to Fan Unit on page 3-...

  • マニュアル

    ...MS TS NS P1 P2 (A) (L) Port1 (I) F 012 9A 78 3456 DE BC F 012 DE BC Port2 9A 78 3456 (M) (L) (K) (F) (J) (E) Letter 4-2 Name Function (A) Marker attachment locations The locations where markers are attached. The markers made by OMRON are installed for the factory setting. Commercially available markers can also be installed. For details, refer to 6-1-8 Attaching Markers on page 6-18. (B) Unit specifications The specifications of the Unit are engraved in the side of the casing. (C) NX bus connector This connector is used ...

  • マニュアル

    ... Displaying the CIF Serial Line Monitor Tab Page The CIF Serial Line Monitor tab page is displayed. NX-series Communications Interface Units User’s Manual (W540) 8-7 8 Serial Line Monitor (A) (B) (C) (D) (E) (F) (G) (H) (I) (J) (...