全 5560 件が検索されました。(2241 - 2260件を表示)
- マニュアル
... Mode Settings SENSING FILTER OUTPUT HOLD 0RESET Default Value Option/Range Pages SEL CH - Input A to input I CALC CH OFF, CH (input A to input I), CALC p.3-15 (THICK, STEP, K+mX+nY, AVE, MAX-MIN) SMOOTH ON OFF, ON AVERAGE 1 1, 2, 4, 8, 16, 32, 64, 128, 256, 512, 1024, 2048, 4096 DIFF OFF OFF, ON - SCALING OFF OFF, ON (AUTO, MAN) - TYPE OFF OFF, PEAK, BOTTOM, P-P, AVERAGE, SAMPLE TRIGGER EXT EXT, SELF-UP, SELF-DN - DELAY OFF OFF, ON (T-DELAY, T-TIME) - TYPE REAL REAL, HOLD - OFFSET 0 -...
- マニュアル
... LCD screen.The details displayed on these differ according to the operating mode. Display LCD screen Alphabet characters that appear on the digital displays A B C D E F G H I J K L M N O P Q R S T U V W X Y Z Section 3 SETUP Control keys ● FUN Mode The LCD screen displays the setup menus. The No. at the top of each menu corresponds to a function key. “← →" displayed at the top right of the LCD screen indicates that the setup menu is made p of two or more pages....
- マニュアル
...1001 9 FE1(HT) EM ) 9 I Y i y 1010 10 FE2(LF) SUB * : J Z j z 1011 11 FE3(VT) ESC + ; K [ k { 1100 12 FE4(FF) IS4(FS) , < L \ l | 1101 13 FE5(CR) IS3(GS) - = M ] m } 1110 14 S0 IS2(RS) . > N ^ n ÅP 1111 15 S1 IS1(US) / ? O _ o DEL CIDRW System User’s Manual TC9(SYN) Undefined Undefined Undefined SECTION 6 Appendix Protective Construction IP- is governed by the test methods described below. Check in advance the seal characteristics under the actual environment and conditions of use. IP is the abbreviation ...
- マニュアル
...: 50% 5: 62.5% 6: 75% 7: 87.5% 0: OFF 1: ON 0: Timing A 1: Timing B 1 to 5 0: OFF 1: Average 2: Peak 3: Bottom 4: Thickness 5: Gap 6: K+mX;+nY ZS Series CompoWay/F Communication Command Reference When the measurement object is changed, the settings are initialized according to the selected object. TASK1 settings. The settings in Unit Number 28h are valid only for multi-task mode. Section 3 Setting Value Obtaining and Changing Command Parameter Parameter X 28h 4h Parameter Y 5h Parameter ...
- マニュアル
... is output in the following format: Z S - L D C 2 CR Version •Other commands Either OK or ER is returned according to the result of the command. The command was executed properly: O K CR The command was not executed properly or the setting was NG: E R CR The delimiter can be selected from the following three types. CR/LF/CR+LF ZS-Series Non-procedural Communication Command Reference 3 zs_normal_E.fm 4 ページ 2006年1月12日 木曜日 午後6時0分 List of Non-...
- マニュアル
...OBJECT ([THICK] is not displayed.) – SYNC (Same as Single-Task mode) – TASKSET NONE*, p.5-24 SETTING LASER MEASURE TASK2 to 4 18 ZS-HL User’s Manual AVERAGE, PEAK, BOTTOM, THICK, STEP, K+mX+nY FILTER (Same as Single-Task mode) – OUTPUT (Same as Single-Task mode) – TASKSET p.5-24 MEASURE NONE*, AVERAGE, PEAK, BOTTOM, THICK, STEP, ...
- マニュアル
...Do not execute the MDS command and MDL command for the same RF Tag. Doing so will prevent managing the service life. 104 RFID System User’s Manual SECTION 4 Functions RF Tag Memory Check The DATA CHECK command (MD C/...
- マニュアル
...+LF)] is selected < Command > When there is only one Controller connected Command data Delimiter When multiple Controllers are connected to each other # Channel No. Space Command data Delimiter < Response > When processing ends successfully Response data O ...
- マニュアル
...RF Tag Communications Range INHIBIT RUN BUSY 100 ms 100 ms NORMAL ERROR SECTION 5 ERR_SUB ID Timing Charts A B C D E F G H I J K A: The PLC turns ON INHIBIT and sends the execution command to the FL Remote ID. B: The FL Remote ID checks that INHIBIT is ON, determines the CMD (command), LEN (data length), and ADDR (start address), and then turns ON BUSY. C: The FL Remote ID starts communications with an RF Tag when one enters the Antenna's communications range. D: The FL Remote ID turns ON NORMAL ...
- マニュアル
... cause of the error. This parameter sets the error reset method. r s t 1 2 3 4 5 Switch to the Abnormal Current Tripping Threshold Setting (C-V). V A Yrs °C s 6 Press the k e y 1 2 3 4 5 6 V A Yrs °C s Key to display the send wait time setting. The setting can be changed by pressing the or Key. KEY: Errors can be reset using the S8AS Reset Key only. ALL: Errors can be reset using the S8AS Reset Key or by turning the power supply OFF. Change the ...
- マニュアル
...BUTTON WRITE BW A/H BA A/H BUTTON AUTO WRITE UW A/H ST A/H DATA FILL FL A/H SA A/H AUTO DATA FILL AF A/H C/K DATA CHECK MD ST C/K DATA CHECK MD OVERWRITE COUNT CONTROL MD ST S/L OVERWRITE COUNT CONTROL MD S CALCULATION WRITE --- --- --- CALCULATION WRITE CW A/S ID CODE READ ID ST H ID CODE READ ID H READ WITH ERROR CORRECTION QR ST A/H --- --- --- WRITE WITH ERROR CORRECTION QW ST A/H --- --- --- V600 and V680 Command Comparison Command code Command name Communications specification Section ...
- マニュアル
... with the RF Tag ID and turns ON BUSY. I: HS output will turn OFF when TRG turns OFF. J: When communications with RF Tag ends in an error, the ID Slave turns ON ERR (Error end) and 72_ERR (RF Tag missing error). ...
- マニュアル
..., or between arguments. • A delimiter, which is determined according to the communication condition settings, is attached at the end of a command. ● Response format The non-procedural command response format is as follows: • In the event that a command is successfully executed: O ...
- マニュアル
...Set any equation to perform addition/subtraction on the measurement result. The equation can be substituted with measurement results obtained by other tasks. Also, when using two Controllers in a gang-mount configuration, calculations can also be performed across channels. Allowable equation: ...
- マニュアル
... in this instance is referred to as a node No. 58 Serial Communication ZG2-DSU User’s Manual Communication Commands Command/Response Format
Command data Delimiter When processing ends successfully Response data O Delimiter ... - マニュアル
... set A is protected even when the monitoring zone is switched to zone set B before tEndZoneA. A simple measure is to modify separation distance (S) used when defining Zone set A such that it includes an additional component (Zextra) defined by the maximum approach speed (...
- マニュアル
...1001 9 FE1(HT) EM ) 9 I Y i y 1010 10 FE2(LF) SUB * : J Z j z 1011 11 FE3(VT) ESC + ; K [ k { 1100 12 FE4(FF) IS4(FS) , < L \ l | 1101 13 FE5(CR) IS3(GS) - = M ] m } 1110 14 S0 IS2(RS) . > N ^ n ÅP 1111 15 S1 IS1(US) / ? O _ o DEL CIDRW System User’s Manual Undefined Undefined Undefined SECTION 6 Appendix Protective Construction IP- is governed by the test methods described below. Check in advance the seal characteristics under the actual environment and conditions of use. IP is the abbreviation of International ...
- マニュアル
...1001 9 FE1(HT) EM ) 9 I Y i y 1010 10 FE2(LF) SUB * : J Z j z 1011 11 FE3(VT) ESC + ; K [ k { 1100 12 FE4(FF) IS4(FS) , < L \ l | 1101 13 FE5(CR) IS3(GS) - = M ] m } 1110 14 S0 IS2(RS) . > N ^ n ÅP 1111 15 S1 IS1(US) / ? O _ o DEL Undefined Undefined Undefined SECTION 7 ASCII Code Table 0000 CIDRW System User’s Manual 117 SECTION 7 Appendix Protective Construction IP- is governed by the test methods described below. Check in advance the seal characteristics under the actual environment and conditions of ...
- マニュアル
...(For details on setting transition charts, see page 158.) Alphabet Display Format The alphabet appears on the main and sub-displays as shown in the following table. A B C D E F G H I J K L M N O P Q R S T U V W X Y Z INDEX SETTING TRANSITION CHARTS 20 Part Names and Functions ZX2 User’s Manual Button Operation The functions of buttons change according to the currently selected mode. CONTENTS Button type Button function RUN mode button Cursor buttons button button button MENU/SET button MENU mode • Normal press:...
- マニュアル
... are output when the command is processed normally, and the command execution result is OK. A delimiter is inserted at the end of the response. The delimiter is always CR. Command Execution Result Parameter 1 0 CR Delimiter O ...