全 5560 件が検索されました。(2121 - 2140件を表示)

  • マニュアル

    ...Section 4-29 FORCED RESET 4-28 FORCED SET Forced sets a bit in an IR, LR, HR, AR, or TC area. Bits need to be force set one at a time. Command Format @ Unit no. X101 X100 K Data area S OP1 OP2 OP3 Word OP4 X103 X102 X101 Bit X100 X101 FCS X100 * CR C I O –...IR area L R – –...LR area H R – –...HR area A R – –...AR area T I M – T I M H C N T – C N T R TC area T M S – T I M W C N T W...

  • マニュアル

    ...2. New Commands The C200H-IDS01-V1 incorporates data management commands, with which it is possible to check the reliability of the Data Carrier’s data. The details of the commands are as follows: Function Checking of data Command MD-...

  • マニュアル

    ... A$;X, Y, A$, I, J PC WRITE Statement Purpose: To write data to the PC Format: PC WRITE “[, ...]”; [,, ...] Note For parameter definitions, refer to Appendix C. Examples: PC WRITE “H4, A2, I3, O4”; 1234, “AB”, ...

  • マニュアル

    ...00 00 00 No. of DM words Program area size Item EM bank number File memory size Kind of file memory Meaning Unit Program area size The size of PC Setup and program area K words (1K words = 1,024 words) No. of DM words Total words in the DM area Words EM bank number Extended Data Memory (EM) Area bank number Bank Kind of file memory 00: No file memory 01: SPRAM 04: First half RAM, second half ROM --- File memory size 0000: 0 (no file memory) 0001: 1000 0002: 2000 Blocks PC status (response): The value of the ...

  • マニュアル

    ..., 15 operating procedures, 14 display functions BK, 16 CAM, 16 DATA, 16 MODE, 16 STEP, 16 E error codes, 30 errors causes and corrections, 46 clearing, 48 data setting console display, 48 indicators, 48 F–...

  • マニュアル

    ... type setting 8 7 9 01 2 3 6 5 4 C200H-TC00@ Setting 0 1 2 3 4 5 6 7 8 9 Sensor type R S K J T E B N L U The switch is factory-set to 2. The selected position is shown by the arrow. Turn the switch with a small flatblade screwdriver. Selected position 11 Section 2-2 Switch Settings C200H-TC10@ OFF ON Setting OFF ON Sensor type JPt Pt The switch is factory-set to OFF. See Appendix B Sensor Temperature Measurement Range for the measurable temperature range. Operation and ...

  • マニュアル

    ...◎nductor 一一一 BX-G 一一一 G旬eraトpurp◎se,standardclass Copper C◎pper B R ●工■ RX-G,SX・G ●●一 AlbywRhcoppgromickglasmak)r◎◎nstRuθnt S ●●一 RX・H,SX・H ●●■ Heat-rgsistant,standardclass K CA KX-G WCA・G Gθ随raトpurpos9,standaζdclass Albywithnickθlorchromeasmajorconstituent Alloyw口hnickθlasmalorcons慌uent KX・GS WCA唱S KX・H WCA-H Heat-resistant,standardclass KX・HS WCA-HS Heat・resistant,precisionclass WX-G WCA{i General・purP◎se,standardclass lron A‖oywロhcoppgrornickθlasmajorcons世U白nt WX・H WCA・H Heat・resistant,...

  • マニュアル

    ... mA, 0 to 5 V, 1 to 5 V, 0 to 10 V, –10 to 10 V Outputs: 0 to 5 V, 1 to 5 V, 0 to 10 V, –10 to 10 V Sensor types: R, S, K, J, T, B, L Sensor types: Pt100, JPt100 1 external input 2 external outputs Note The Analog Input Units, Analog Output Units, Temperature Input Units, and Counter Units belong to a group called Special I/O Units. The front-panel indicators and other parts of Special I/O Units differ from those of other I/O Units. One I/O ...

  • マニュアル

    ... Sensor Unit models and available temperature sensors. Only one kind of temperature sensor can be connected to the C200H-TS001 or C200H-TS002. Each Temperature Sensor Unit connects to a maximum of four temperature sensor inputs. Model Connectable temperature sensor C200H-TS001 ...

  • マニュアル

    ...and UM ALLOCATION instructions. 1. Clear memory. CLR SET NOT RESET EXT MONTR Note UM allocation is not possible unless memory is cleared first. 2. The expansion DM area can be set to 0, 1, 2, or 3 K words. The following key sequence creates a 2-KW expansion DM area (DM 7000 to DM 8999). CLR FUN VER CHG 2 SET 9 7 1 3 WRITE Press the 0 Key to eliminate the expansion DM area (0 KW). or Press the 1 Key to allocate DM 7000 to DM 7999 (1 KW). or Press the 2 Key to allocate ...

  • マニュアル

    ...xii xiii xiii 1 2 14 16 19 23 24 34 38 55 Appendices: System Protocols A B C D E F G H I J K L E5K Digital Controller Read Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . E5K Digital Controller Write Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . E5ZE Temperature Controller Read Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . E5ZE Temperature Controller Write Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . E5J Temperature Controller Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . ES100 Digital Controller Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . K3T Intelligent Signal Processor Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . V500/V520 Bar Code Reader Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3Z4L Laser Micrometer Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Visual Inspection System Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . V600/V620 ID Controller Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Hayes Modem AT Command Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Index . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 59 77 93 115 135 149 191 213 225 257 275 311...

  • マニュアル

    ...External device Details LPRT When not outputting Chinesederived characters (Kanji) No conversion from Shift JIS code to JIS code. NKPRT When outputting Chinese-derived Shift JIS code is converted to JIS code and characters, the printer control code KI (Kanji In): [ESC]...

  • マニュアル

    ... rate for all nodes on the same network. • Be sure to set routing tables for CVM1 and CV-series PLCs. When a CVM1 or CV-series PLC is connected to the network, set routing tables at all the nodes. C C L P ...

  • マニュアル

    ... current is 20 mA) Clockwise (CW) Rotation Max. response frequency 30 KHz Output phase difference A/B phase difference 90°±45° (1⁄4±1⁄8T) Output rise/fall time 1.0 µs max. (Control output voltage 5 V, load resistance 1 ...

  • マニュアル

    ... axes that are to be edited. It is assumed here that the MCSS has already been installed. 8-8-1 Selection of MC Model 1, 2, 3... 1. Turn on the power supply to the computer, and start up the MCSS. 2. Select “...

  • マニュアル

    ...4.3 mA ON voltage 17.4 V min. OFF voltage 3.0 V max. ON response time 1 ms max. OFF response time 2.5 ms max. Circuit Configuration +24 V 24 VDC 680 Ω 5 6 kΩ 5.6 Photocoupler The circuit in the table below is used to interface outputs RUN (X and Y) and ALMRS (X and Y). Item Specification Max. switching capacity 50 mA/24 VDC Circuit Configuration +24 V Leakage current 0.1 mA max. Output Residual voltage 1.0 V max. External supply voltage 24 VDC ± 10% Photocoupler The circuit in the table below ...

  • マニュアル

    ...-V1 Expansion Memory Unit Uploads the ladder program and DM 6144 to DM 6655 from the PC to the EEPROM and downloads the ladder program and DM 6144 to DM 6655 from the EEPROM to the PC. EEROM-JD EEPROM 256 ...

  • マニュアル

    ... to the same Rack does not exceed the maximum current provided for the Rack. Limitations Due to Unit Current Consumption Rack type Number of Analog I/O Units that can be mounted on the same Rack Rack model C200HX/HG/HE CPU R ...

  • マニュアル

    ... max. 19 Section Specifications Output Specifications Item 2-1 Specification Maximum switching capacity Minimum switching capacity Leakage current 30 mA at 4.75 to 26.4 VDC (NPN open collector) (16 mA: Terminals with 1.6-...

  • マニュアル

    ...CQM1H-PRO01-E LCD display Mode switch FUN SFT A ST OR H AA LD AC OUT N M 7 0 . −IR TR J *EM WR/LR K AR HR EM DM P CH *DM Q CONT # R 6 T DEL MON 2 3 Y TEXT ! CLR VRFY NOT B C CHG W INS TN AND G H AC OUT N M 7 E F 4 6 0 6 D 2 DR IR . −IR TR J *EM WR/LR ...