全 5560 件が検索されました。(2281 - 2300件を表示)
- マニュアル
... D Communications........................................................................................................D-1 Appendix E Calibration ..................................................................................................................E-1 Appendix F Read Cycle.................................................................................................................. F-1 Appendix G Symbologies ............................................................................................................. G-1 Appendix H I/O Parameters ...........................................................................................................H-1 Appendix I Symbol Quality ............................................................................................................. I-1 Appendix J Matchcode................................................................................................................... J-1 Appendix ...
- マニュアル
...Cable with Connectors on Both Ends (M12 Straight/M12 Straight) Shield Strengthening Connector cable *3 M12/Smartclick Connectors Wire Gauge and Number of Pairs: AWG22, 2-pair Cable Cable color: Black 1-8 Model 0.3 XS5W-T421-AMD-...
- マニュアル
...C C EAN-8/JAN-8 FF FF B B EAN-13/JAN-13 F F A A Bookland EAN F F A A Code 128 L
None K K GS1-128 L None P P Code 39 C None M M Code 39 Full ASCII None None M M Trioptic None None None None Code 32 None None None None Code 93 None None L L I 2 of 5 I None I I D 2 of 5 H None H H IATA H None H H Codabar N None N N... - マニュアル
... active job slot number when the operation is done. CmdCode and ExeCmd Operation Example: Job change EXE CMD EXE CMD ACK ONLINE TRIGGER READY A,B,C,D,E,F G H I Task 3-20 J K Description LM EIP Output Assembly Prerequisite The Smart Camera must not be controlled by AutoVISION, FrontRunner, Web Monitor, or Custom User Interface. A Stop triggering the inspection. If running a continuous inspection (without triggers), it is recommended to go offline before starting job change. GO OFFLINE = TRUE B If Data Valid or Error is TRUE, clear these outputs. RESET DATA ...
- マニュアル
...Appendix E Calibration................................................................................................................E-1 Appendix F Read Cycle ............................................................................................................... F-1 Appendix G Symbologies ........................................................................................................... G-1 Appendix H I/O Parameters .........................................................................................................H-1 Appendix I Symbol Quality ......................................................................................................... I-1 Appendix J Matchcode................................................................................................................ J-1 Appendix ...
- マニュアル
... bytes) The total number of characters in the Command String. • Command String (256 byte maximum) The ASCII character array of the command sent from the PLC to the code reader. Command Length 0x08 0x00 0x00 Command String 0x00 0x3C('<') 0x4B('...
- マニュアル
... more than enough for a typical packet to reach its destination host but can be configured to last longer or shorter per network requirements. Default = 128 Examples The following section provides examples of how to configure the custom Ethernet object using the Custom Ethernet Link ...
- マニュアル
... bytes) The total number of characters in the Command String. • Command String (256 byte maximum) The ASCII character array of the command sent from the PLC to the code reader. Command Length 0x08 0x00 0x00 Command String 0x00 0x3C('<') 0x4B('...
- マニュアル
...11 Click on the gear icon on the upper right of the screen and select Advanced. 12 The Advanced Settings Screen appears. Select the Communications Tab and check that the settings are as follows. [RS232A] Baud Rate: 115.2 ...
- マニュアル
... Single-Task mode) – SETTING LASER MEASURE TASK2 to 4 18 ZS-HL-N User’s Manual OBJECT ([THICK] is not displayed.) – SYNC (Same as Single-Task mode) – TASKSET NONE*, AVERAGE, PEAK, BOTTOM, THICK, STEP, ...
- マニュアル
...: 50% 5: 62.5% 6: 75% 7: 87.5% 0: OFF 1: ON 0: Timing A 1: Timing B 1 to 5 0: OFF 1: Average 2: Peak 3: Bottom 4: Thickness 5: Gap 6: K+mX;+nY ZS-HL-N Series CompoWay/F Communication Command Reference When the measurement object is changed, the settings are initialized according to the selected object. TASK1 settings. The settings in Unit Number 28h are valid only for multi-task mode. Section 3 Setting Value Obtaining and Changing Command Data No. 3h Parameter Parameter X 28h 4h Parameter Y 5h Parameter ...
- マニュアル
... is output in the following format: Z S - L D C 2 CR Version •Other commands Either OK or ER is returned according to the result of the command. The command was executed properly: O K CR The command was not executed properly or the setting was NG: E R CR The delimiter can be selected from the following three types. CR/LF/CR+LF ZS-HL-N Series Non-procedural Communication Command Reference 3 List of Non-procedural Commands List of Non-procedural Commands Command name Format Returned value Description MEASURE MEASURE
Acquires ... - マニュアル
... the reader, the light color will be set automatically for you. If you are using an external light, pick either Narrow Band if you are using a single-color LED such as red, or White if you are using an external white light. 3) Wavelength (nm) / Color Temp (...
- マニュアル
...................................................................................3-53 Display Select..................................................................3-54 I/O lines........................................................................... 2-17 indicators........................................................................... 2-8 Initial Output.................................................................... 3-51 Initialize............................................................................3-33 Input Select......................................................................3-43 installing the Amplifier Unit.............................................. 2-13 installing the Sensor Head...............................................2-10 ...
- マニュアル
...XS6W-6PUR8SS200CM-YF 3 XS6W-6PUR8SS300CM-YF 5 XS6W-6PUR8SS500CM-YF Cable with Connectors on Both Ends OMRON (RJ45/RJ45) Rugged RJ45 plugs *1 Cable color: Light blue *1. Recommended manufacturer 0.3 XS5W-T421-AMD-...
- マニュアル
... r o r h a s o c c u r r e d a t t h e A m p l i f i e r U n i t . *1 No Test command transmission Yes Response received C h e c k t h e n a t u r e o f t h e r e s p o n s e . *2 No C h e c k i f t h e A m p l i f i e r U n i t s e t t i n g ...
- マニュアル
...Reads in timing chart data from a file. Writes timing chart data to a file. Tool Bars Windows Status Bar Next Pane Previous Pane Zoom In Function F5 F10 Ctrl+F5 Shift+F5 Ctrl+J Ctrl+K Ctrl+R Prints the timing chart. Displays recently used files. Closes the application and saves the file. Copies the selected area of the timing chart and saves it to the clipboard. Pastes the contents of the clipboard onto the timing chart. Deletes the selected tags in the Timing Chart Window or Watch Window. Displays/Hides the tool bars. Displays/Hides windows. Displays/Hides ...
- マニュアル
.... 2 SEL NX-series Safety Control Unit Instructions Reference Manual (Z931) 2 - 73 2 Standard Functions MUX This function selects one of multiple selections. Instruction Name Multiplexer MUX FB/FUN Graphic expression FUN MUX ...
- マニュアル
...なります A b c d E F G h I J (13) 入出力コード コントローラリンクユニット (別売) K L m n o P q r S t (1)CF パワー LED メモリカード(コンパクトフラッシュ)への電源供給状態を表します。 電源 ON 時に点灯、OFF 時に消灯します。 (2)CF アク...
- マニュアル
...クシステム等放出口の表示操作位置光学系の調整保護眼鏡保護衣難燃性素材の使用 保護具 * 1 1 4 7 2 1 5 - 4 K * 作業管理等 © OMRON Corporation 2008-2016 All Rights Reserved. 点検・整備安全衛生教育 安全上のご注意 前眼部検査 健康管理 ●警告表示の意味掲示 正しい取...