全 5560 件が検索されました。(2161 - 2180件を表示)

  • マニュアル

    ... first (rightmost → leftmost). Byte Order when Sending The following tables show the order in which data stored in the buffer memory’s transmission data area is sent to the GP-IB bus. • Leftmost byte first (leftmost → rightmost) Word in PLC Bits 8 to 15 ...

  • マニュアル

    ... Supply Voltage Number of Common • 24VDC Digital Output (2 outputs) Specifications Circuitry 100mA/24VDC +V 1mA or lower 1.5V or lower 24VDC ±10% 2 DO_00 L Internal circuits 3-3-4 33 kΩ DO_01 L 33 kΩ 24 VDC Fuse 36 DO_COM Section 3-4 Wiring • 24VDC Digital Input Specifications 24VDC ±10% Rated Input Current ON Voltage 4.06~4.48mA ι24VDC ϕ Min. ≅9.5V OFF Current ON Response Time OFF Response Time Number of commons Max. ≅4.5V 1ms or less Circuitry DI_00 2.7 ...

  • マニュアル

    ... shows the local network table settings for a PLC to which multiple CPU Bus Units are mounted. Ethernet network Controller Link network (Network #A) (Network #B) PS: CPU: ETN: CLK: E C C P T L P S N K U Power Supply Unit CPU Unit Ethernet Unit Controller Link Unit Unit #a Unit #b Local Network Table No. 1 2 ■ Local network A B CPU Bus Unit a b Example 2: Three Interconnected Networks This example shows the relay network table settings for three different interconnected networks. Relay Network Table PLC #1 Node #a Network #A PLC #2...

  • マニュアル

    ...recv send ACK Power interruption E SYN connect SYN, ACK ACK send F G ACK H I send Connection error check RST close recv recv J K FIN send close FIN close ACK connect L Connection is closed using TCP/IP protocol procedure. ACK 1,2,3... In steps 1 to 4 the FINS message send and receive processing is performed using the FINS FRAME SEND command. 5. This example assumes that the host computer’s power is unexpectedly interrupted. The normal close processing cannot be performed at the host computer, and an attempt is made to establish a TCP ...

  • マニュアル

    ... local network table settings for a PLC to which multiple Communication Units (CPU Bus Units) are mounted. Ethernet network Controller Link network (Network #A) (Network #B) PS: CPU: ETN: CLK: E C C P T L P S N ...

  • マニュアル

    ... increasing the number of retries for applications using UDP. b) Insert a noise filter right next to the Unit’s power supply terminals. 24 VDC 24-VDC power supply Noise filter As close as possible Recommended filter: MAS-1206-33 by Nemic-Rambda ...

  • マニュアル

    ...” “T” “D” 06 “o” ““ “0” “R” “W” 13 13 “0” “R” “L” 02 13 “E” “V” “V” “.” “F” “0” “A” “-” 01 07 “T” “K” “N” 01 03 30 “C” “E” 13 “L” 30 13 “F” “*” “S” “N” “A” “O” 01 “R” 0A “A” “N” 07 “-” 81 07 “L” 13 “0” “0” “R” 13 Device Communications I/O Data Device Communications I/O Data Resources These resources are specific for each device called from the register data memory. The program area is also included in one of the resources, but the programs here are strictly indicating areas for storing programs ...

  • マニュアル

    ... word address, the data that is passed will be the data in the form and size specified by the variable data type starting from the specified word address. Program Instance of Function Block Definition A Input D100 m Input D200 n ...

  • マニュアル

    ..., select File - Print and select the desired data from the following Print Choice Dialog Box. The following data and parameters can be selected for printing. Item A B C D E F G H I J K L 88 Name Function Project Tree If this option is selected, the project tree is printed. MC Unit If this option is selected, the specified MC Unit parameters are printed. All Data or Specified Data These options specify the range of MC Unit parameters to print. All Data Print all of the data. Specified Data Print only selected data and parameters. Unit ...

  • マニュアル

    ... Series Models 3G3RV-V1 High-function General-purpose Inverters Setup Manual DeviceNet Communications Unit/Card 3G3MV-PDRT2, 3G3RV-PDRT2 User's Manual SMARTSTEP2 Series Servomotors/Servo Drives Models R88M-G@ (Servo-motors)/R7D-BP@ (Servo Drives) User’s Manual OMNUC G5 Series Models R88M-...

  • マニュアル

    ...for SYSDRIVE MX2/RX Series I582-E1 MX2/RX Series DriveProgramming User’s Manual Servomotors/ SMARTSTEP2 Series Servomotors/Servo Drives Models R88M-G (Servo-motors)/R7DServo Drives BP (Servo Drives) User’s Manual I580-E1 I561-E1 OMNUC G5 Series Models R88M-...

  • マニュアル

    ... Series GRT1-TS2T DRT2-TS04T Thermocouple input Terminal block and main block can be Removable terminal block separated. Hardware DIP switch setting, software Setting Tool. Each input bit can be set up individually when using the Setting Tool. R, S, ...

  • マニュアル

    ....078 ms 0.103 ms 0.206 ms 3.305 ms 512 input words, 512 output words 0.142 ms 0.188 ms 0.377 ms 6.048 ms 0.291 ms 4.674 ms 0.035 ms + K (See note.) 0.567 ms + K (See note.) 256 input words, 256 output bits + 128 0.110 ms 0.146 ms input bits, 128 bit outputs 1,024 input words, 1,024 output words 0.13 ms + ...

  • マニュアル

    ... inputs Model CRT1-TS04T 6 X1 X10 63] [0- 04 AD T1- AL CR MIN N TER RO G ALO OM AN CRT1-TS04P Features Thermocouple input (Switchable between R, S, K, J, T, E, B, N, L, U, W, and PL2.) Platinum resistance thermometer input (PT100 only) Expansion Units Type Expansion Units with 2-tier Terminal Block Appearance I/O capacity 8 inputs (NPN) 8 inputs (PNP) 8 outputs (NPN) 8 outputs (PNP) 16 inputs (NPN) 16 inputs (PNP) 16 outputs (NPN) 16 outputs (PNP) Model XWT-ID08 XWT-ID08-1 XWT-OD08 XWT-OD08-1 XWT-ID16...

  • マニュアル

    ...DC voltage input 1 to 5 V, 0 to 5 V, 0 to 10 V Platinum resistance thermometer input Pt100 (JIS, IEC) Pt1000, JPt100 V DC current input 4 to 20 mA, 0 to 20 mA Thermocouple input K, J, T, L, R, S, B mA Isolation between Channels The input channels are isolated in the Universal Input Unit, so unwanted current paths will not occur between thermocouple inputs or voltage inputs that share the same power supply. Signal converters are not needed to prevent interference between inputs. Universal Input Unit Channel 1 Isolation Channel 2 Isolation Channel 3 Isolation...

  • マニュアル

    ... Model 585) 8 outputs (4 to 20 mA) CJ1W-DA08C Ao8-point Terminal (Block Model 585) 2 outputs (1 to 5 V/ 4 to 20 mA, etc.) CJ1W-DA021 Ao2- point Teminal (Block Model 591) 4 inputs (B, E, J, K, L, N, R, S, T, U, WRe526, PLII, mV) CJ1W-PTS51 Ai4- point Terminal (Block Model 566) 2 inputs (B, E, J, ...

  • マニュアル

    ...insert menu, 13 creating SFC programs, 66 inserting SFC programs, 66 creating simultaneous sequence convergences, 82 creating simultaneous sequence divergences, 81 creating subchart programs, 83 creating transition programs, 70 J jump, 86 jump (loop), 62 135 Index ...

  • マニュアル

    ...  terminal of the B7A Link Terminal to be connected to port 3. J Port 4 power supply: V4 Connect to the + terminal of the B7A Link Ter- n+3 minal to be connected to port 4 (only when using a common power supply). ...

  • マニュアル

    ...-IA4-2 GRT1-TS2T Four-point SmartSlice AC Input Unit (Input voltage: 100 to 120 VAC 50/60 Hz) Four-point SmartSlice AC Input Unit (Input voltage: 200 to 240 VAC 50/60 Hz) Two-channel SmartSlice Temperature Input Unit for Thermocouples (input types: R, S, ...

  • マニュアル

    ...200g CP1W-DA042 4 analog outputs 1 to 5 V, 0 to 10 V, -10 to 10 V, 0 to 20 mA, and 4 to 20 mA Resolution: 1/12,000 0.070A 0.160A 200g CP1W-TS001 Thermocouple inputs K or J, 2 inputs 0.040A 0.059A 250g CP1W-TS002 Thermocouple inputs ...