全 5560 件が検索されました。(2141 - 2160件を表示)
- マニュアル
... increasing the number of retries for applications using UDP. b) Insert a noise filter right next to the Unit’s power supply terminals. 24 VDC 24-VDC power supply Noise filter As close as possible Recommended filter: MAS-1206-33 by Nemic-Rambda ...
- マニュアル
... input terminal and G) OFF voltage OFF current Input current 88 Specification Model Internal I/O common Input impedance 6.0 mA max./point at 24 V DC 3.0 mA min./point at 17 V DC 4.4 kΩ ON delay time OFF delay time 1.5 ms max. 1.5 ms max. Section 4-5 Transistor Remote I/O Terminals with Connectors Item Max. simultaneously ON input points 32 points (See note.) Specification Number of circuits 32 points with one common Note All 32 inputs can be ON simultaneously if the Remote I/O Terminal is mounted...
- マニュアル
... the information contained in this publication. Trademarks • Microsoft, and Windows are either registered trademarks or trademarks of Microsoft Corporation in the United States and other countries. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • COMBICON is a registered trademark of Phoenix Contact ...
- マニュアル
...CQM1HCPU11 Number of I/O points (see note) 512 256 Program capacity (words) CPU Unit external input points DM capacity (words) DC: 16 6K 6K 7.2 K 6K None 3.2 K 3K 15.2 K EM capacity (words) Built-in serial communications ports Peripheral port RS-232C port With With Inner Boards Communications Units Supported Supported Not supported Not supported Without 9 Section 1-2 System Configuration Note Number of I/O points = Number of input points (≤ 256) + Number of output points (≤ 256). Maximum Number of Units CPU Block Only CPU Unit Maximum number of Units connectable CQM1H-...
- マニュアル
..., CJ1W-PDC15 and CJ1W-PH41U Analog I/O Units. • Standard accuracy: ±5% The following conditions were used in the immunity test of the CS1W-PTS51/ PTS52/PTS55/PTS56, PDC55 and CJ1W-PTS51/PTS52. CS1W-PTS51 R or S thermocouple CS1W-PTS55 CJ1W-PTS51 ...
- マニュアル
..., the standby Controller Link Unit will take over operation, and communications operation will continue. Also, Controller Link Units with errors can be replaced without turning OFF the power (i.e., online replacement). Same unit number, same node address CS1D C L ...
- マニュアル
... the block diagram is selected When a step ladder program is selected When a sequence table is selected Overview of User Interface Menu Settings, g , i d continued Submenu/ Command Function Cut Bl k Block Copy Paste Increment Block Address FBD Copy Paste User-defined Blocks Section Description Cuts a function block from the Project Workspace. Copies a function block in the Project Workspace. Pastes a function block in the Project Workspace. Selects and increments the function block address by 1. If the next address is being used, it is also incremented by 1. 2-2 Conditions for selection...
- マニュアル
... of two Basic PID blocks is monitored and manipulated on CX-Process Monitor. So, specify each of the Basic PID blocks as the source designation Control block addresses in the 1-Block Send Terminal to Computer block (Block Model 403). Bas ic PID
... - マニュアル
...Block Name Block Address <147> Lead/Delay 100 to 349 7 Time Fu nction blocks <147> Lead/Delay 100 to 34 9 Outline This function block performs lead/delay operation of control signals on single analog signals. Y1(s) = ...
- マニュアル
...A23 + N.C. contact N.C. contact CCW limit input signal OMRON E2R-A01 Proximity Sensor (NPN-output model). A14 Signal Input common PK564AW stepping motor – CW CCW output (with 1.6-k A8 resistance) 24-V power supply for output A1 Origin Input signal Example: DFU1514W stepping motor driver, made by Oriental Motor Co. 24 V 0V CW output (with 1.6-...
- マニュアル
... can be mounted to the CPM2C-S. There are 2 models of Temperature Sensor Unit: One for input from a thermocouple sensor and one for input from a platinum resistance thermometer sensor. There are 2 input points on each Temperature Sensor Unit. • Thermocouple inputs (and measurement ranges): ...
- マニュアル
... time: 50 ms OFF delay time: 200 ms max. Inputs for normal input (8 points with one common): ON delay time: 100 ms OFF delay time: 1 ms max. Circuit configuration Customizable Counter Unit Input indicator Interrupt inputs 4.7 ...
- マニュアル
... of information. Note Indicates information of particular interest for efficient and convenient operation of the product. 1,2,3... 1. Indicates lists of one sort or another, such as procedures, checklists, etc. Trademarks and Copyrights COMBICON is a registered trademark of Phoenix Contact ...
- マニュアル
... mA 0 to 5 V, 1 to 5 V, 0 to 10 V, –10 to 10 V Outputs: 0 to 5 V, 1 to 5 V, 0 to 10 V, –10 to 10 V Sensor types: R, S, K, J, T, B, L Sensor types: Pt100, JPt100 1 external input 2 external outputs Note The front-panel indicators and other parts of Analog Input Units, Analog Output Units, and Counter Units differ from those of other I/O Units. These Units belong to a group called Special I/O Units. One I/O Unit Connecting Cable (cable length 40 ...
- マニュアル
...Section Specifications and Configurations 1-2 1-2-6 Indicators Optical System (H-PCF Cable) RUN Name Operating g ERR Error Color Green Status Red INS Participating g i network k in Yellow LNK Sending g data li ...
- マニュアル
..., . / 0 1 2 3 4 5 6 7 8 9 : ; < = > ? @ A B C D E F G H I J K L M N O P Q R S T U V W X Y Z [ \ ] ^ _ ` a b c d e f g h i j k l m n o p q r s t u v w x y z { | } ~ ! ” # $ % & ’ ( ) * + , . / 0 1 2 3 4 5 6 7 8 9 : ; < = > ? @ A B C D E F G H I J ...
- マニュアル
... freedom, and output results through open collector outputs. There are two main types of Unit: One provides four control loops and the other provides two control loops with a heater burnout detection function. Each of these has one model that is compatible with thermocouples (R, S, ...
- マニュアル
...E Z I Filter Selection 10 kHz 50 kHz 500 kHz A <3 <3 J J * Maximum allowed frequency of Z-pulses is 1 kHz * M aximum a llowed f requency of Z-pulses is 1 k Hz Note I I Counter Input ZI * Counter Input Z * On On 0V 0V Off Off Z 50% 50% 12 G B C >50 >100 >10 >20 Do not use. * Maximum allowed frequency of Z-pulses is 1 kHz * Maximum allowed frequency of Z-pulses is 1 ...
- マニュアル
... mounting screws: 0.5 N·m Output Specifications (for One Relay) Item Relay Rated load Rated carry current Maximum switching voltage Maximum switching current Maximum switching capacity Minimum applicable load (reference value) Specifications DRTA-NY5W-...
- マニュアル
...Analog Output Unit 4 outputs (1 to 5 V/4 to 20 mA, etc.) CS1W-DA041 Isolated-type Thermocouple Input Unit 8 outputs (1 to 5 V, etc.) CS1W-DA08V 8 outputs (4 to 20 mA) CS1W-DA08C 4 inputs (B, E, J, K, N, R, S, T, CS1W-PTS01-V1 DC±80 mV) 4 inputs (B, E, J, ...