全 367 件が検索されました。(201 - 220件を表示)
- マニュアル
...cyleakagecurrentfromthecabl白increasθs,causingthelnverteroutputcurfeRt toincreaseaswell.Thismayalsoaffectperipheraldevices.Toprevent!his,ad・ justthecarrierfrequencyaccordingtothefollowingstandards: ●Cablelengthof50metersor{ess=10kHzorless eCablelengthof50to100meters:5kHzorless Note1.Thesettingrangeforthe400●VACc!assis"1to5.日 4・20 ◆ 〕 ,◇ 》{: ソ'∨イ》、、 ㊨ ---------------------[End of Page 4202]--------------------- Prepan'ngforOperation Chapter4 Note2.Thefactorysettingforthe3G3EV・A4015・CUε{...
- マニュアル
... is automatically set by the CX-Protocol. (R(3N+3), 4) The Inverter’s actual data to be sent. This example selects Variable and Read R() and sets the operand. Set Data to 3N + 3 because the RUN command data uses four bytes each from ...
- マニュアル
... is automatically set by the CX-Protocol. (R(3N+3), 4) The Inverter’s actual data to be sent. This example selects Variable and Read R() and sets the operand. Set Data to 3N + 3 because the RUN command data uses four bytes each from ...
- マニュアル
...: Beginning Command Storage Word Specify the beginning word address for the command data transferred to the DeviceNet Master Unit. Preset the data to be transferred in consecutive words as shown in the following table. Bits Word address S S+1 S+2 ...
- マニュアル
...Frequency reference to Slave 1 Second Slave address 0002 RUN command to Slave 2 Frequency reference to Slave 2 Third Slave address 0003 RUN command to Slave 3 Frequency reference to Slave 3 Protocol macro function S 1 S 2 ...
- マニュアル
...Command code (Set Explicit Message FINS command 2801.) S+1 Node address of slave or master to which message is to be sent: 0 to 3F Hex (0 to 63) S+2 Class ID code (Sets the DeviceNet class code for the function.) ...
- マニュアル
...S: Beginning Command Storage Word Specify the beginning word address for the command data transferred to the DeviceNet Master Unit. Preset the data to be transferred in consecutive words as shown in the following table. Word address S S+1 S+2 ...
- マニュアル
... stored in the Controller as shown below. ● Controller Alarm Codes • Alarm codes such as the following are stored at the Controller for alarms that occur at the Servo Driver. Controller alarm (error) code: 40@@ (Hex) The leftmost two digits from the Servo Driver'...
- マニュアル
... is automatically set by the CX-Protocol. (R(3N +3), 4) The Inverter’s actual data to be sent. This example selects Variable and Read R() and sets the operand. Set Data to 3N + 3 because the RUN command data uses four bytes each from ...
- マニュアル
...Node address of the Slave/Master to which the Explicit Message is sent: 0 to 3F hex (0 to 63) S+2 Class ID code (Set the DeviceNet Class code of the target function.)*1 Explicit Message service codes Write: 10, Read: 0E ...
- マニュアル
...0 Command code (Set the FINS Explicit Message command (2802).) S+1 Node address of the Slave/Master to which the Explicit Message is sent: 0 to 3F hex (0 to 63) S+2 Explicit Message service codes Write: 10, Read: 0E ...
- マニュアル
...力パルス周期の求め方入力電力によって変化する出力パルス周期は以下の式で求められます。 出力パルスの周期(s)=3,600(s)/(入力電力/パルス出力単位) 例: 三相3線式で、入力電力が200kW、パルス出力単位が10kW・hのときは、 出力パルスの周期=3,...
- マニュアル
...) Communications port (internal logical port): 0 to 7 Hex D Send Data Word Allocations (Third Operand of PMCR Instruction) Word No. S+0 Data format No. of send data words (4-digit Hex) S+1 Reserved S+2 ...
- マニュアル
.... CTBL(882) with High-speed Analog Sampling Function CTBL P M S S P: Port specifier (#0003) M: Register target value comparison table and start comparison. S: Target value comparison table Target value S+1 S+2 ...
- マニュアル
... copied to D through D+4 and program execution continues with the next instruction after MCRO(099). 384 Section 3-17 Subroutines MCRO(099) S A510 MCRO S+1 A511 N S+2 A512 S S+3 A513 D S+4 A514 MCRO Input N Execution of subroutine between SBN(092) and RET(093). MCRO(099) D A515 D+1 A516 D+2 A517 D+3 A518 D+4 A519 S' D' Output SBN N The subroutine uses A510 to A514 as inputs and A515 to A519 as outputs. MCRO(099) can be used to consolidate two or more ...
- マニュアル
...(×1, ×2, or ×4). When the multiplier is disabled, the counter 1 input method (×1, ×2, or ×4) is used. CTBL(882) Settings for the High-speed Analog Sampling Function CTBL P M S S S+1 S+2 S+3 P: Port specifier (#0003) M: Register target value comparison table and start comparison. S: Target value comparison table Target value 8-digit hex First word of data sample storage area 0000 to 7FFF hex (DM Area address) Number of data samples 0001 to 8000 hex 295 Section 7-9 Analog Input Functions Example CTBL #3 #0 D00000 Sampling ...
- マニュアル
...Code DOUBLE FLOATING TO 16-BIT BINARY FIXD @FIXD 841 FIXD(841) S D Function Converts the specified double-precision floating-point data (64 bits) to 16bit signed binary data and outputs the result to the destination word. ...
- マニュアル
... allocated, the ladder program in the interrupt task is not checked by compile on the CX-Programmer. 19 Target value comparison table Item CPM1A S Number of target values S+1 to S+2 Lower word of target value: BCD ...
- マニュアル
... not checked by compile on the CX-Programmer. Allocate the task type and check the program. 19 Target value comparison table Item CPM2A S Number of target values S+1 to S+2 Lower word of target value: BCD ...
- マニュアル
...+1 Target value #1, lower 4 digits (BCD 8 digits) S+1 Lower word of target value 1 (BIN 8 digits) S+2 Target value #1, upper 4digits F8388608 to 08388607 S+2 Upper word of target value 1 S+3 Subroutine number (Incremental) 0000 to 0255 ...