全 367 件が検索されました。(301 - 320件を表示)
- マニュアル
...Ambient temperature Operating: 0 to 40 ; Storage: -25 to 60 Ambient humidity 35% to 85% (with no condensation) Ambient environment No corrosive gases 10 to 150 Hz; half-amplitude: 0.35 mm Vibration resistance (max. acceleration: 50 m2/s) Shock resostance 150 m2/...
- マニュアル
...) Dielectric strength 500 V AC, 50/60Hz for 1 min(between case and cable terminals) Vibration resistance 10 to 150Hz ,1.5mm double amplitude for 4 sweeps of 8min each in X, Y, and Z directions Shock resistance 300m/...
- マニュアル
... column C from the 16-word set (S to S+15) to the 16 bits of word D (00 to 15). 133 Section 5-14 Data Movement C Bit 15 Bit 00 S S+1 S+2 S+3 . . . 0 0 0 0 1 1 1 0 0 0 1 0 0 0 0 1 S+15 0 1 1 1 0 0 0 1 1 0 0 0 1 0 1 0 1 1 0 1 0 0 1 0 0 1 1 1 0 0 0 1 0 0 0 1 1 0 1 1 0 0 ...
- マニュアル
...白itavethe 費CiaPROGRAIvlrnode,{lortheP-RO胡Wr#er,P繍e瀬t舗aceU寵、 書tc,),besuret。 selectth…舗。 debe言。 鵡c。 nnectingthepe勅erai device,oraiternative}ysapPlypowerto語ePCa討er語eperiphera{ deviceisCO!「nected. 2-...
- マニュアル
... Area Command Allocations DM Wd 118 b15-b12 b11-b8 b7-b4 s 0 3 0 4 s+1 1 0 0 0 s+2 1 0 1 0 s+3 1 0 5 0 s+4 1 0 6 0 b3-b0 Application Program Examples Section 8-4 DM Area Data Allocations DM Wd b15-b12 b11-b8 b7-b4 b3-b0 r 1 0 0 4 r+1 0 0 0 0 r+2 0 0 0 0 r+3 0 1 7 7 r+4 0 5 4 4 r+5 1 0 1 4 r+...
- マニュアル
... the word-to-digit conversions that they produce are shown below. Di: 0030 Di: 0011 R R S 0 S 0 S+1 1 S+1 1 2 S+2 2 3 S+3 3 Di: 0013 Flags Di: 0032 S R 0 S R 0 S+1 1 S+1 1 2 S+2 2 3 S+3 3 ER: Undefined digit designator, or S plus number of digits exceeds a data area. Content of a source word is 0. Indirectly addressed DM word is non-existent. (Content of *DM word is not BCD, or the DM area ...
- マニュアル
...). STARTmustbeexecutedinordertobeginp◎sitioningagain.WhenPCINTERRUPTisalsoclearedandSTARTisexecuted,p◎sitjonjngwillproceed directlytoP◎inte(address1124),thetargetp◎s口ionforthenextPOsitioning action. 63 ---------------------[End of Page 9628]--------------------- "OOOO・ IRAreaAlloeations Section5-1 CautionThePositionControlUnitreceivesb◎thPCarldextemalinterrupts.Therela・・ tionshipbetWeenthetWotypesofinterruptsisalogicafOR.inetherwords, anintemLptoccursifeitherisON;tocleartheinterrupt,b◎thmustbeOFF. ORIGENSEARCH(Bit14} iNCHCCW(Blt15} 5--...
- マニュアル
...Di RB Operands Converts up to four hexadecimal digits in source channel (S) into decimal values from 0 to 15 and turns ON, in result channel(s) (R), bit(s) corresponding to converted value. Digits designated in Di channel. 3 ...
- マニュアル
... the word-to-digit conversions that they produce are shown below. Di: 0011 Di: 0030 R R S 0 S 0 S+1 1 S+1 1 2 S+2 2 3 S+3 3 Di: 0013 Di: 0032 R R S S+1 0 S 0 1 S+1 1 2 S+2 2 3 S+3 3 159 Section 5-14 Data Conversion Flags ER: Undefined digit designator, or S plus number of digits exceeds a data area. Content of a source word is 0. Indirectly addressed DM word is non-existent. (Content of *DM word is ...
- マニュアル
... R is OFF and CP goes from OFF to ON. Counting will resume when SI is turned ON again. The count pulse for CNTH(24) is input bit 0000 and the hard reset input is input bit 0001. The count signal must be at least 150 µ...
- マニュアル
... of circle” 130 INPUT ”Input radius (to end, radius = 0)”;R% 140 IF R%=0 THEN END 150 GOSUB *CAL 160 PRINT ”Area of radius ”;R%;” is ”;S!;”.” 170 GOTO *START 180 ‘ 190 *CAL . ................... Subroutine calculating area of circle 200 ...
- マニュアル
... the execution condition is ON, CTW(63) copies bit column C from the 16-word set (S to S+15) to the 16 bits of word D (00 to 15). C Bit 15 Bit 00 S S+1 S+2 S+3 . . . 0 0 0 0 1 1 1 0 0 0 1 0 0 0 0 1 S+15 0 1 1 1 0 0 0 1 1 0 0 0 1 0 1 0 1 1 0 1 0 0 1 0 0 1 1 1 0 0 0 1 0 0 0 1 1 0 1 ...
- マニュアル
... words 3: 4 words Not used. Some example Di values and the word-to-digit conversions that they produce are shown below. Di: 0011 Di: 0030 R S S+1 0 1 2 3 R S+3 Di: 0013 Di: 0032 R S S+1 Flags ER: 0 1 2 3 S S+1 S+2 0 1 2 3 S S+1 S+2 ...
- マニュアル
... the word-to-digit conversions that they produce are shown below. C: 0011 C: 0030 R R S 0 S 0 S+1 1 S+1 1 2 S+2 2 3 S+3 3 C: 0013 C: 0032 R R 0 S 0 S S+1 1 S+1 1 2 S+2 2 3 S+3 3 The following is an example of a one-digit encode operation to digit number 1 of R, i.e., here C would be 0001. First source word 0 0 0 1 0 0 0 1 0 0 0 1 0...
- マニュアル
...CV500-TDL21canstartandstopoperationwiththeRUN/STOPselectoronthe CV500-TDL21'sfrontpanel.Referto3-5PCSettingsfordetaiisonthesettings ofCPUBusUnitsystemsetuparea. HardwareReset(Restart) WordAOOIoftheCVSOO-TDし21'sauxiliaryareaisusedasaCPUBusUnitrestartbits.AsinglebitofthewordisallocatedtotheCV500-TDL21accordingto theCV500-TDL21'sunitnumber. 1514131211109876543210 WdAOO1 Unitno. WhenrestartingtheCV500-TDL21,turnonthebitcorrespondingtotheunit numberthathasbeenpresetwiththeunitnumberselectoronthe CV500-TDL21'sfrontpanel.TheCV500-TDL21willnotrestartafterchanging theunitnumberorthesettingsoftheCPUBusUnitsystemsetuparea,inwhich caseturntheCPUoffandon. ...
- マニュアル
... through S+(N/2)–1, converted to ASCII, and transmitted through the specified port. The bytes of source data shown below will be transmitted in this order: 12345678... MSB 1 3 5 7 S S+1 S+2 S+3 LSB 2 4 6 8 The following diagram shows the format for host link command (TXD) sent from the ID Controller. The ID Controller automatically attaches the prefixes and suffixes, such as the node number, header, and FCS. @ X X Node number X X Header code X X ......... X Data (122 ASCII characters max.) X X FCS ∗ CR Terminator...
- マニュアル
... contains the number of words to be sent and S+1 and the following words contains the actual data to be sent, as shown in the following diagram. S: No. of send words S+1: Send data S+2: Send data S+3: . . . . . . . Specifies the number of words to send, including S (256 words max.) The first input word, D, specifies the address of the first word in which to store the receive data. If there is no receive data, set D to a dummy address. If a constant is specified, the Error Flag (SR 25503) will turn ON ...
- マニュアル
...3032 hex (not 02 hex). Further, to write the CompoWay/F command to the command storage area using CMND(490) in frame order (without creating empty bytes), the SID component of the CompoWay/F command requires 1 byte of ASCII as 30 hex, so the subsequent components (...
- マニュアル
...: First Command Word) Word Contents (Hex) Meaning S 28 01 S+1 02 1C EXPLICIT MESSAGE SEND command code: 28 01 Hex Slave node address: 2 BYTE DATA READ command service code: 1C Hex S+2 S+3 00 2F 00 01 Class ID: 002F Hex Instance ID: For IR Area 1: 0001 Hex S+4 0A 00 S+5 28 00 Read start address: 10 = 000A Hex Address L: 0A Hex, Address H: 00 Hex No. of bytes of read data: 40 bytes = 28 Hex (The rightmost byte is not used.) D: Response Words (D: First Response Word)...
- マニュアル
...S CIO 0002 0 1 5 5 CIO 005000 S+1 CIO 0003 2 5 0 6 CIO 005001 S+2 CIO 0004 1 0 2 9 CIO 005002 S+3 CIO 0005 6 0 4 7 CIO 005003 S+4 CIO 0006 4 1 0 6 CIO 005004 S+5 CIO 0007 7 9 1 0 CIO 005005 S+6 CIO 0008 1 0 5 0 CIO 005006 S+7 CIO 0009 9 8 0 0 CIO 005007 5-13-6 COUNTER: CNT Ladder Symbol CP R Operand Data Areas N: Counter number # CNT N S S: Set value...