全 2903 件が検索されました。(2041 - 2060件を表示)
- マニュアル
...Additionally there may be significant property damage. DANGER Make sure to test the operation of the product after setting with the DIP Switch to verify that the product operates as intended. WARNING Do not try to disassemble, repair, or modify this product. Doing ...
- マニュアル
...14.5 11 CAUTION Make sure to connect the cables properly to prevent them being disconnected during settings. Instruction sheet (this document) (1) dia. 4.6 Do not connect the dedicated cables of this product with another device. Doing ...
- マニュアル
....omron.com/f3sg-r_tool © OMRON Corporation 2014-2022 All Rights Reserved. Original Instruction 9600137-6D Dimensions Suitability for Use [Unit: mm] Ratings/Specifications Safety Precautions Do not connect the dedicated cables of this product with another device. Doing ...
- マニュアル
...(1) Attach the Spatter Protection Cover to the Safety Light Curtain. (Fig. 1 ) (2) Hook the Bracket in the groove on the back of the Safety Light Curtain. (Fig. 2 ) (3) Push the Bracket to the Safety Light Curtain ...
- マニュアル
...) (1) Attach the Spatter Protection Cover to the Safety Light Curtain. (Fig. 1 ) (2) Hook the Bracket in the groove on the back of the Safety Light Curtain. (Fig. 2 ) (3) Push the Bracket to the Safety Light Curtain ...
- マニュアル
... may result in serious injury or death. Additionally there may be significant property damage. [F3SG-□RA Receiver] [F3SG-□RR Receiver] Screw (M2.5) Screw (M2.5) Lamp WARNING Do not try to disassemble, repair, or modify the product. Doing ...
- マニュアル
... cables are connected with the polarity reversed, the load will not operate, or the operation indicator will not light. ・Make sure that signal lines are always connected through a load. ・Use Sensors that meet the specifications. ・Do not pull on the connectors and cables. Doing ...
- マニュアル
... make good use of the descriptions before installing and operating the product. Keep this document at the place where the operator can refer to whenever necessary. © OMRON Corporation 2016-2023 All Rights Reserved. Do not try to disassemble, repair, or modify this product. Doing ...
- マニュアル
...-R before replacing the End Cap. Function End Cap Description Black 24 V Active (factory default setting) White 0 V Active External Test Input Selection - Do not remove the insulating rubber attached to the End Cap. Failure to do ...
- マニュアル
... stop before a person reaches the hazardous part, resulting in serious injury. Do not connect each line of F3SG-R to a DC power supply of higher than 24 VDC+20%. Also, do not connect it to an AC power supply. Failure to do ...
- マニュアル
... go undetected, resulting in serious injury. Make sure to install the F3SG-RR at the safe distance from the hazardous part of the machine. Otherwise, the machine may not stop before a person reaches the hazardous part, resulting in serious injury. Install a protective structure ...
- マニュアル
... go undetected, resulting in serious injury. Make sure to install the F3SG-R at the safe distance from the hazardous part of the equipment. Otherwise, the machine may not stop before a person reaches the hazardous part, resulting in serious injury. Install a protective structure ...
- マニュアル
... go undetected, resulting in serious injury. Make sure to install the F3SG-R at the safe distance from the hazardous part of the equipment. Otherwise, the machine may not stop before a person reaches the hazardous part, resulting in serious injury. Install a protective structure ...
- マニュアル
...F3SG-RR before replacing the End Cap. Function End Cap Description Black 24 V Active (factory default setting) White 0 V Active External Test Input Selection - Do not remove the insulating rubber attached to the End Cap. Failure to do ...
- マニュアル
... up gradually. Malfunctions in case that the power supply picks up gradually. In case that the input circuits close before the power supplies, internal logic may malfunction. (2) Handling Do not drop the F3SP-B1P or shock or vibrate the F3SP-B1P excessively. Doing ...
- マニュアル
... the following locations. Inappropriate and insufficient measures may result in malfunction. ・Locations subject to static electricity or other forms of noise. ・Locations subject to possible exposure to radioactivity. ・Locations close to power supplies. ●Installation / Mounting ・ Do not drop or disassemble. Doing ...
- マニュアル
... in EU.) When using a commercialized switching regulator, be sure to ground FG (frame ground terminal). (If not grounded, it may cause erroneous operations due to the switching noises.) Use appropriate control devices to materialize the safety functions. Failure to do ...
- マニュアル
... in EU.) When using a commercialized switching regulator, be sure to ground FG (frame ground terminal). (If not grounded, it may cause erroneous operations due to the switching noises.) Use appropriate control devices to materialize the safety functions. Failure to do ...
- マニュアル
... in connection with this product may behave in an unexpected way. Ensure that the connections are made properly at the input and output terminals. Failure to ensure this may cause an electric shock or damage the safety functions. Ensure that sufficient attention is given ...
- マニュアル
... in EU.) When using a commercialized switching regulator, be sure to ground FG (frame ground terminal). (If not grounded, it may cause erroneous operations due to the switching noises.) Use appropriate control devices to materialize the safety functions. Failure to do ...