全 5559 件が検索されました。(1661 - 1680件を表示)
- マニュアル
...選択した場合C、華氏を選択した場合Fを表示します。 ■セグメント表示 7SEG 11SEG 7SEG 11SEG A B C D E F G H I J K a b c d e f g h i G H a b c d e f g h i j k L M N O P Q R l I N o p J K l m n o p q r S T U V W X Y Z 0 1 2 3 ...
- マニュアル
...)2 Tempareture ±5°C two hours or later after the power turns ON (However, only after correction according to the surrounding environment) Low-cut current setting value 0.1% to 19.9% of rated input with 0.1% increments ■Wiring diagram Power supply side(...
- マニュアル
...P0 P2 NC ⑥ DO NOT USE ⑦ NC ⑧ ∼ + − − + ⑨ * * RS-485 ⑩ ⑮ 3S EV2 COM2 ⑯ 3L CT2 ⑰ NC EV1 ⑱ COM3 B(+) ⑲ OUT1 A(−) ⑳ OUT2 k ℓ k ℓ * Voltage input or None voltage input <at 1-phase 3-wire/3-phase 3-wire> Load side(L) Power supply side(...
- マニュアル
... is shown. When choosing Fahrenheit, °F is shown. ■Segment display 7SEG 11SEG 7SEG 11SEG A B C D E F G H a b c d e f g h a b c d e f g h I J K i G H i j k S T U V W X Y Z 0 1 s t u W X Y y Z Y 1 s t u v w x y z 0 1 2 2 2 L M N O P Q R l I N o p J ...
- マニュアル
...(*1) ±1.0%F.S.±1digit(定格周波数の±5Hzの範囲における、 周囲温度23℃、定格入力、力率1の時の電力の割合) EV2 COM2 ⑯ 3L k CT2 ℓ ⑰ NC EV1 ⑱ COM3 B(+) ⑲ OUT1 A(−) ⑳ OUT2 偶数、奇数、なし 最大伝送距離 500m 最大接続台数 CompoWay/F:31台、Modbus:99台 ■外形寸法(単位:㎜) ⑦ P3 負荷側 (L) 電源側 (...
- マニュアル
...偶数、奇数、なし 最大伝送距離 500m 最大接続台数 CompoWay/F:31台、Modbus:99台 ■外形寸法(単位:㎜) LOW ⑦ P3 EV2 COM2 ⑯ 3L ℓ k CT2 ℓ ⑰ NC EV1 ⑱ COM3 B(+) ⑲ OUT1 A(−) ⑳ OUT2 負荷側 (L) 電源側 (K) R N S T * * RS-485 1L ⑬ 2S ⑭ COM2 ℓ ⑯ 3L ...
- マニュアル
... setting: Short-circuited with Pins No. 15 and 17 using a jumper pin. 16 I COM OUT 18 to 19 RESERVE (reserved) 20 NC This section explains the specifications of the terminal blocks and I/O connector. 3.9 ...
- マニュアル
..., or other wireless devices may suffer reception interference.. IX Alphabetic Characters for Setting Data This manual uses the following alphabetic characters for setting data. X a b c d e f g h i j k l m A B C D E F G H I J ...
- マニュアル
... may cause welding of contact points or burning. VII Alphabetic Characters for Setting Data This manual uses the following alphabetic characters for setting data. VIII a b c d e f g h i j k l m A B C D E F G H I J ...
- マニュアル
... errors. Appendices Provides specifications and settings lists. VIII ● Settings data notation The letters of the alphabet in settings data are displayed as shown below. a b c d e f g h i j k l m A B C D E F G H I J ...
- マニュアル
.... Appendices Provides specifications and settings lists. XII Settings Data Notation The letters of the alphabet in settings data are displayed as shown below. a b c d e f g h i j k l m A B C D E F G H I J ...
- マニュアル
...Response MRC SRC Response code "05" "03" "0000" Format Buffer size "00D9" Response codes: The above indicates a normal end. For the response codes, see 1-7 Operation Commands (CompoWay/F Communications) (page 1-11). Model ...
- マニュアル
.... Appendices Provides specifications and settings lists. XII Settings Data Notation The letters of the alphabet in settings data are displayed as shown below. a b c d e f g h i j k l m A B C D E F G H I J ...
- マニュアル
...ASCII Character Hex. @ 40 A 41 B 42 C 43 D 44 E 45 F 46 G 47 H 48 I 49 J 4a K 4b L 4c M 4d N 4e O 4f ASCII Character Hex. P 50 Q 51 R 52 S 53 T 54 U 55 V 56 W 57 X 58 Y 59 Z [ 5a 5b \ 5c ] ^ 5d 5e _ 5f ASCII Character Hex. ` 60 a 61 b 62 c 63 d 64 e 65 f 66 g 67 h 68 i 69 j 6a ...
- マニュアル
...Ports 4 ports Communications Protocol CompoWay/F, Modbus RTU Maximum Connections 31 devices for 1 port (total for the device: 31 devices 4 ports = 124 devices) Terminal Resistor Built-in (120 ) Communication Speed 9.6 ...
- マニュアル
...- . / 0 1 2 3 4 5 6 7 8 9 : ; < = > ? @ A B C D E F G H I J K L M N O P Q R S T U V W X Y Z [ ¥ ] ^ _ ` a b c d e f g h i j k l m n o p q r s t u v w x y z { | } ~ 4-90 4 Operations of Setup & Management Tool EQ-Manager 4.6.4.7 EQ100 RS-485 Communications Port Setting To connect an RS-485-connected measurement device to EQ100, you must configure RS-485 communications ports....
- マニュアル
...- . / 0 1 2 3 4 5 6 7 8 9 : ; < = > ? @ A B C D E F G H I J K L M N O P Q R S T U V W X Y Z [ ¥ ] ^ _ ` a b c d e f g h i j k l m n o p q r s t u v w x y z { | } ~ 4-94 4.Operations of Setup & Management Tool EQ-Manager EQ100 RS-485 Communications Port Setting To connect an RS-485-connected measurement device to EQ100, you must configure RS-485 communications ports. Specify the communications conditions ...
- マニュアル
...CT4 ̶ ̶ ̶ • Connect the CT cables for CT1/CT2/CT3/CT4 to the terminals on the main unit that are labeled CT1/CT2/CT3/CT4. • For details about how to wire the CTs,connect the S1 terminal to the CT power supply side (...
- マニュアル
... and wire type Measuring circuits • Connect the CT cables for CT1/CT2/CT3/CT4 to the terminals on the main unit that are labeled CT1/CT2/CT3/CT4. • For details about how to wire the CTs,connect the S1 terminal to the CT power supply side (...
- マニュアル
... Components 2-2 Nomenclature and Functions of the K6CM Device 2-2 Nomenclature and Functions of the K6CM Device 2-2-1 K6CM Device (G) 2 (A) 2-2-1 K6CM Device (B) (C) (D) (K) (J) (E) (I) (F) (H) (G) Symbol Name (A) Upper terminal (B) Function Connect Push-in Plus terminals. Refer to Push-In Plus Terminals Layout on page 2-5 later in this document for details. Alarm bar dis- During monitoring, the following colors are displayed.*1 play • Green: Alarm status (normal) • Yellow: Alarm status (warning) • Red: Alarm status (critical) Turns OFF when one ...