全 5559 件が検索されました。(1721 - 1740件を表示)

  • マニュアル

    ...:Windows7) USB cable (USB 2.0 type B connector) Ethernet cable (with industrial Ethernet connector) Sensor Communications Unit (EtherCAT slave) Fiber Sensor Model NJ501-1500 NJ1W-PA3001 SYSMAC-SE2[][][] Version Ver.1.01 XS5W-T421-[]M[]-...

  • マニュアル

    ...Version Date see in the Watch Tab Page as shown in the right figure and 1 . 3 1 2 0 1 1 / 0 8 / 0 1 CR check them. Space *The response data differ Delimiter O K CR depending on the device used. Delimiter *Refer to 9.2. Destination Device Command for details on the command. 24 8. Initialization Method 8. Initialization Method This document explains the setting procedure from the factory default setting. If the device settings have been changed from the factory default setting, some settings may not be applicable as described in this procedure. 8.1. Controller...

  • マニュアル

    ...- DS-Bus Model CJ1W-NCF82 CJ2M-CPU12 CJ1W-PA202 CXONE-AL[][]C-V4 /AL[][]D-V4 (Included in CX-One) - Version Ver.1.3 Ver.2.0 Ver.4.[][] Ver.9.43 XS5W-T421-[]M[]-K E3NW-ECT Ver.1.0 E3NW-DS E3NX-FA0 - Ver.1.0 Ver.1.0 Precautions for Correct Use The connection line of EtherCAT communication cannot be shared with other Ethernet networks. Make sure to directly connect the PLC to the destination device with the Ethernet cable. Please use the cable (double shielding with aluminum tape and braiding) of Category 5 or higher, ...

  • マニュアル

    ...OMRON Fiber Amplifier E3NX-FA0 Ver.1.0 - DS-Bus communications cable - OMRON OMRON OMRON Model NJ501-1500 Version Ver.1.04 NJ-PA3001 SYSMAC-SE2[][][] - Ver.1.05 XS5W-T421-[]M[]-K Precautions for Correct Use The connection line of EtherCAT communication cannot be shared with other Ethernet networks. Make sure to directly connect the Controller to the destination device with the Ethernet cable. Please use the cable (double shielding with aluminum tape and braiding) of Category 5 or higher, and use the shielded connector of Category 5 or higher. Connect the cable shield to the connector hood at ...

  • マニュアル

    ... Controller (Camera 2ch type) Camera Camera cable Monitor (analog RGB monitor) Monitor conversion cable USB connected mouse Model NJ501-1500 NJ-PA3001 SYSMAC-SE2[][][] - - Version Ver.1.06 Ver.1.07 XS5W-T421-[]M[]-...

  • マニュアル

    ...(Supplied with Sensor Head) OMRON 24 VDC power supply S8VS-06024 OMRON OMRON OMRON OMRON NJ-PA3001 SYSMAC-SE2[][][] W4S1-05C - Version Ver.1.10 Ver.1.15 Ver.1.00 XS5W-T421-[]M[]-K ZW-7000 Rev.1.0 (for Sensor Controller) (DC24V 2.5A 60W) Precautions for Correct Use The connection line of EtherCAT communications cannot be shared with other Ethernet networks. Do not use devices for Ethernet such as a switching hub. Use the Ethernet cable (double shielding with aluminum tape and braiding) of Category 5 or higher, and use the shielded connector of Category 5 ...

  • マニュアル

    .../O power supply (24 VDC) IO-Link Photoelectric Sensor E3Z-D82-IL3 2M Model NJ501-1500 Version Ver.1.12 NJ-PA3001 SYSMAC-SE2[][][] (Included in Sysmac Studio) - Ver.1.16 Ver.2.2 XS5W-T421-[]M[]-K NX-ECC202 Ver.1.2 NX-ILM400 Ver.1.0 E3Z-D82-IL3 2M Ver.1.00 Precautions for Correct Use The connection line of EtherCAT communications cannot be shared with other Ethernet networks. Do not use devices for Ethernet such as a switching hub. Use an Ethernet cable (double shielding with aluminum tape and braiding) of Category 5 or higher, ...

  • マニュアル

    .../O power supply (24 VDC) IO-Link Proximity Sensor E2E-X3B4-IL3 2M Model NJ501-1500 Version Ver.1.12 NJ-PA3001 SYSMAC-SE2[][][] (Included in Sysmac Studio) - Ver.1.16 Ver.2.2 XS5W-T421-[]M[]-K NX-ECC202 Ver.1.2 NX-ILM400 Ver.1.0 E2E-X3B4-IL3 2M Ver.1.00 Precautions for Correct Use The connection line of EtherCAT communications cannot be shared with other Ethernet networks. Do not use devices for Ethernet such as a switching hub. Use an Ethernet cable (double shielding with aluminum tape and braiding) of Category 5 or higher, ...

  • マニュアル

    ...-series IO-Link Master Unit Unit power supply (24 VDC) I/O power supply (24 VDC) IO-Link Photoelectric Sensor E3Z-D82-M1TJ-IL3 Model NJ501-1500 NJ-PA3001 SYSMAC-SE2[][][] (Included in Sysmac Studio) XS5W-T421-[]M[]-...

  • マニュアル

    .../O power supply (24 VDC) IO-Link Proximity Sensor E2E-X3B4-M1TJ-IL3 Model NJ501-1500 Version Ver.1.12 NJ-PA3001 SYSMAC-SE2[][][] (Included in Sysmac Studio) - Ver.1.16 Ver.2.2 XS5W-T421-[]M[]-K GX-ILM08C Ver.1.0 E2E-X3B4-M1TJ-IL3 Ver.1.00 Precautions for Correct Use The connection line of EtherCAT communications cannot be shared with other Ethernet networks. Do not use devices for Ethernet such as a switching hub. Use an Ethernet cable (double shielding with aluminum tape and braiding) of Category 5 or higher, and use a shielded connector ...

  • マニュアル

    ... up the communication speed. ON 1 2 3 4 Set the communication rate of the master unit to 125K bps. In this example, switches 1 and 2 are set to OFF. Pin Baud Rate 1 2 OFF OFF 125 K bit/s ON OFF 250 K bit/s OFF ON 50 ...

  • マニュアル

    .../Cancel of of bits/coils bits/coils are are enabled enabled in in the the same same way. way. Shortcut Key Shortcut Key Ctrl+J: Ctrl+J: Force Force On On Ctrl+K: Ctrl+K: Force Force Off Off Display Project Workspace. [Alt] + 1 Double-click [Memory]. Click the [Address] tab. Double-click [Forced Status]. 2-11 mark indicates that the bit is now being forced on/off. Once bits/coils are forced on/off, the forced statuses are held until cancelled or the reverse procedures of on/off are taken. The statuses do not change by an external ...

  • マニュアル

    ....ia.omron.com Regional Headquarters OMRON EUROPE B.V.(Representative and Importer in EU) Wegalaan 67-69, 2132 JD Hoofddorp,The Netherlands Tel: (31)2356-81-300/Fax: (31)2356-81-388 OMRON Electronics Ltd. Opal Drive, Fox Milne, Milton Keynes MK15 0DG, U....

  • マニュアル

    ....ia.omron.com Regional Headquarters OMRON EUROPE B.V.(Representative and Importer in EU) Wegalaan 67-69, 2132 JD Hoofddorp,The Netherlands Tel: (31)2356-81-300/Fax: (31)2356-81-388 OMRON Electronics Ltd. Opal Drive, Fox Milne, Milton Keynes MK15 0DG, U....

  • マニュアル

    ... 3 times the load voltage Average rectified current:1A When both set(IN1) and reset(IN2)signals are input simultaneously.The set input takes precedence over the reset input. NC(6) NO(5) COM(4) OUTPT RELAY CONTACT (S3D2-□...

  • マニュアル

    ...クキラーを使用していただくようお願いします。 COM(4) センサ1 センサ2 ■出力のリレー接点 について (S3D2-□K□) NO(5) ・形S3D2-BK/フリップフロップ動作 センサ1 S3D2-□□Bタイプ NC(6) 3 ON (IN1:ワイヤードOR) OUT1(5) T T 形S3D2-AK/-AKD 茶 OFF COM(4) T センサ2個の場...

  • マニュアル

    ... display related to a branch output (outputs 1 to 6). (See note 2.) J Unit Indicator (Orange) Lights or flashes when there is a unit (e.g., V, A, Yrs, °C, s) related to the value shown on the 7-segment display. ...

  • マニュアル

    ... in parallelo /Conmutador de operación en paralelo オムロン株式会社 Precauzioni per l'utilizzo corretto R ⌘˖ 1.ཆ䜘⭥ⓀѪ4.5㠣12.5Vᰦˈᰐ䴰䲀⍱⭥䱫RDŽཆ䜘⭥ⓀѪ12.5 㠣24.5Vᰦˈ䈧ᨂ‫ޕ‬K¡Ⲵ䲀⍱⭥䱫RDŽ 2.䘎᧕ಘ৽ੁ䘎᧕ਟ㜭Պᦏൿ޵䜘‫ݳ‬ಘԦDŽ 3.+RC઼-RCㄟᆀᱟ⭥ⓀⲴҼ⅑⭥䐟DŽ䈧֯⭘SELV䗃ࠪ⭥Ⓚ֌ Ѫཆ䜘⭥ⓀDŽ䚕᧗⭥䐟о⭥ⓀⲴҼ⅑䗃ࠪ㔍㕈˄࣏㜭㔍㕈˅DŽ / IT Descripción ķ ...

  • マニュアル

    ... measures to reduce interference.  Pollution degree 3: Branch Output Terminal (−) (Class 2 Output) 4: NC 2  Conformance to EU and UK Directives Max. 70°C at 58.3% load, 45°C at 100% load (>45°C Load derating: 1.67%/...

  • マニュアル

    ... isolating transformer: 3. Rated maximum ambient temperature: Ta=40°C *1 *3 *1 *3 *2 *1 Ambient temperature / Surrounding Air Temperature Max. 55°C at 80% load, 40°C at 100% load (>40°C Load derating: 1.33%/...