全 5559 件が検索されました。(1561 - 1580件を表示)

  • マニュアル

    ... 0.044 (m) D Reflective floor 6-3. Safety Distance How to calculate the safety distance specified by International Standard ISO 13855(European standard EN ISO 13855)(Reference) If a person approaches the detection zone of the F3SJ-B-01T perpendicularly S = ...

  • マニュアル

    ... 0.044 (m) D Reflective floor 6-3. Safety Distance How to calculate the safety distance specified by International Standard ISO 13855(European standard EN ISO 13855)(Reference) If a person approaches the detection zone of the F3SJ-B-01TS perpendicularly S = ...

  • マニュアル

    ... 0.044 (m) D Reflective floor 6-3. Safety Distance How to calculate the safety distance specified by International Standard ISO 13855(European standard EN ISO 13855)(Reference) If a person approaches the detection zone of the F3SJ-B-02TS perpendicularly S = ...

  • マニュアル

    ...[0631530-0K] F3SP-B1P コントロールユニット 取扱説明書 (日/英語) © OMRON Corporation 2004-2022 All Rights Reserved. 0631530-0 K 規格 センサ用コネクタ ●警告表示の意味正しい取扱いをしなければ、この危険のために、軽傷・中程度の傷害を負ったり、万一の場合には重傷や死亡に至る恐れ...

  • マニュアル

    ...替時に再認識処理が発生すると、計測時間が延びるなどの影響があります。 ② ③ ④ G H I A ⑤ ⑥ J B K ⑪ ⑦ C ⑧ ⑫ ⑨ ⑬ ⑩ D E ⑭ L F コネクタの名称 内容 A SDメモリカード装着コネクタ SDメモリカードを装着します。 計測稼働中にSDメモリカードを抜き差ししな...

  • マニュアル

    ... of connecting the sensor controller and monitor with a switcher and splitter: ・Do not use devices that may require re-recognition of the monitor by the sensor controller. Re-recognizing the monitor during switch may slow the inspection speed down. J B ...

  • マニュアル

    ...30.) 19 Shield braid misalignment The shield braid of the connector cable peeks out from the connector. The cable sheath shifted due to excessive repetitive bending. Is the cable repeatedly bent from the connector part? XS5W-T421GMC-...

  • マニュアル

    ...Constant-current: G3PW-A2@@EC-@-FLK Phase control, optimum cycle control, and ON/OFF control G3PW-A220E@-@-@@@: 20 A G3PW-A245E@-@-@@@: 45 A G3PW-A260E@-@-@@@: 60 A 4 to 20 mA DC (Input impedance: 100 Ω) 1 to 5 V (Input impedance: 30.1 ...

  • マニュアル

    ...接続してください。 お断りなく仕様などを変更することがありますのでご了承ください。 ,0'--2 G5 Series AC Servomotors (Model: R88M-K@/-KP@/-KH@) AC Servo Drives (Model: R88D-KT@/-KN@/-KE@) INSTRUCTION SHEET Thank you for purchasing this OMRON product. Please read this Instruction Sheet and the User’s Manual, and thoroughly familiarize yourself with the functions and characteristics of the product before use. Be sure you are using the most recent version of ...

  • マニュアル

    ... Supply that is connected to the product from I/O Power Supply that is for load. (14) Be sure to warm up more than 30 minutes before you use. 9 ↑ON * 1 Exceptions in accuracy Accuracy Input Type and Condition Input Type ...

  • マニュアル

    ... one EU. Parameter Notation The following table shows the alphabet notation used for parameter abbreviations and settings displayed on the E5ZN-SDL Setting Display Unit. vi a b c d e f g h i j k l m A B C D E F G H I J ...

  • マニュアル

    ... symbols displayed on the displays and alphabet characters. a A b B c C d D e E f F g G h H i I j J k K l L m M n N o O p P q Q r R s S t T u U V w x V W X y Y z Z xi About this Manual: Purpose ● Overview ● Setup ● Basic Operations ● Operations for Applications ● Appendices xii Relevant section Details Section 1 introduces the features, components, and main specifications of the E5CSV/E5CS-U Digital Temperature Controllers. Section 2 describes the work...

  • マニュアル

    ... or ±1°C, (±0.2% of indication value or ±0.8°C, thermometer input whichever is greater) ±1 digit max. whichever is greater) ±1 digit max. Analog input (±0.5% FS) ±1 digit max. (±0.2% FS) ±1 digit max. Thermocouple input ...

  • マニュアル

    ... becomes the minimum scaling unit. xviii How to Read Display Symbols The following tables show the correspondence between the symbols displayed on the displays and alphabet characters. The default is for 11-segment displays. a b c d e f g h i j ...

  • マニュアル

    ...°C/−199.9 to 900.0°F) Pt (0.0 to 100.0°C/0.0 to 210.0°F) JPt (−199.9 to 500.0°C/−199.9 to 900.0°F) JPt (0.0 to 100.0°C/0.0 to 210.0°F) K (−200.0 to 1300.0°C/−300.0 to 2300.0°F) K (−20.0 to 500.0°C/0.0 to 900.0°F) J (−100.0 to 850.0°C/−100.0 to 1500.0°F) J (−20.0 to 400.0°C/0.0 to 750.0°F) T (−...

  • マニュアル

    ...Conventions Used in This Manual How to Read Display Symbols The following tables show the correspondence between the symbols displayed on the displays and alphabet characters. a b c d e f g h i j k l m A B C D E F G H I J ...

  • マニュアル

    ... for FAQs: E5CC/E5EC Setting the Sensor Type Select and set the sensor type (i.e., the Input Type parameter) to the set value that corresponds to the type of sensor used in the application and the required temperature range. The parameter is set to 5 (...

  • マニュアル

    ...Conventions Used in This Manual How to Read Display Symbols The following tables show the correspondence between the symbols displayed on the displays and alphabet characters. a b c d e f g h i j k l m A B C D E F G H I J ...

  • マニュアル

    ....0°C/0.0 to 210.0°F) H'00000003 (3): JPt (−199.9 to 500.0°C/−199.9 to 900.0°F) H'00000004 (4): JPt (0.0 to 100.0°C/0.0 to 210.0°F) H'00000005 (5): K (−200 to 1300°C/−300 to 2300°F) H'00000006 (6): K (−20.0 to 500.0°C/0.0 to 900.0°F) H'00000007 (7): J (−100 to 850°C/−100 to 1500°F) H'00000008 (8): J (−20.0 to 400.0°C/0.0 to 750.0°F) H'00000009 (9):...

  • マニュアル

    ...Conventions Used in This Manual How to Read Display Symbols The following tables show the correspondence between the symbols displayed on the displays and alphabet characters. a b c d e f g h i j k l m A B C D E F G H I J ...