全 41926 件が検索されました。(1381 - 1400件を表示)

  • マニュアル

    ...(122) Operands 000000 0050 D02000 0002 SVs Completion Flags S CIO 0002 0 1 5 5 CIO 005000 S+1 CIO 0003 2 5 0 6 CIO 005001 S+2 CIO 0004 1 0 2 9 CIO 005002 S+3 CIO 0005 6 0 4 7 CIO 005003 S+4 CIO 0006 4 1 0 6 CIO 005004 S+5 CIO 0007 7 9 1 0 CIO 005005 S+6 CIO 0008 1 0 5 0 CIO 005006 S+7 CIO 0009 9 8 0 0 CIO 005007 5-13-6 COUNTER: CNT Ladder Symbol CP R Operand Data ...

  • マニュアル

    ...(06) is an instruction that causes a non-fatal error. The following will occur when an FAL(06) instruction is executed: 1, 2, 3... 1. The ERR/ALM indicator on the CPU Unit will flash. PC operation will continue. 2. The instruction’...

  • マニュアル

    ... the PC. FAL(06) is an instruction that causes a non-fatal error. The following will occur when an FAL(06) instruction is executed: 1. The ERR/ALM indicator on the CPU Unit will flash. PC operation will continue. 2. The instruction’...

  • マニュアル

    ... can be sent each time the instruction is executed. • The bytes of source data shown below will be sent in the following order. If most significant bytes first is specified (0): 12345678.. If least significant bytes first is specified (1): 21436587.. S S+1 ...

  • マニュアル

    ... 3 hex 0 (0 hex) Decimal point position (from right) for instantaneous value when 100% input --- Bit 04 to 07: 0 to 4 hex 0 (0 hex) Instantaneous value time unit (matching conversion period) 0: 1 s; 1: 3 ...

  • マニュアル

    ... and receiving responses. The data that is sent and received is all hexadecimal unless otherwise noted. 160 Section 6-4 FINS Commands and Responses 1 byte @CMND Command S 1 byte Word 15 S S+1 S+2 87 0 D C 1 byte Word 15 D D+1 D+2 Response 2 bytes 1 byte 87 0 2,000 bytes max. FINS header Controller Link Unit Automatically pre- Command code pared and added. CPU Unit Text Computer CS, CVM1, CV-series, or CQM1Hseries PLC Command Controller Link Support Board Response 2 bytes 2 bytes 1,998 bytes max....

  • マニュアル

    ...FAL(06) is an instruction that causes a non-fatal error. The following will occur when an FAL(06) instruction is executed: 1,2,3... 1. The ERR indicator on the CPU Board will flash. PLC operation will continue. 2. The instruction’...

  • マニュアル

    ... note a.) Tag name Link number Comment Comment from user link table (only through 24th character) Number of links Automatically set by system (number of tags referenced) Cycle Refresh cycle (0 to 8) (0: System common operating cycle, 1: 0.01 ...

  • マニュアル

    ...Master’s node number: 63 Slave’s network address: 1 Slave’s node number: 2 Section 6-3 Explicit Message Communications CMND(194) Operand Details [CMND S D C] • Command Words Word S S+1 S+2 S+3 S+4 S+5 Contents Function (Hex) 28 01 EXPLICIT MESSAGE SEND command code = 2801 (Hex) 02 1C Slave node number = 02 (Hex) READ BYTE DATA command service code = 1C (Hex) 00 2F Class ID = 002F (Hex) 00 01 Instance ID = 0001 (Hex) specifies data area 0A 00 Starting read address = 000A (Hex) specifies IR 010 Address L = 0A (Hex); Address ...

  • マニュアル

    ...(06) is an instruction that causes a non-fatal error. The following will occur when an FAL(06) instruction is executed: 1,2,3... 1. The ERC indicator on the Customizable Counter Unit will flash. Operation will continue. 2. The instruction’...

  • マニュアル

    ...C S S D D Local node S 1st response word Remote Master Unit CPU Unit Interpretation1 Interpretation2 Command data Response No. of command bytes Response Response monitoring time ...... S+2 S+3 S+4 Command Destination node Local Master Unit CPU Unit S+1 Operands C: Control code S: 1st source word D: Destination information Execution L Execution ... Response data 1: For commands addressed to Master Unit 2: For commands addressed to CPU Unit Description IOWR transfers data from the words beginning at S to the specified Special I/ O Unit. The control code (C) specified parameters for the ...

  • マニュアル

    ... byte, IN size: 3 bytes Node address 2: OUT size: 1 byte, IN size: 2 bytes 15 Allocation size setup table I 1 5 s I+1 4 3 s+1 I+2 1 2 s+2 : : s+3 OUT block 1 15 k 00 00 01 01 k+1 00 00 01 01 k+2 02 k+3 Not usable : k+4 00 Not usable 01 01 Not usable 01 02 k+5 l: First word of the allocation size setup table s: First word of OUT block 1 k: First word of IN block 1 Note 00...

  • マニュアル

    ... the remote node. If the response is not be received within the response time, the request is timed out. The Message Monitoring Timer Service API functions are used to set the message monitoring timer for each remote device. The default message time is 2 ...

  • マニュアル

    ... ON, XFER(70) copies the contents of S, S+1, ..., S+N to D, D+1, ..., D+N. S D 3 4 5 2 3 4 5 2 S+1 D+1 3 4 5 1 3 4 5 1 S+2 D+2 3 4 2 2 3 4 2 2 S+N D+N 6 4 5 2 6 4 5 2 Note XFER(70) can be used to shift data by setting the operands so that data is moved between overlapping areas. 35 Section Data Movement Instructions 2-7 N Equal to 9999 When the execution ...

  • マニュアル

    ...: CCW Pulse output method (See note.) 0 hex: CW/CCW 1 hex: Pulse + direction Always 0 hex. Note: Use the same pulse output method when using both pulse outputs 0 and 1. S: First Word of Settings Table The content of S to ...

  • マニュアル

    ... 6WDWXV &RQWDLQVVWDWXVUHDGIURP7HPSHUDWXUH&RQWURO OHU ‡ 7DUJHWWHPSHUDWXUH &RQWDLQV Note The decimal point position has to be managed by the user since the Temperature Controller’s decimal point position is not transferred in SYSWAY (X format) communications. Status (Offset: +2 and +10) The read data area’...

  • マニュアル

    ... before operation is started) is possible CX-Process Tool or FINS command. Standard: Operation of all function blocks is executed at the same operation cycle preset to ITEM 004 in the System Common block. Settable operation cycles: 0.1 s, 0.2 s, 0.5 s, 1 ...

  • マニュアル

    ... s: 50 h 10 min: 300 days 10 s: 100 h 30 min: 900 days 30 s: 300 h 60 min: 1,800 days Collection cycle Data display Horizontal axis Collection cycle 1 min: 2 h to 10 days 1 s: 2 min to 240 min 5 min: 10 h to 50 days 2 s: 4 min to 240 min 10 min: 20 h to 100 days 5 s: 10 min to 240 min 30 min: 60 h to 300 days 10 s: 20 min to 240 min 60 min: 5 days to 600 days 30 s: 20 min ...

  • マニュアル

    ... because the input is ON twice when a measurement is taken. Measured approx. every 1 s ON OFF 0.5 s Figure B ■ Measuring an ON Time of 1.5 s In Figure C, the actual ON time is 3 s (2 × 1.5 s) but the total ON time is measured as 4 s because the input is ON 4 times when a measurement is taken. 507 Section 11-3 Functions of Digital I/O Slave Units Measured approx. every 1 s ON OFF 1.5 s Figure C Settings Using the CX-Integrator 1,2,3......

  • マニュアル

    ... the System Common Block (block model 000) ITEM type ITEM Data contents Data range Default Parameter 050 HMI EM bank number 0 to C (Hexadecimal) 0 051 HMI function's operation cycle (s) 1 (0.1 s), 2 (0.2 s), 3 (0.5 s), 4 (1 s), or 5 (2 s) Note: Always stop operation before changing this ITEM. 1 to 5 4 (1 s) 056 Reception stop switch 0: Normal; 1: Stop reception 0 or 1 0 057 Transmission stop switch 0: Normal; 1: Stop transmission 0 or 1 0 059 HMI function disable switch 0: Used; ...