全 41926 件が検索されました。(1361 - 1380件を表示)
- マニュアル
...電流1mA以下 耐電圧 10∼150Hz、複振幅1.5mmの振動を X,Y,Z各方向に1掃引8分間で2掃引印加し異常ないこと 300m/s 2 の衝撃をX,Y,Z各方向に各3回計18回印加し異常ないこと 耐振動耐衝撃 保護構造ケーブル長 IEC60529規格 IP40 0.1m 中継ケーブ...
- マニュアル
...(63) copies bit column C from the 16-word set (S to S+15) to the 16 bits of word D (00 to 15). 133 Section 5-14 Data Movement C Bit 15 Bit 00 S S+1 S+2 S+3 . . . 0 0 0 0 1 1 1 0 0 0 1 0 0 0 0 1 S+15 0 1 1 1 0 0 0 1 1 0 0 0 1 0 1 0 1 1 0 1 0 0 1 0 0 1 1 1 0 0 0 1 0 0 0 1 1 0 1 ...
- マニュアル
...act PC設erm:{noぎma目yOi)en)iRpvS − Relayladtierterm:normailycloseCtc◎ntact PC言efm:{normallyciosξ≧d}input −〇 ReiayiadCierterrri:coii PCteぎm:oUtput Whenyouhave掴shedwr聲ingyo剖adderdiagram,thenex重stepisto encotiethediagram;nt。 alanguagethatthePCcanvnCierstand・ ...
- マニュアル
...Word l+1 : Word l+16 DM Area Command Allocations DM Wd 118 b15-b12 b11-b8 b7-b4 s 0 3 0 4 s+1 1 0 0 0 s+2 1 0 1 0 s+3 1 0 5 0 s+4 1 0 6 0 b3-b0 Application Program Examples Section 8-4 DM Area Data Allocations DM Wd b15-b12 b11-b8 b7-b4 b3-b0 r 1 0 0 4 r+1 0 0 0 0 r+2 0 0 0 0 r+3 0 1 7 7 r+4 0 5 4 4 r+...
- マニュアル
... ON, XFER(70) copies the contents of S, S+1, ..., S+N to D, D+1, ..., D+N. S D 3 4 5 2 3 4 5 2 S+1 D+1 3 4 5 1 3 4 5 1 S+2 D+2 3 4 2 2 3 4 2 2 S+N D+N 6 4 5 2 6 4 5 2 ER: Flags N is not BCD S and S+N or D and D+N are not in the same data area. Indirectly addressed DM word is non-existent. (Content of *DM word is not ...
- マニュアル
...>9.9 µs >9.5 µs >9.9 µs >9.8 µs >9.9 µs >9.8 µs <100 Kpps >4.6 µs >4.9 µs >4.9 µs >4.8 µs >4.9 µs >4.8 µs <200 Kpps >2.4 µs >2.1 µs >2.4 µs >2.3 µs >2.4 µs >2.4 µs <250 Kpps >1.9 µs >1.5 µs >1.9 µs >1.8 µs >1.9 µs >1.9 µs Note Specifications other than those above correspond to the output specifications of the preceding page. 243 Appendix C Standard Models Product ...
- マニュアル
... the contents of S, S+1, ..., S+N–1 to D, D+1, ..., D+N–1. Flags S D 3 4 5 2 3 4 5 2 S+1 D+1 3 4 5 1 3 4 5 1 S+2 D+2 3 4 2 2 3 4 2 2 S+N–1 D+N–1 6 4 5 2 6 4 5 2 ER: N is not BCD S and S+N–1 or D and D+N–1 are not in the same data area. Indirectly addressed DM word is non-existent. (Content of *DM word...
- マニュアル
... executed. When the execution condition is ON, CTW(63) copies bit column C from the 16-word set (S to S+15) to the 16 bits of word D (00 to 15). C Bit 15 Bit 00 S S+1 S+2 S+3 . . . 0 0 0 0 1 1 1 0 0 0 1 0 0 0 0 1 S+15 0 1 1 1 0 0 0 1 1 0 0 0 1 0 1 0 1 1 0 1 0 0 1 0 0 1 1 1 0 0 0 1 0 0 0 1 1 ...
- マニュアル
..., 2, 3... FAL(06) is an instruction that causes a non-fatal error. The following will occur when an FAL(06) instruction is executed: 1. The ERR/ALM indicator on the CPU Unit will flash. PC operation will continue. 2. The instruction’...
- マニュアル
...(70) copies the contents of S, S+1, ..., S+N to D, D+1, ..., D+N. ER: S 3 4 5 2 D 3 4 5 2 S+1 3 4 5 1 D+1 3 4 5 1 S+2 3 4 2 2 D+2 3 4 2 2 S+N 6 4 5 2 D+N 6 4 5 2 N is not BCD S and S+N or D and D+N are not in the same data area. Indirectly addressed DM word is non-existent. (Content of *DM word is not BCD, or the ...
- マニュアル
... ON, XFER(70) copies the contents of S, S+1, ..., S+N to D, D+1, ..., D+N. S D 3 4 5 2 3 4 5 2 S+1 D+1 3 4 5 1 3 4 5 1 S+2 D+2 3 4 2 2 3 4 2 2 S+N D+N 6 4 5 2 6 4 5 2 161 Section 5-16 Data Movement Flags ER: N is not BCD between 0000 and 2000. S and S+N or D and D+N are not in the same data area. Indirectly addressed DM ...
- マニュアル
...+1, ..., D+N. XFER(70) can thus be used to shift data in memory. Description Precautions S D 3 4 5 2 3 4 5 2 S+1 D+1 3 4 5 1 3 4 5 1 S+2 D+2 3 4 2 2 3 4 2 2 S+N D+N 6 4 5 2 6 4 5 2 S and S+N must be in the same data area, as must D and D+N. DM 6144 to DM 6655 cannot be used for D. Flags ER: N is not BCD S and S+N ...
- マニュアル
...Word n+1, bit 2 Y1 Sets first RAM address a in S Write source first address First RAM address B Data Data Sets parameters and conversion data in S+1 Sets parameters and conversion data in S+2 Writes data from m words starting from S+1 to the addresses starting from a in the Analog Output Unit. (= Flag) 159 Section Data Exchange with CPU Unit 9-3 Four-word Operating Mode Writing Data 1, 2, 3... 1. The CPU Unit uses MOV or another similar instruction to set data in word n of the allocated I/O words....
- マニュアル
... IP67 construction. Do not attempt to use the Water-resistant Terminals for applications where the Water-resistant Terminals are always underwater. 3. The Unit is a plastic resin mold product. Do not tread on the Unit or put objects on the Unit. OMRON’...
- マニュアル
... not be executed. S actually contains the number of words to be sent and S+1 and the following words contains the actual data to be sent, as shown in the following diagram. S: No. of send words S+1: Send data ...
- マニュアル
... following diagram shows the data format for sending FINS commands and receiving responses. The data that is sent and received is all hexadecimal unless otherwise noted. 1 byte @CMND Command S D C Word 15 S S+1 ...
- マニュアル
..., 2, 3... FAL(06) is an instruction that causes a non-fatal error. The following will occur when an FAL(06) instruction is executed: 1. The ERR/ALM indicator on the CPU Unit will flash. PC operation will continue. 2. The instruction’...
- マニュアル
...(06) 1, 2, 3... FAL(06) is an instruction that causes a non-fatal error. The following will occur when an FAL(06) instruction is executed: 1. The ERR indicator on the SRM1 will flash, but operation will continue. 2. The instruction’...
- マニュアル
... register No. in the leftmost byte of S+5. Setting location Set 2804 hex in controller data s of the CMND(490) instruction. Set 0210 hex in controller data s+1 of the CMND(490) instruction. Set 0002 hex in controller data ...
- マニュアル
...Command Words (S: First Command Word) Word Contents (Hex) Meaning S 28 01 S+1 02 1C EXPLICIT MESSAGE SEND command code: 28 01 Hex Slave node address: 2 BYTE DATA READ command service code: 1C Hex S+2 S+3 00 2F 00 01 Class ID: 002F Hex Instance ID: For IR Area 1: 0001 Hex S+4 0A 00 S+5 28 00 Read start address: 10 = 000A Hex Address L: 0A Hex, Address H: 00 Hex No. of bytes of read data: 40 bytes = 28 Hex (The rightmost byte is not used.) D: Response Words (D: First ...