全 132 件が検索されました。(121 - 132件を表示)

  • マニュアル

    ...S No.: Bit memory table number S Hist: Execution/non-execution of bit status check (reading) for alarm history S #: Presence/absence of screen switching function S Table: Character-string memory table displayed in the alarm list/ history S ...

  • マニュアル

    ... area of CVM1/CV series PC is used exclusively for special application in the system, and cannot be used for other application. When Data Memory (DM) is specified, the bit number (00 to 15) is specified following the channel number. Example of setting: Table ...

  • マニュアル

    ... Area of CV series PC is used exclusively for special applications in the system, and cannot be used for other application. When specifying the DM Area, specify the bit number (00 to 15) along with the word address. Example of setting: Table entry ...

  • マニュアル

    ... by pressing the ”stop” touch switch. Updating of the trend graph display is also started at the same time. On the NTH25/NTH25C, the ”restart” touch switch operates on all data within a group. During sampling, the ”restart” (continue) touch switch is lit. ...

  • マニュアル

    ...the trend graph is redisplayed and logging restarts automatically. Restart (Continue) touch switch Restarts halted data sampling. At the same time, updating of the trend graph display restarts. 250 Graphs Section 6-9 During data sampling, the touch switch is lit. ...

  • マニュアル

    ... page (rewind)) After pressing the touch switch is pressed to return to a past display and then the (restart (continue)) touch switch is pressed to restart sampling, past data will not be displayed and the display of new data will start again. Example: ...

  • マニュアル

    ..., if the (previous page (rewind)) (restart touch switch is pressed to return to a past display and then the (continue)) touch switch is pressed to restart sampling, past data will not be displayed and the display of new data will start again. Example: ...

  • マニュアル

    ...PV 006 PV source designation --- --- --- PV_ABN 018 PV error contact source designation --- --- --- RSP 021 External ratio setting source designation PV 021 PV measured value --- --- --- SP_DSP 022 Set point --- --- --- MV_C 023 Manipulated variable SP 029 Current SP setting Abbreviation for analog input ITEMs ITEM number PV 006 PV_ABN Data Data 307 ITEM Notation in Block Diagrams 308 Appendix B Appendix C Setting Segment Programs A special input interface is provided for setting program patterns and bank data for Segment Program 2 (Block Model 157) and Segment Program 3 (Block Model 158) blocks. This section describes how to ...

  • マニュアル

    ... "i1-t: Input 1 input type" is "15: 4 to 20 mA". 15 l.0 inp.1 3. Press the M key repeatedly to select "inp.1: Scaling input value 1". Set to “5” with the UD keys. 5 l.0 dsp.1 4. Press the M key to select "...

  • マニュアル

    ...] Displays the current measuring cycle. p.260 500 to 10000 s (default value: 2000) Controller information [C.INFO] Software version [VER] MAC Address [MAC.ADR] Error history [ERR.LOG] Error history display [LOG....

  • マニュアル

    ...] Displays the current measuring cycle. p.334 500 to 10000 s (default value: 2000) Controller information [C.INFO] Software version [VER] MAC Address [MAC.ADR] Error history [ERR.LOG] Error history display [LOG....

  • ...アル Turbo PMAC のメモリ Turbo PMAC は、Y メモリと X メモリの、2 つのメモリ領域を使用する 24 ビットアーキテクチャを持つ、DSP(デジタル信号プロセッサ)を使用します。 メモリは M 変数を使って、 PMAC プログラム内でアクセスされます。 M 変数の定義に...