全 113 件が検索されました。(61 - 80件を表示)
- マニュアル
...電力量、積算進み・遅れ・総合無効電力量、簡易温度計測の初期値は off 0 は常時点灯単位:分 表示点灯時間 0~99 63.dsp 0 電圧誤結線検出簡 温度単位易温 温度補正値度設定 off、on c、f 64.v-e 65.d-u on c -50.0~50.0 t.ad 0.0 c:摂氏、単位:℃ f:華氏、単位:...
- マニュアル
...4 モードの構成とキー操作 設定範囲 off、on 第 2 表示 62.d.sl 初期値備考欄参照 表示点灯時間 0~99 63.dsp 0 電圧誤結線検出簡 温度単位易温度 温度補正値設定 off、on c、f 64.v-e 65.d-u on c -50.0~50.0 t.ad 0.0 備考計測モード各パラメータに...
- マニュアル
...the trend graph is redisplayed and logging restarts automatically. Restart (Continue) touch switch Restarts halted data sampling. At the same time, updating of the trend graph display restarts. 250 Graphs Section 6-9 During data sampling, the touch switch is lit. ...
- マニュアル
..., if the (previous page (rewind)) (restart touch switch is pressed to return to a past display and then the (continue)) touch switch is pressed to restart sampling, past data will not be displayed and the display of new data will start again. Example: ...
- マニュアル
...PV 006 PV source designation --- --- --- PV_ABN 018 PV error contact source designation --- --- --- RSP 021 External ratio setting source designation PV 021 PV measured value --- --- --- SP_DSP 022 Set point --- --- --- MV_C 023 Manipulated variable SP 029 Current SP setting Abbreviation for analog input ITEMs ITEM number PV 006 PV_ABN Data Data 307 ITEM Notation in Block Diagrams 308 Appendix B Appendix C Setting Segment Programs A special input interface is provided for setting program patterns and bank data for Segment Program 2 (Block Model 157) and Segment Program 3 (Block Model 158) blocks. This section describes how to ...
- マニュアル
...input [KEY.IN] TIMING/ RESET key input [KEY.IN] p.253 Controller information [C.INFO] Software version [VER] MAC Address [MAC.ADR] Error history [ERR.LOG] Error history display [LOG.DSP] Error clear [LOG.CLR] Energization time (h)*2 [RUN.TIM] Sensor head information [H.INFO] Off [OFF]*/On [ON] Displays the version. p.268 Displays the current MAC address. Clears/displays the error history. − No.01 to No.64 (default value: No.01) − OK [OK]/Cancel [CAN] − Energization time (h) Model [MODEL] Displays the model. Serial No. [SER.NO] Displays the serial No.. p.199 p.268 *1. For ...
- マニュアル
.... • You can confirm the error history on the Sensor Controller's digital display. To confirm the error history, set the FUNC mode and switch the following menu. 7 System setting [SYSTEM] - Controller information [C.INFO] - Error history [ERR.LOG] - Error history display Troubleshooting [LOG....
- マニュアル
... (DAC) — A VLSI circuit used to convert digitally processed images to analog for display on a monitor. Digital Imaging — Conversion of an image into pixels by means of an Analog-to-Digital Converter where the level of each pixel can be stored digitally. Digital Signal Processor (...
- マニュアル
... (DAC) — A VLSI circuit used to convert digitally processed images to analog for display on a monitor. Digital Imaging — Conversion of an image into pixels by means of an Analog-to-Digital Converter where the level of each pixel can be stored digitally. Digital Signal Processor (...
- マニュアル
... (DAC) — A VLSI circuit used to convert digitally processed images to analog for display on a monitor. Digital Imaging — Conversion of an image into pixels by means of an Analog-to-Digital Converter where the level of each pixel can be stored digitally. Digital Signal Processor (...
- カタログ
...形態−オペレーション 内容ユニットマニュアル/オートオペレーションプロテクトヒステリシスウィズス 略称 DSP AVE BAR AUT ECO 内容ディスプレイアベレージバーオートエコ 単位−キロパスカル Width(幅) A B C D E F G H I J K L M N O P Q R ...
- カタログ
...了後 ボタンを押すと、表示更新速度設定へ移行します。 表示更新速度設定測定値の表示更新速度を設定します。 ・ 「dSP」が表示されている状態で またはボタンを押して、表示更新速度を[s]を選び、 ボタンを押します。 ・全ての設定が完了し、測定モ...
- カタログ
...をフロント部にあるZEROキー操作にてワンタッチで調整できます。 ください。 表示値(g、kgなど) K 3 N V dsp.2 K 3 N R K 3 ※プロテクトメニューにて強制ゼロ 操作解除のときのみ有効 dsp.1 入力値(mV) A ●実入力値で設定可能 F スケーリング...
- カタログ
...性とワイドバリエーションで使いやすさを追及 ACサーボモータ ACサーボドライバ ●出力容量60Wから7200W。 ●高速DSPの採用により、制御系をオールディジタル化。 定格回転数も1200/2000/4000r/minと全30機種のラインアップ。 ●各種パラメータがフロント...
- カタログ
...像度1000本。 ちらつきのないプログレッシブスキャン方式。 新開発 1/2 インチ150万画素のオンチップ型CCDと新開発DSP搭載により、水平・垂直ともに解像度1000本を達成。 高繊細・高画質を追求しました。 シャッターを切った瞬間の映像をそのま...
- カタログ
...デル追加前 パターンサーチ 10,000回/分 高速ラインに対応 CPUとは別に独自のサーチ専用エンジンと画像処理用DSP(データ・シグナル・プロセッサ)を搭載。 画像取り込みとパターンサーチを並行処理するという画期的な手法で、高速化を実現...
- マニュアル
... 0 - 11 off mav.4 output 1 trl.1 TRL.1:Transfer lower limit M inp.2 off upper limit M -200.0 CH mav.1 trh.1 TRH.1:Transfer output 1 M dsp.1 dsp.2 sl-h SL-H:SP upper limit *1 *4 alt1 L less than 1 second M M M 1300.0 M off sbo.4 M M 4 ...
- マニュアル
... Auto shift mode setting of all channels is finished, if the button is pressed, it will shift to Setting of indication updating interval . Setting of indication updating interval Sets the interval to update the indication of measured value. • Press or button with [...
- マニュアル
...level1)withintherarigelto100%醐−scale. TheNo,1disp]ayindicat£s鐸ぱ‡『whe】ns¢ningthe-'`fixedSP"parameter. (〕tPeraLζi(}llmt)de(sett▲nglevel1) Par醐e総r −Sett量ng .ρ日銀麟SPmo(是 o:L◎c顧SP1:RemotcSP2:Fi賠...
- マニュアル
... 20 mA DC are scaled to 0.0 to 100.0°C. Input type (initial setting level: in-t): 4 to 20 mA DC (4-20) Scaling input value 1 (initial setting level: inp.1): 4 mA (4.00) Scaling display value 1 (initial setting level: ...