全 1430 件が検索されました。(1341 - 1360件を表示)

  • マニュアル

    ... the FG terminal is grounded. • If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. • Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...

  • マニュアル

    ... is equipped with an anti-chattering function, but if the chattering is 100 µs or longer, a faulty input may occur. (Input signals of 99 µs or shorter are ignored. Signals of 100 µs or longer are treated as input signals.) • Use no-contact output devices (...

  • マニュアル

    ... the FG terminal is grounded. • If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. • Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...

  • マニュアル

    ... that the FG terminal is grounded. • If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. • Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...

  • マニュアル

    ...The following alert symbols are used in this document. Cautions to indicate potential laser beam hazard Z5FP Setup Manual 5 INTRODUCTION INTRODUCTION Laser Safety WARNING Do not to expose your eyes to the laser radiation either directly or indirectly (i....

  • マニュアル

    ... that the FG terminal is grounded. • If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. • Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...

  • マニュアル

    ...4. Conforming Standards (1) European standards EN61496-1 (Type 4 and Type 2 ESPE), EN 61496-2 (Type 4 and Type 2 AOPD), EN61508-1 through -4 (SIL 3 for Type 4 and SIL 1 for Type 2), EN ISO 13849-1:2015 (PL ...

  • マニュアル

    ... FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(S) IS PROPERLY RATED AND INSTALLED FOR THE INTENDED USE WITHIN THE OVERALL EQUIPMENT OR SYSTEM. ...

  • マニュアル

    ... product in any of the following environments as the product may, in rare cases, be damaged. (a) Dusty area (b) Area with oil mist floating in the air (c) Area subject to impact or vibration (d) Area subject to sudden change in the ambient temperature (...

  • マニュアル

    ... product in any of the following environments as the product may, in rare cases, be damaged. (a) Dusty area (b) Area with oil mist floating in the air (c) Area subject to impact or vibration (d) Area with high humidity (of 85% RH or higher) (...

  • マニュアル

    ... Directives: Machinery Directive 2006/42/EC EMC Directive 2014/30/EU 4. Conforming Standards (1) European standards EN61496-1 (Type 4 ESPE), EN 61496-2 (Type 4 AOPD), EN61508-1 through -4 (SIL 3 for Type 4), EN ISO 13849-1:2015 (PL ...

  • マニュアル

    ... EC/EU Directives: Machinery Directive 2006/42/EC EMC Directive 2014/30/EU 4. Conforming Standards (1) European standards EN61496-1 (Type 4 ESPE), EN 61496-2 (Type 4 AOPD), EN61508-1 through -4 (SIL 3), EN ISO 13849-1:2015 (PL ...

  • マニュアル

    ... EC/EU Directives: Machinery Directive 2006/42/EC EMC Directive 2014/30/EU 4. Conforming Standards (1) European standards EN61496-1 (Type 4 ESPE), EN 61496-2 (Type 4 AOPD), EN61508-1 through -4 (SIL 3), EN ISO 13849-1:2015 (PL ...

  • マニュアル

    ... 3) Standards EN ISO 13849-2:2012 EN 62061:2005/A2:2015 (SIL CL 2) EN 61000-6-2:2005 EN 61000-6-3:2007 3) North American Standards: cULus: Listed (ANSI/UL 508, CSA C22.2 No.14) file number: E195653 E SCC-1224A Safety Mat / Edge Controller User Manual i Introduction Terms and Conditions Agreement Warranties (a) Exclusive Warranty. Omron's exclusive warranty is that the Products will be free from defects in materials and workmanship for a period of twelve months from the date of sale by Omron (or such other period expressed in writing by ...

  • マニュアル

    ... strong impact. ・ When inserting or removing an SD memory card, securely hold the product to prevent it from dropping, which may cause damage. Do the same when inserting or detaching an alarm output cable or connector. ・ Do not bring the product close to magnetic products (...

  • マニュアル

    ... ([Input image]), inspection/measurement ([Measurement]), image correction ([Compensate image]), inspection/measurement support ([Support measurement]), process branching ([Branch]), results external output ([Output result]), resulting image display ([Display result]), etc. You can freely classify processing items to handle a wide range of applications. Scene A scene (i....

  • マニュアル

    ... to the number of parameters. Response output Result of the command procedure can be returned to the system by setting the value on these variables. Variable name Type Content ResponseValue&() Array of Integers Response data Outputs the response data, i....

  • マニュアル

    ... DeviceNet Standard Master. Safety Logic Operations and Safety I/O Control Network Configurator Standard PLC Standard Master NE1A Safety Master Standard Slave Standard Slave Non-safety-related Control (Standard Control) The PLC system monitors the NE1A (i....

  • マニュアル

    ... Controller enables building a safety control system that satisfy the following: • Requirements for SIL 3 (Safety Integrity Level 3) in IEC 61508, IEC/EN 62061, Safety Standard for Safety Instrumented Systems (Functional Safety of Electrical/ Electronic/Programmable Electronic Safety-related Systems) • Requirements for PLe (Performance Level ...

  • マニュアル

    ...(カタログ番号 SGTA-702) 通信機能ユーザーズマニュアル(カタログ番号 SGTA-703) オムロン株式会社 OMRON Corporation 2006 All Rights Reserved. 0631762-0 E ̪ग़ࡱǻǡ੏̽ ●警告表示の意味 【取り扱い】 (1)ZENの使用環境は、IEC60664-1に基づく ”汚染度2 ”と”過電圧カテゴリⅡ ”です。 (2)使用周囲湿度...