全 1430 件が検索されました。(1321 - 1340件を表示)
- マニュアル
...4-29 4.8.6 Selecting the Bank Switching Method (F8) .................................. 4-30 4.8.7 Bank Copy (F9) ............................................................................ 4-31 E24 Detection Enable/Disable (F10) ........................................................ 4-32 APPENDICES Appendix A Appendix B Appendix C Appendix D Appendix ...
- マニュアル
..., V670-H51Q O’EIPA, KAI KOYPOΛHPΨ V670-CD1D O’EIPA SYMMOPF ONETAI ΠPOS TIS OYSIO∆EIS AΠAITHSEIS KAI TIS ΛOIΠES SXETIKES ∆IATAΞEIS THS O∆HΓIAS 1999/5/EK. Italian Con la presente Omron dichiara che la RFID Sistema, Antena V670-H11Serie, V670-H51 Serie, V670-H51Q Serie, ...
- マニュアル
... the FG terminal is grounded. • If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. • Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...
- マニュアル
... following readers. • • • • Persons in charge of introducing FA devices Persons who design FA systems Persons who install or connect FA devices Persons who manage working FA installations Persons who use this product must have sufficient knowledge of electrical systems (i....
- マニュアル
... manual is intended for the following readers. • Persons in charge of introducing FA devices • Persons who design FA systems • Persons who install or connect FA devices • Persons who manage working FA installations Persons who use this product must have sufficient knowledge of electrical systems (i....
- マニュアル
...20 * Not yet supported with this CIDRW system Optional Section 4 4.3 Support attributes 46 V700-L21 User's Manual Section 4 SECS Protocol Specifications 4.4 Message specifications (1) Message list 0 S,H←...
- マニュアル
...COMM ID ERR Points to check Lit Not lit Not lit Not lit • RS-232C cable connection (incorrect hard wiring) • Command format ([SOH] included or not) Lit Not lit Not lit Lit • Host communications settings (...
- マニュアル
... no condensation) • Locations not within the specified humidity range • Locations subject to direct vibration or shock outside the specified ranges 2. ID Tag Installation • The product communicates with Tags using the 13.56-MHz frequency band. Some transceivers, motors, monitoring devices, power supplies (...
- マニュアル
...30 (65) E3X-DRT21-S User’s Manual 21 Section 2 Connecting Sensors Connecting Sensors Connectable Sensors The Communication Unit can be connected with the following Sensors. Section 2 Installation and Connection An optional reduced-wiring connector (i....
- マニュアル
... FG terminal is grounded. -If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. -Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...
- マニュアル
... following readers. • • • • Persons in charge of introducing FA devices Persons who design FA systems Persons who install or connect FA devices Persons who manage working FA installations Persons who use this product must have sufficient knowledge of electrical systems (i....
- マニュアル
... its power supply the secondary coil of an insulated transformer that satisfies the following conditions: • Maximum voltage (with no-load): 30 Vrms (42.4 V peak) OR • Maximum current: (1) 8 A (including when shorted) OR (2) A current restricted by a circuit protective device (...
- マニュアル
... the FG terminal is grounded. • If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. • Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...
- マニュアル
... is the allowed current. In actual applications, use a current below the maximum recommended current. Current (A) Wiring the Power Supply and Branch Outputs 40 Use a DC power supply with sufficient capacity and little voltage fluctuation, i....
- マニュアル
... FG terminal is grounded. • If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. • Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...
- マニュアル
... the FG terminal is grounded. • If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. • Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...
- マニュアル
...Number of reading digits 32 digits MAX (Changes according to bar width and reading size) Reading performance (*1) Resolution 0.15 mm (at PCS 0.9) Contrast (PCS) 0.45 or more (white reflectance 70 % or more) Interface EAN/UPC (A, ...
- マニュアル
...0 8 0 0 0002H 0 8 0 0 0 0 0 1 0003H 1 Section 2 RF Tags 0001H 0 3 1 0 0 1 E 7 • Settings to not write-protect any addresses: Address 0000H 0001H 0002H 0003H Bit 7 6 0 0 5 4 3 2 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 The write protection function is a function of the V680-CA5D-V Controller and the C1W-...
- マニュアル
... the FG terminal is grounded. • If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. • Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...
- マニュアル
... system. However, the code used for this reader is special as a space mark is used as the start and stop codes. (Normally “*”) You can create a menu sheet using readily available code creation software, as shown below. Section 2 Preparation 38 ...