全 1430 件が検索されました。(1301 - 1320件を表示)
- マニュアル
... Sensor, data is read from or written to the specified address in the Data Carrier. 3. When data is read, it is sent from the Amplifier to the host system and output by DeviceNet. When data is written, the result of the write processing (i....
- マニュアル
...× × × × × × × × × × × × × × × × × *2 *3 Name/Application DO 1 DO 3 Measurement easu e e results lt output t t DO 5 × Name/Application DO 0 DO 2 Measurement easu e e results lt output t t DO 4 DO 7 DO 6 NC Not connected COM OUT (*2) For DO 0 to DO 7 DO 9 Measurement easu ...
- マニュアル
... wiring communications cables. a) Separate communications cables from power lines or high-tension lines. b) Do not bend communications cables. c) Do not pull on communications cables with excessive force. d) Do not place heavy objects on communications cables. ...
- マニュアル
... Operation) RS-232C cable F160 Computer Multi-drop Connection (No-protocol) Communications between one computer and several F160s is possible using Link Adapters. 31 Units max. RS-422 cable Link Adapter RS-422 cable OMRON 3G2A9-AL004-...
- マニュアル
... O’EIPA, V670-H51Q O’EIPA, KAI KOYPOLHPY V670-CD1D O’EIPA SYMMOPF ONETAI PPOS TIS OYSIODEIS APAITHSEIS KAI TIS LOIPES SXETIKES DIATAXEIS THS ODHGIAS 1999/5/EK. Italian Con la presente Omron dichiara che la RFID Sistema, Antena V670-H11Serie, V670-H51 Serie, V670-H51Q Serie, ...
- マニュアル
... not operating near the V690. 2) If the V690 causes radio interference to a local area wireless station for mobile object identification, change the channel immediately or stop the V690 from emitting radio waves. Then, contact your nearest OMRON representative to take necessary actions to prevent interference (...
- マニュアル
... product. Indicates pages where additional information can be found. 1,2,3... 1. Indicates a procedure. The step numbers in the procedure correspond to the numbers in any related illustrations. Screen Messages In this manual, screen messages are given in bold/italic. ...
- マニュアル
... left. The Fiber Amplifier Units connected to the Communication Unit are identified according to their unit numbers. Unit numbers are automatically assigned to the Units in order from unit number 1 starting from the Unit next to the Communication Unit. Some Fiber Amplifier Units, i....
- マニュアル
... two different models: V530-R150E-3 (input/output type: NPN) and V530-R150EP-3 (input/output type: PNP). In this manual, both models are referred to under the model number “V530-R150.” Screen Messages In this manual, screen messages are given in bold/italic. ...
- マニュアル
... in the wavelength range from 400 nm to 700 nm, protection is afforded by aversion responses including the blink reflex. For other wavelengths the hazard to the unaided eye is no greater than for Class 1. Direct intrabeam viewing of Class 3A lasers with optical aides (...
- マニュアル
... Laser Beam Hazard Z500 Setup Manual 7 Z158-E1-02C.book Page 8 Wednesday, August 9, 2006 6:13 PM INTRODUCTION Laser Safety WARNING Laser Safety Do not to expose your eyes to the laser radiation either directly or indirectly (i....
- マニュアル
... to indicate potential laser beam hazard 10 PRECAUTIONS Laser Safety b WARNING The laser radiation has a high power density and exposure may result in loss of sight. Do not to expose your eyes to the laser radiation either directly or indirectly (i....
- マニュアル
...[Z169-E1-04] V530-R160E/R160EP 2D Code Reader User's Manual T EN RIG T C 2D Code Reader ES T IF SH -KP 50 E F1 SOL N O C V530-R160E/V530-R160EP USER'S MANUAL Cat. No. Z169-E1-04 Product Availability Some of the products listed may not be available in some countries. Please contact your nearest OMRON sales office by referring to the addresses provided at the back of this manual. © OMRON, 2002 All rights reserved. No part of this publication may be reproduced, stored in a retrieval system, or transmitted, in any ...
- マニュアル
... under RS-232C/Operating mode. (Normal is no-protocol.) The status of communications can be checked with the I/O monitor. The Unit operates well initially, but after a while there is no response from the F160. The reception buffer on the external device (...
- マニュアル
... explode if mishandled. Do not disassemble the Data Carrier, or subject it to high pressure or high temperatures (of 100 °C or more), or dispose of it by incineration. xiv Operating Environment Precautions 4 !WARNING Provide safety measures in external circuits, i....
- マニュアル
...) The minimum duration of the override function amounts to 60 seconds. If the buttons are released before this time has elapsed, the override function will be immediately stopped. F3SP Power OFF ON Status indicator 8 7 ・・・ ≡ 1 ...
- マニュアル
... in this document. Cautions to indicate potential laser beam hazard 4 Setup Manual 0intro.fm Page 5 Monday, April 19, 2004 3:17 PM INTRODUCTION INTRODUCTION Laser Safety Do not expose your eyes to the laser radiation either directly or indirectly (i....
- マニュアル
..., solenoids, and magnetic coils). If a noise filter is used for the power supply, check the voltage and current, and install the noise filter as close as possible to the product. Separate the product as far as possible from devices generating strong high-frequency noise (...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 104 Appendices A B C D E Product Configurations . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 105 Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 109 Ladder Program Execution . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 121 Application Examples . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 123 Allocations and Setting Sheets . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 137 Index . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 145 Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 149 viii Z183-01.book Page ix Friday, November 28, 2003 6:43 PM About this Manual: This manual describes the installation and operation of the ZEN Programmable Relay and includes the sections described below. Please read this manual carefully and be sure you understand the information provided before attempting to install or operate the ZEN. Be sure to read the precautions provided in the following section. Precautions provides general precautions ...
- マニュアル
... use it for such purposes. 4 Z550 Setup Manual setup.book Page 5 Friday, June 3, 2005 5:22 PM INTRODUCTION INTRODUCTION Laser Safety WARNING Do not expose your eyes to the laser radiation either directly or indirectly (i....