全 2493 件が検索されました。(1221 - 1240件を表示)

  • マニュアル

    ...(INT) (BOOL) UnitNo Done (INT) (BOOL) Axis Command Aborted (BOOL) (BOOL) Execute Error (REAL) (WORD) Position ErrorID (REAL) Velocity (REAL) Acceleration (REAL) Deceleration (INT) Select CS-series Position Control Unit Operation Manual (W376) CJ-series Position Control Unit Operation Manual (W397) 11-5 Error Code Lists Positioning completed Bit B Abort Bit C Error flag Bit D Error code (May be omitted.) 3-7 Position controller Variable name EN Data type BOOL Default Range Unit No. Axis No. UnitNo Axis INT INT &0 &1 &0 to &95 &1 to &4 Start Position command Execute Position BOOL REAL 0 (OFF) +...

  • マニュアル

    ..., refer to 1-6 Version Upgrade Information. For information on functionality other than function blocks and structure text, refer to the following manuals. • CX-Programmer : CX-Programmer Operation Manual (W446) and CX-Programmer Operation Manual: SFC (W469) • CPU Unit : The operation manuals for the ...

  • マニュアル

    ... OS: Windows 2000, XP, or Vista Ver. 2.24 Applicable OS: Windows 2000, XP, Vista, or 7 Improvements from Version 2.1 to Version 2.2 New functions are listed in the following table. Ver. 2.1 Motion Control Units in ...

  • マニュアル

    ... not be as specified under all possible conditions. Check the warranty information from the manufacturer. 10 Section 1-3 System Configuration PLC Serial Communications Unit / Board connection Configuration CX-Drive Peripheral port Or RS-232C port ...

  • マニュアル

    ... not be as specified under all possible conditions. Check the warranty information from the manufacturer. 10 Section 1-3 System Configuration PLC Serial Communications Unit / Board connection Configuration CX-Drive Peripheral port Or RS-232C port ...

  • マニュアル

    ... and construction of a DeviceNet netW267 work, including installation procedures and specifications for cables, connectors, and other connection devices, as well as information on functions, operating procedures, and applications. Read this manual carefully and be sure you understand the information provided before attempting to use DeviceNet. ...

  • マニュアル

    ... specifications for cables, connectors, and other connection devices, as well as information on functions, operating procedures, and applications. Read this manual carefully and be sure you understand the information provided before attempting to use DeviceNet. Describes the specifications, functions, operating procedures, and W380 applications of ...

  • マニュアル

    ... dealing with problems that might occur with CompoNet Master Units. Related Manuals: Cat. No. Models W456 CS1W-CRM21 and CJ1W(this manual) CRM21 W457 CRT1 Series W464 CXONE-AL@@C-V@ CXONE-AL@@D-V@ Name ...

  • マニュアル

    ...@-@ CP1E-N@@D@-@ NSJ@-@@@@(B)-G5D NSJ@-@@@@(B)-M3D CXONE-AL@@D-V4 W464 xii Name CompoNet Slave Units and Repeater Unit Operation Manual TM Description Provides the specifications of CompoNet Slave Units and Repeater Unit. ...

  • マニュアル

    ...Select [Help] - [Help Contents] from the main menu. CX-Programmer Help will be displayed. 4 Creating Programs ■Referencing PLC Instruction Sets For details on instructions used in ladder programs, refer to PLC Instruction Sets. ●From CX-Programmer 1. Select [Help] - [Instruction Reference] - [...

  • マニュアル

    ... I/O tables is displayed using Unit model numbers. • Model and unit version checks can be performed when transferring data to actual Units. • Device types on the network can be confirmed using Unit models. Note 2 Component and Network Profile Sheet (CPS) files contain ...

  • マニュアル

    ...[W464-E1-15] CXONE-AL[][]D-V4 CX-Integrator Ver.2.[] Operation Manual Cat. No. W464-E1-15 SYSMAC CS/CJ/CP/NSJ/NJ Series CX-Integrator Ver. 2. CXONE-ALD-V4 OPERATION MANUAL NOTE All rights reserved. No part of this publication may be reproduced, stored in a retrieval system, or transmitted, in any form, or by any means, mechanical, electronic, photocopying, recording, or otherwise, without the prior written permission of OMRON. No patent liability is assumed with respect to the use of the information contained herein. Moreover, because OMRON is constantly striving to ...

  • マニュアル

    ... using the most recent version for your area. Name SYSMAC CJ-series CJ1G-CPU@@, CJ1G/H-CPU@@H, CJ1M-CPU@@ Programmable Controllers Operation Manual Cat. No. Contents W393 Describes the installation and operation of the CJ-series PLCs. SYSMAC ...

  • マニュアル

    ... the Loop Controllers Section2 describes the procedure to build an example system on the Loop Controller. Section3 provides the names and functions of parts, and provides other information required toinstall and operate Loop Controllers. Section 4 describes application cases of PLC-based Process Control system. The ...

  • マニュアル

    ... the CX-Programmer Operation Manual (Cat. No. W446). Describes the general CX-Programmer operations that are not specifically related to SFC programming, function block functions, and structured text programming functions. Describes operating procedures for the CX-Integrator Network Configuration Tool for ...

  • マニュアル

    ...NSJ12-TS@@(B)-G5D NSJ Controllers NSJ5-TQ@@(B)-M3D NSJ5-SQ@@(B)-M3D CJ1-H CPU Units CS1-H CPU Units NSJ5-TQ@@(B)-G5D CJ2M-CPU3@ CJ2M-CPU1@ Pulse I/O Module for CJ2M CPU Units CS Series NSJ8-TV@@(B)-M3D CS1D CPU Units CS1D CPU Units for Duplex Systems CS1D-CPU@@H CS1D CPU Units for Simplex Systems CS1D-CPU@@S CS1D Process-control CPU Units CJ1H-CPU@@H-R CS1D-CPU@@P CJ1H-CPU@@H CJ1G-CPU@@H CJ1G -CPU@@P (Loop CPU Units) CS1 CPU Units CS1H-CPU@@(-V) CJ1M CPU Units CS1G-CPU@@(-...

  • マニュアル

    ...This manual tells you about the models, functions, specificaI/O Units Operation Mantions, and operating procedures of the SmartSlice I/O Units. ual W456 This manuals tells you about the CompoNet network, commuCS/CJ Series CompoNet Master Unit Opera- nications specifications, connection procedures, and the ...

  • マニュアル

    .../NA(S)D- An application model of CPU Unit that supports connections to Programmable Terminals, inverters, and servo drives. The CP Series is centered around the CP1H, CP1L, and CP1E CPU Units and is designed with the same basic architecture as the ...

  • マニュアル

    .../NA(S)D- An application model of CPU Unit that supports connections to Programmable Terminals, inverters, and servo drives. The CP Series is centered around the CP1H, CP1L, and CP1E CPU Units and is designed with the same basic architecture as the ...

  • マニュアル

    ...……D…-… A model of CPU Unit that supports Ethernet connection and enhanced positioning functions such as 4-axis linear interpolation and pulse. The CP Series is centered around the CP1H, CP1L, CP1E and CP2E CPU Units and is designed with the same basic architecture as the ...