全 2493 件が検索されました。(1281 - 1300件を表示)

  • マニュアル

    ...Signal name 4-4 ZS-DSU User’s Manual 8 9 Signal name NC SD(TXD) 2 2 RD(RXD) RD(RXD) 3 3 SD(TXD) RS(RTS) 4 4 NC CS(CTS) 5 5 SG(GND) NC 6 6 NC NC 7 7 RS(RTS) NC 8 8 CS(CTS) SG(GND) NC 9 9 NC 10 Section 4 RS-232C Input/Output Setting the Communication Specifications Set the RS-232C communications specifications. Match the communication specifications of the ZS-DSU to those of the external device. FUN Mode-[SYSTEM]-[COM] Setting RS232C Range LENGTH 8BIT, 7BIT (default value: ...

  • マニュアル

    ...2 RD SD 3 3 SD NC 4 4 NC SG 5 5 SG NC 6 6 NC RS 7 7 RS NC 8 8 CS NC 9 9 NC Ground shielded wires either at the CIDRW Controller side or at the PC/AT side. CIDRW System User’s Manual SECTION 2 Connections and Wiring CIDRW Controller V700-L22 D-SUB, 9-pin Socket type #4-40 29 SECTION 2 Installation and Connections/Wiring Amplifier Unit ■ Connector for connecting a CIDRW Head 1. Align the pin on the connector with the Connections and Wiring SECTION 2 channel in the cable ...

  • マニュアル

    ...Controller side 3 7 4 8 5 9 Signal name NC SD(TXD) 2 2 SD(TXD) RD(RXD) 3 3 RD(RXD) RS(RTS) 4 4 RS(RTS) CS(CTS) 5 5 CS(CTS) NC 6 6 NC NC 7 7 NC NC 8 8 NC SG(GND) NC FG 9 9 SG(GND) 10 Shell Shell FG Note 1: Plug type connector ZS-HL User’s Manual 7-5 Section7 Connecting Using a RS-232C Cable  RS-232C Cable for Connecting to a Personal Computer • ZS-XRS2 (cable length: 2 m) Controller side Personal computer side (PC/...

  • マニュアル

    ...Product Configuration A V680-series RFID System consists of an ID Controller, one or more Amplifiers, one or two Antennas, and Section 1 Product Configuration RF Tags. Select the models suitable for the application.  Using Antennas with Separate Amplifiers Programmable Controller (SYSMAC ...

  • マニュアル

    ...) Product versions are displayed on the monitor display when the power supply is turned ON. To use the V680-CA5D01-V2, it must be version 2.3 or newer. To use the V680-CH@D, it must be version 1.1 or newer. To use the ...

  • マニュアル

    ...Product Configuration A V680-series RFID System consists of an ID Controller, one or more Amplifiers, one or two Antennas, and Section 1 Product Configuration RF Tags. Select the models suitable for the application. „ Using Antennas with Separate Amplifiers Programmable Controller (SYSMAC ...

  • マニュアル

    ...Product Configuration A V680-series RFID System consists of an ID Controller, one or more Amplifiers, one or two Antennas, and Section 1 Product Configuration RF Tags. Select the models suitable for the application.  Using Antennas with Separate Amplifiers Programmable Controller (SYSMAC ...

  • マニュアル

    ...3 SD 3 SD 4 N.C. 4 ER 5 SG 5 SG 6 N.C. 6 DR 7 N.C. 7 RS 8 N.C. 8 CS 9 N.C. 9 CI Shell FG COMMUNICATIONS WITH EXTERNAL DEVICES Connector Pin Arrangement and Connection Example with a PC * Pin Nos. may vary with the type and model of the external device to be connected. For details, refer to the instruction manual of your PC or PLC. ZX-GT User’s Manual RS-232C 101 About Communications Commands Command/Response Format Important The command/response format differs according to the RS-...

  • マニュアル

    ...3 SD 3 SD 4 N.C. 4 ER 5 SG 5 SG 6 N.C. 6 DR 7 N.C. 7 RS 8 N.C. 8 CS 9 N.C. 9 Connector hood CI FG * Pin Nos. may vary with the type and model of the external device to be connected. For details, refer to the instruction manual of your programmable controller or personal computer. ZN System Manual Section 4 Specifications and Dimensions Clean Monitoring System Item Power supply voltage ZN-SFW11 ZN-SFW12 Supplied from ZN-PDA Current consumption 45 mA with 24 VDC without Amplifier Unit Available ...

  • マニュアル

    ...a host computer. • Insert a Cramp Filter (E04SR301334 manufactured by SEIWA) in the cable as a countermeasure against noise. RS-232C interface Computer Name Pin Pin CD RD SD ER SG DR RS CS C1 1 2 3 4 5 6 7 8 9 1 2 3 4 5 6 K3SC-10 Name Name PWR NC SG PWR SD RD SG RDA(−) SDA(−) NC RDB(+) SDB(+) RS-485 Pin 7 8 9 10 11 12 (See note.) S8AS A(−) B(+) Clamp filter We recommend twisting the RS-485 communications lines. (See note.) RS-485 S8AS A(−) B(+) (See note.) Power ...

  • マニュアル

    ... use the V680/V680S-series RFID System correctly. • Keep this manual in a safe and accessible location so that it is available for reference when required. READ AND UNDERSTAND THIS DOCUMENT Section 1 Features and System Configuration Introduction SECTION 1 Introduction Section 2 ...

  • マニュアル

    ... use the V680/V680S-series RFID System correctly. • Keep this manual in a safe and accessible location so that it is available for reference when required. READ AND UNDERSTAND THIS DOCUMENT Section 1 Features and System Configuration Introduction SECTION 1 Introduction Section 2 ...

  • マニュアル

    ... sure that the version allows setting the Tag memory setting to CA1D Mode. To use the V680-CA5D01-V2/-CA5D02-V2, it must be version 2.3 or newer. To use the V680-CH@D, it must be version 1.1 or newer. To use the ...

  • マニュアル

    ... can be used to read and set Sensor parameters and to execute measurements. 1-2 1-1 Features and System Configuration 1-1-2 Features 1 „ Communications Interface That Connects Smart Sensors with a Host, Including OMRON PLCs (such as the ...

  • マニュアル

    ... layout. ZS-XRS2 (cable length: 2 m) 4 10 Fitting section 1 Personal computer side (PC/AT compatible) (Note 1) 5 4 3 2 1 9 Signal name NC SD (TXD) RD (RXD) RS (RTS) CS (CTS) NC NC NC SG (GND) NC FG Pin No. 1 2 3 4 5 6 7 8 9 10 Shell 8 7 6 Pin No. 1 2 3 4 5 6 7 8 9 Signal name NC RD (RXD) SD (TXD) NC SG (GND) NC RS (RTS) ...

  • マニュアル

    ...2 RD SD 3 3 SD NC 4 4 NC SG 5 5 SG NC 6 6 NC RS 7 7 RS NC 8 8 CS NC 9 9 NC Ground shielded wires either at the CIDRW Controller side or at the PC/AT side. CIDRW System User’s Manual SECTION 2 Connections and Wiring CIDRW Controller V700-L22 D-SUB, 9-pin Socket type #4-40 39 SECTION 2 Installation and Connections/Wiring Amplifier Unit ■ Connector for Connecting a CIDRW Head 1. Align the pin on the connector with the channel in the cable connector and insert SECTION 2 ...

  • マニュアル

    ... as PLCs, are connected. (Setup Mode) − [Sensor settings] − [Network] − [Ethernet] 1 2 Set [Auto] to [OFF]. Set the IP address and subnet mask according to the network where the external devices, such as PLCs, are connected. Note If you connect OMRON ...

  • マニュアル

    ...Manual Configuration RFID System V680 Series User's Manual ID Sensor Units (Cat. No. Z271) Section 6 Description SECTION 1 Features and System Configuration This section describes the features and system configuration of ID Sensor Unit. SECTION 2 ...

  • マニュアル

    ...2 Installation and Connections (Setup Mode) − [Sensor settings] − [Network] − [Ethernet] 1 2 Set [Auto] to [OFF]. Set the IP address and subnet mask according to the network where the external devices, such as PLCs, are connected. Note If you connect OMRON ...

  • マニュアル

    ...Wire color Pin No. Signal name Function Reader Green 1 SD Transmission data White 2 RD Received data Gray 3 RS Transmission request Signal direction Upper equipment Blue 4 CS Transmission allowed Brown 5 TRIG External trigger signal - 6 NC Not connected Black 7 S.GND 0V Red 8 VCC Power supply External External Yellow - (Note) OK READ OK output External Orange - (Note) NG READ NG output External When you make a connection cable, use the following connectors. Recommended parts for the connector Usage Manufacturer Model For cable relay Hosiden Corporation TCS8587-0170477 For panel installation Hosiden Corporation TCS1080-0120177...