全 2493 件が検索されました。(1241 - 1260件を表示)

  • マニュアル

    ... Master Board for Provides the specifications of PCI Bus and for CompactPCI the CompoNet Master Board Bus Operation Manual Provides the specifications of CR1-series CompoNet TM Slave Units and Repeater Unit CompoNet Slave Units and Repeater Units Operation Manual TM ...

  • マニュアル

    ... use the Units. Section 7 Common Items This chapter explains the operating procedure common among Analog Input Units, Output Units and I/O Units. Appendices --- CJ-series Analog I/O Units Operation Manual for NJ-series CPU Unit(W490) Manual Configuration ...

  • マニュアル

    ... Unit when it is used in an NJ-series Controller are described. CompoNet Slave Units and Repeater Unit Operation Manual W457 CRT1 Series Learning about CompoNet Slave Units The models, functions, specifications, operating procedures, and other details are described. ...

  • マニュアル

    ... the Serial Communications Unit. Reference This section describes the details on the standard system protocols provided by the CX-Protocol and the Serial Communications Unit. Appendix --- CJ-series Serial Communications Units Operation Manual for NJ-series CPU Unit(W494) Manual Configuration SYSMAC ...

  • マニュアル

    ... take corrective actions for errors and conduct a routine inspection. Appendix This section describes the details on the commands for the message communciations and the completion codes of the message communications. CJ-series DeviceNet Units Operation Manual for NJ-series CPU Unit(W497) Manual Configuration ...

  • マニュアル

    .../PH41U), and describes the operating procedure and how to wire the Unit. Appendices --- CJ Series Analog I/O Unit Operation Manual (Cat. No. W368) Section Section 1 Overview and Feature 4 Description This section presents an overview of the ...

  • マニュアル

    ...-series Digital I/O Units User's Manual (W521) 4 Installation and Wiring Precautions for Safe Use Additional Information The Digital I/O Units with 32 points and Fujitsu/OTAX connectors have the same connector pin allocations as the C200H High-density I/O Units, ...

  • マニュアル

    ... CPU Unit or NYseries Industrial PC that is compatible with the EtherNet/IP Coupler Unit. Sysmac Studio version that is compatible with the NX Unit, EtherNet/IP Coupler Unit, CPU Unit, and Industrial PC. Application with a ...

  • マニュアル

    ... CPU Unit or NYseries Industrial PC that is compatible with the EtherNet/IP Coupler Unit. Sysmac Studio version that is compatible with the NX Unit, EtherNet/IP Coupler Unit, CPU Unit, and Industrial PC. Application with a ...

  • マニュアル

    ... CPU Unit or NYseries Industrial PC that is compatible with the EtherNet/IP Coupler Unit. Sysmac Studio version that is compatible with the NX Unit, EtherNet/IP Coupler Unit, CPU Unit, and Industrial PC. Application with a ...

  • マニュアル

    ...of the NX Unit Corresponding unit versions/versions Application with an NJ/NX/NY-series Controller EtherNet/IP Coupler Unit Unit version of EtherNet/IP Coupler Unit that is compatible with the NX Unit Application with a ...

  • マニュアル

    ... Controllers CX-Designer *1. Application The CX-Designer is used to create screens for NS-series PTs. If the NJ/NX-series Controller is a target device, you may also use Sysmac Studio version 1.10 or higher. Use the Network Configurator if a ...

  • マニュアル

    ... Unit User’s Manual (W536) 25 Precautions for Safe Use Program the Slave Terminal Status (refer to 9-2-3 I/O Allocation Information on page 9-12 ) and/or Unit status CIO bits as an interlock condition in the user program. Refer to the ...

  • マニュアル

    ...NX-series Communications Interface Units User’s Manual (W540) 1 Features and System Configuration Slave Terminal Communications master Usability • NJ/NX-series CPU Unit • NY-series Industrial PC EtherCAT Coupler Unit Usable*1 EtherNet/IP Coupler Unit Not usable ...

  • マニュアル

    ... USB port of the Box PC to connect the Sysmac Studio with the Machine Controller Software. 2-4-2 Configurations That Do Not Allow Online Connections This section gives information on configurations that do not provide a connection to the Sysmac Studio. 2 Routing through ...

  • マニュアル

    ... port of the Panel PC to connect the Sysmac Studio with the Machine Controller Software. 2-4-2 Configurations That Do Not Allow Online Connections This section gives information on configurations that do not provide a connection to the Sysmac Studio. 2 Routing through ...

  • マニュアル

    ... the axes group is enabled, linear interpolation is executed. MV_LIN_ABS MC_Group000 MC_Group000.Status.Ready Mv_Lin_Abs_Pos Mv_Lin_Abs_Vel Mv_Lin_Abs_Acc Mv_Lin_Abs_Dec Mv_Lin_Abs_Jrk Mv_Lin_Abs_Cs Mv_Lin_Abs_Bm Mv_Lin_Abs_Tm MC_MoveLinear AxesGroup AxesGroup Done Execute Busy Position Velocity Active Acceleration CommandAborted Deceleration Error ErrorID Jerk CoordSystem BufferMode TransitionMode Mv_Lin_Abs_D Mv_Lin_Abs_Bsy Mv_Lin_Abs_Act Mv_Lin_Abs_Ca Mv_Lin_Abs_Err Mv_Lin_Abs_ErrID If the external button turns ON (...

  • マニュアル

    .../IP port) (NX701-) These Units are used to connect to an EtherNet/IP network. OMRON PLCs CJ2 (built-in EtherNet/IP port) (CJ2H-CPU-EIP or CJ2M-CPU3) CJ-series EtherNet/IP Unit* (CJ1W-EIP21) CS-series EtherNet/IP Unit (CS1W-EIP21) (2) Twisted-pair cable The twisted-pair cable has a RJ45 Modular Connector at each end. This cable is used to connect the built-in EtherNet/IP port or EtherNet/IP Unit to an Ethernet switch. Use an STP (shielded twisted-pair) cable of category 5, 5e, or higher. (3) ...

  • マニュアル

    ... between Unit Versions of Units The items that are used in the version combination table are given below. NX Unit Corresponding unit versions/versions Application with an NJ/NX/NY-series Controller Model Model number of NX Unit. Application with a ...

  • マニュアル

    ... and Heater Burnout Detection Units (W566) 7-7 7 7-2-3 System Configuration For details on the analog control instructions of the NJ/NX/NY-series Controllers, refer to the instructions reference manual for the connected CPU Unit or Industrial PC. Refer to the ...