全 2493 件が検索されました。(1321 - 1340件を表示)
- マニュアル
... No. Name Name FG 1 1 NC SD 2 2 Host_RxD RD 3 3 Host_TxD RS-232C RS-232C RS 4 4 NC Interface Interface CS 5 5 0V 5V 6 6 NC DR 7 7 NC ER 8 8 NC SG 9 9 NC FG Shell Shell FG D-SUB 9 Pin D-SUB 9 Pin Cable Connector Type: Male Cable Connector Type: Male NJ501-1500 CJ1W-SCU22 F430-F00M12M DC24V RS-232C cable I/O Cable V430-W8-3M RS-232C-I/O Pronge cable V430-W2-W3 2 10 6.3. Communication Verification Example...
- マニュアル
... is not necessary to connect with a PC during operation. Additional Information The cable to use for Serial (RS-232C) communication is RS-232C-I/O Y cable (V430WQR-3M). Please use this cable when connecting to a PC by RS-232C. When connecting with OMRON ...
- マニュアル
... with a non-defective one, and restart both the FH series Sensor Controller and the 3D vision sensor. 1-2 Camera Image Input AOS When judgment is NG with no image input 1 Input Image Character string Measurement items Camera status ...
- マニュアル
...-1 Interconnect Cable with RS-232 Breakout V430-WQR-3M* 3 M12-to-Flying Leads Cable V430-W8-M *Insert the V430-WQR-3M cable between the V440-F and the V430-W8 cable. *1. If connecting Omron’s CS/CJ/NJ Controller, check the connector shape and signal lines (pin assignments) and prepare the additional RS-232C conversion cable. If connecting to Omron’s NX Machine Automation Controller, no additional RS-232C cable is required. 2-10 V440-F C-Mount Code Reader User Manual 2 Quick Start 2-4 Connect to WebLink 2-...
- マニュアル
...gurator to set up the Tag Data Links (tags, tag sets, and connection settings). For more detailed information on Tag Data Link settings, please refer to the following manuals. • NJ/NX-series CPU Unit Built-in EtherNet/IP Port User’s Manual (Cat. No. W506) • ...
- マニュアル
...gurator to set up the Tag Data Links (tags, tag sets, and connection settings). For more detailed information on Tag Data Link settings, please refer to the following manuals. • NJ/NX-series CPU Unit Built-in EtherNet/IP Port User’s Manual (Cat. No. W506) • ...
- マニュアル
...Controller side 3 7 4 8 5 9 Signal name NC SD(TXD) 2 2 SD(TXD) RD(RXD) 3 3 RD(RXD) RS(RTS) 4 4 RS(RTS) CS(CTS) 5 5 CS(CTS) NC 6 6 NC NC 7 7 NC NC 8 8 NC SG(GND) NC FG 9 9 SG(GND) 10 Shell Shell FG Note 1: Plug type connector ZS-HL-N User’s Manual 7-5 Section7 Connecting Using a RS-232C Cable RS-232C Cable for Connecting to a Personal Computer • ZS-XRS3 (cable length: 2 m) Controller side Personal computer side (...
- マニュアル
...3 M12-to-Flying Leads Cable V430-W8£££-£M 4 RS-232C Conversion Cable Required for Legacy Omron PLCs V430-WPLC-2M*2 Insert the V430-WQR-3M cable between the VHV5-F and the V430-W8£££-£M cable. When connecting Omron’s ...
- マニュアル
... (Z477-E) 1-3 1 Communication Specifications Overview Additional Information The cable to use for Serial (RS-232C) communication is RS-232C-I/O Y cable (V430WQR-3M). Please use this cable when connecting to a PC by RS-232C. When connecting with OMRON ...
- マニュアル
...9.1.2. TCP Socket Communications by Manipulating Dedicated Control Bits This section provides an overview of TCP socket communications by manipulating dedicated control bits and the general movement of send and receive messages. Note For details, refer to Section 6 Socket Services in the ...
- マニュアル
...--- CR (Carriage Return) and LF (Line Feed) are control characters that indicate line breaks in a text file. CR returns the cursor to the beginning of the line. LF moves the cursor to the next line. CX-Programmer --- Configuration Support Software for OMRON ...
- マニュアル
... Example ZP-RSA External device Signal SD 1 RD RD 2 SD SG 3 ER RQ 4 SG SG 5 DR SLD 6 2 RS Shield CS FG • Terminal numbers 3, 5, and 6 are short-circuited internally. • Terminal numbers 3, 5, and 6 are common to the blue wire of the master Amplifier Unit. • The recommended connection method may differ depending on the type and model of the external device to be connected. Check the instruction manual for your PLC or computer. Short-circuit the RS and ...
- マニュアル
... Standard Master can perform standard I/O communications with a Standard Slave using default I/O assembly data only. This function must be used to perform I/O communications using other I/O assembly data. 84 Section 3-2 Remote I/O Allocations ...
- マニュアル
... target network will start if the Yes Button is clicked here. If there is another device that must be added after the upload has completed, add the device following the same procedure as in Adding Devices from the Hardware List, above. IMPORTANT If there is a ...
- マニュアル
... Input Monitor • Local Output Monitor • When the I/O type of a Target I/O is Target IN, data for communications between this Unit and a Safety Slave performing DeviceNet Safety communications can be included in the I/O data. IMPORTANT When connected to an OMRON ...
- マニュアル
... addresses of the devices on the virtual network so that they match the node address switch settings for the actual devices. Right-click Match the node addresses. Note The node addresses will affect memory allocations of the I/O Memory Area for the OMRON ...
- マニュアル
...This indicator flashes during serial communications. RS-232C Connector 5 1 9 6 Pin Abbr. 1 2 3 4 5 6 7 8 FG SD (TXD) RD (RXD) RS (RTS) CS (CTS) 5V DR (DSR) ER (DTR) 9 Connector hood SG (0 V) FG Signal Frame ground Send data Receive data Request to send Clear to send Power Data set ready Data terminal ready Signal ground Frame ground Signal direction --Outputs Inputs Outputs Inputs --Inputs Outputs ----- Precautions for Correct Use Always turn OFF the power supply to the G9SP-series Controller before mounting or removing Option Boards. Communications Specifications Only ...
- マニュアル
...RS-232C Serial Communications Board Connector Pin No. Pin No. Signal FG 1 1 CD SD 2 2 RD RD 3 3 SD RS 4 4 ER CS 5 5 SG 5V 6 6 DR DR 7 7 RS ER 8 8 CS SG 9 9 RI Connector D-Sub male 9-pin Sample Ladder Programming for Mitsubishi Electric PLC Q series This section provides an example of programming to monitor Safety Input terminal data of a G9SP-series Controller from a Mitsubishi Electric Standard PLC Q series. RS-232C Serial Communications Sequence The G9SP-series Controller returns a response ...
- マニュアル
...ださい。 2 信号 端子番号 SD RD SG RQ SG SLD 1 2 3 4 5 6 RD SD ER SG DR RS CS FG シールド ※ 端子番号3、5と6は内部で短絡されています。 ※ 端子番号3、5と6はアンプユニット親機の青色線と共通になっています。 ※ 推奨される接続方法は外部機器...
- マニュアル
... A * 安全上の要点 8 9 信号名 NC NC SD(TXD) 2 2 SD(TXD) RD(RXD) 3 3 RD(RXD) RS(RTS) 4 4 RS(RTS) CS(CTS) 5 5 CS(CTS) NC 6 6 NC NC 7 7 NC NC 8 8 NC SG(GND) NC FG 9 9 SG(GND) 10 シェル シェル 動作時:0∼+50℃、保存時:−15∼+60℃ (ただし、氷結、結露なきこと) 周囲湿度 動作時、保存時:35∼85%RH (...