全 41926 件が検索されました。(1121 - 1140件を表示)

  • マニュアル

    ... note a.) Tag name Link number Comment Comment from user link table (only through 24th character) Number of links Automatically set by system (number of tags referenced) Cycle Refresh cycle (0 to 8) (0: System common operating cycle, 1: 0.01 ...

  • マニュアル

    ... Tool or FINS command. block Function block Standard: Operation of all function blocks is executed at the same operation cycle preset operation cycle to ITEM 004 in the System Common block. Settable operation cycles: 0.1 s, 0.2 s, 0.5 s, 1 ...

  • マニュアル

    ...r R – – 0: Normal, Other: Error(See Appendix "Execution Error Code List.") Parameter 004 System common 1 to 5 4 – R/W(S) – – – operation cycle (sec) (:1s) 1: 01.s, 2: 0.2s, 3: 0.5s, 4: 1s, 5: 2s Note: Before changing the operation cycle, first stop the Loop Control Unit., 40 Data Length (bytes) 1 24 2 2 2 1 System Common blocks <000> System Common blocks 000 (fixed) CPU Unit run status *1:On the CX-Process Monitor, the R/W mode is indicated in the Tuning screen or in the Control screen. COLD R/W Mode...

  • マニュアル

    ...Master’s node number: 63 Slave’s network address: 1 Slave’s node number: 2 Section 6-3 Explicit Message Communications CMND(194) Operand Details [CMND S D C] • Command Words Word S S+1 S+2 S+3 S+4 S+5 Contents Function (Hex) 28 01 EXPLICIT MESSAGE SEND command code = 2801 (Hex) 02 1C Slave node number = 02 (Hex) READ BYTE DATA command service code = 1C (Hex) 00 2F Class ID = 002F (Hex) 00 01 Instance ID = 0001 (Hex) specifies data area 0A 00 Starting read address = 000A (Hex) specifies IR 010 Address L = 0A (Hex); Address ...

  • マニュアル

    ...(06) is an instruction that causes a non-fatal error. The following will occur when an FAL(06) instruction is executed: 1,2,3... 1. The ERC indicator on the Customizable Counter Unit will flash. Operation will continue. 2. The instruction’...

  • マニュアル

    ...C S S D D Local node S 1st response word Remote Master Unit CPU Unit Interpretation1 Interpretation2 Command data Response No. of command bytes Response Response monitoring time ...... S+2 S+3 S+4 Command Destination node Local Master Unit CPU Unit S+1 Operands C: Control code S: 1st source word D: Destination information Execution L Execution ... Response data 1: For commands addressed to Master Unit 2: For commands addressed to CPU Unit Description IOWR transfers data from the words beginning at S to the specified Special I/ O Unit. The control code (C) specified parameters for the ...

  • マニュアル

    ... byte, IN size: 3 bytes Node address 2: OUT size: 1 byte, IN size: 2 bytes 15 Allocation size setup table I 1 5 s I+1 4 3 s+1 I+2 1 2 s+2 : : s+3 OUT block 1 15 k 00 00 01 01 k+1 00 00 01 01 k+2 02 k+3 Not usable : k+4 00 Not usable 01 01 Not usable 01 02 k+5 l: First word of the allocation size setup table s: First word of OUT block 1 k: First word of IN block 1 Note 00...

  • マニュアル

    ... the remote node. If the response is not be received within the response time, the request is timed out. The Message Monitoring Timer Service API functions are used to set the message monitoring timer for each remote device. The default message time is 2 ...

  • マニュアル

    ... ON, XFER(70) copies the contents of S, S+1, ..., S+N to D, D+1, ..., D+N. S D 3 4 5 2 3 4 5 2 S+1 D+1 3 4 5 1 3 4 5 1 S+2 D+2 3 4 2 2 3 4 2 2 S+N D+N 6 4 5 2 6 4 5 2 Note XFER(70) can be used to shift data by setting the operands so that data is moved between overlapping areas. 35 Section Data Movement Instructions 2-7 N Equal to 9999 When the execution ...

  • マニュアル

    ... before operation is started) is possible CX-Process Tool or FINS command. Standard: Operation of all function blocks is executed at the same operation cycle preset to ITEM 004 in the System Common block. Settable operation cycles: 0.1 s, 0.2 s, 0.5 s, 1 ...

  • マニュアル

    ... s: 50 h 10 min: 300 days 10 s: 100 h 30 min: 900 days 30 s: 300 h 60 min: 1,800 days Collection cycle Data display Horizontal axis Collection cycle 1 min: 2 h to 10 days 1 s: 2 min to 240 min 5 min: 10 h to 50 days 2 s: 4 min to 240 min 10 min: 20 h to 100 days 5 s: 10 min to 240 min 30 min: 60 h to 300 days 10 s: 20 min to 240 min 60 min: 5 days to 600 days 30 s: 20 min ...

  • マニュアル

    ... the radius of the sphere. SI Derived Units Quantity Unit name Plane angle Solid angle Frequency radian steradian hertz Unit symbol rad sr Hz Force newton N 1 N = 1 kg·m·s−2 Pressure, stress pascal Pa Energy, work, quantity of heat Power, radiant flux joule J 1 Pa = 1 N·m−2 1 J = 1 N·m watt W 1 W = 1 J·s−1 Electric charge, coulomh quantity of electricity Electric potential, volt electromotive force Electric capacitance farad C 1 C = 1 A·s V 1 V = 1 W·A−1 F 1 F = 1 C·...

  • マニュアル

    ...171.104 μs 171.104 μs K Calculation Example Conditions Baud rate 3.0 Mbit/s Word outputs Word inputs Bit outputs 7 Units 8 Units 9 Units Bit inputs 10 Units K = (7 × 5.312 µs) + (2 × 5.312 µs) ≅ 0.048 ms • TOUT: Output Slave Unit output delay time For details on delay times for individual Slave Units, refer to the output specifications for individual Slave Units in the CompoNet Slave Unit Operation Manual (Cat. No. W457). 143 Section 5-3 Remote I/O Communications Performance ■ Reference Example The following table shows the calculation results for ...

  • マニュアル

    ... because the input is ON twice when a measurement is taken. Measured approx. every 1 s ON OFF 0.5 s Figure B ■ Measuring an ON Time of 1.5 s In Figure C, the actual ON time is 3 s (2 × 1.5 s) but the total ON time is measured as 4 s because the input is ON 4 times when a measurement is taken. 507 Section 11-3 Functions of Digital I/O Slave Units Measured approx. every 1 s ON OFF 1.5 s Figure C Settings Using the CX-Integrator 1,2,3......

  • マニュアル

    ... the System Common Block (block model 000) ITEM type ITEM Data contents Data range Default Parameter 050 HMI EM bank number 0 to C (Hexadecimal) 0 051 HMI function's operation cycle (s) 1 (0.1 s), 2 (0.2 s), 3 (0.5 s), 4 (1 s), or 5 (2 s) Note: Always stop operation before changing this ITEM. 1 to 5 4 (1 s) 056 Reception stop switch 0: Normal; 1: Stop reception 0 or 1 0 057 Transmission stop switch 0: Normal; 1: Stop transmission 0 or 1 0 059 HMI function disable switch 0: Used; ...

  • マニュアル

    ....016 s min.; Special Instructions: 0.048 s min. Basic Instructions: 0.04 s min.; Special Instructions: 0.06 s min. Interrupts I/O Interrupts and External Interrupts Interrupt task startup time: 26 s or 17 ...

  • マニュアル

    ... of 1 condition. You cannot write the data of multiple sequences or multiple conditions with 1 instruction. S: Rightmost Word Number of Transfer Source Prepare the transfer data as follows in the word which you specified in S. Words S S+1 ...

  • マニュアル

    ... Comparison Table Depending on the number of target values in the table, the target-value comparison table requires a continuous block of 4 to 19 words. 15 S 0 Number of target values S+1 Lower word of target value 1 ...

  • マニュアル

    ... through S1+2: Present Time Data S2 through S2+2: Comparison Time Data S1 through S1+2 contain the present time data. S1 through S1+2 must be in the same data area. S2 through S2+2 contain the comparison time data. ...

  • マニュアル

    .../s Word Outputs Word Inputs 7 Units 8 Units Bit outputs 9 Units Bit inputs 10 Units 1.5 Mbit/s 0.77 ms + M 93.75 kbit/s 7.32 ms + M K = (7 × 5.37 µs) + (2 × 5.37 µs) ≈ 0.048 ms TCrmIn (Input Processing Time at Master Board) Data rate TCrmIn 4.0 Mbit/s 0.47 ms + M 3.0 Mbit/s 0.52 ms + M M = (Number of Word Output Slave Units connected × 1.09 µs) + (Number of Word Input Slave Units connected × 4.53 µs) + (Number of Bit ...