全 41926 件が検索されました。(1201 - 1220件を表示)

  • マニュアル

    ...a l - 1 Alarm value 1 a l - 2 Alarm value 2 a l - 3 Alarm value 3 t s 1 s Time signal 1 step selection o n 1 Time signal 1 ON time o f 1 Time signal 1 OFF time t s 2 s Time signal 2 step selection o n 2 Time signal 2 ON time o f 2 Time signal 2 OFF time PV/Present SP SP U Program Control stops at the following mode. 8 9 Absolute-value upper-limit alarm Absolute-value upper-limit alarm Absolute-value 10 upper-limit alarm with standby ...

  • マニュアル

    ....59N・m at maximum. Even for this type of installation, do not fail to use the tie bands. Mechanical durability : 10 to 55Hz , 1.5mm double amplitude in X, Y, and Z directions, respectively for 2 hours each Shock Mechanical durability : 500m/...

  • マニュアル

    ....59N・m at maximum. Even for this type of installation, do not fail to use the tie bands. Mechanical durability : 10 to 55Hz , 1.5mm double amplitude in X, Y, and Z directions, respectively for 2 hours each Shock Mechanical durability : 500m/...

  • マニュアル

    ... (or object resolution) of the F3SG-R Safety distance (S) Hazard Calculation Example for Systems with a Detection Capability of 40 mm or Less Use K = 2,000 mm/s and C = 8 x (d - 14 mm) in formula (1) for the calculation. ...

  • マニュアル

    ... (or object resolution) of the F3SG-R Safety distance (S) Hazard Calculation Example for Systems with a Detection Capability of 40 mm or Less Use K = 2,000 mm/s and C = 8 x (d - 14 mm) in formula (1) for the calculation. ...

  • マニュアル

    ... (or object resolution) of the F3SG-R Safety distance (S) Hazard Calculation Example for Systems with a Detection Capability of 40 mm or Less Use K = 2,000 mm/s and C = 8 x (d - 14 mm) in formula (1) for the calculation. ...

  • マニュアル

    ... (or object resolution) of the F3SG-R Safety distance (S) Hazard Calculation Example for Systems with a Detection Capability of 40 mm or Less Use K = 2,000 mm/s and C = 8 x (d - 14 mm) in formula (1) for the calculation. ...

  • マニュアル

    ... (or object resolution) of the F3SG-RR Safety distance (S) Hazard Calculation Example for Systems with a Detection Capability of 40 mm or Less Use K = 2,000 mm/s and C = 8 x (d - 14 mm) in formula (1) for the calculation. ...

  • マニュアル

    ...㎜micat蜘sGuide. 嘩遼 ---------------------[End of Page 8827]--------------------- 6'、■「'.裟;燐:三…ひ蹴 ',羅_=言,綴:・."4:■"・'1:泌=セ;4・ン .ぢ・.■ : び1 :1: マ・、' .・〉 1裟〃ン宮雛雛 ' ' ソ S.2髄am㊧s◎響Pa醜s ■Mainpa『k$ Thefigureb¢1owshewsthemain茎}artsof也eES10◎P,ar}ddescribeseachof tkeirfunctions. FoずmOtedetailsOSt費1esemair1{)ans,seethepagenumbersfore〔麹ch descdption. 荊ea『case C◎n嘘ainsthem創nun薩。 Rearpanei Herea陀bca鎚癩termin剖s拍rw{ringand 白xpanded置ノOconnector$、 DIPswitches The$白arelocated◎『...

  • マニュアル

    ... communications is being used and can be calculated as described next. Only Message Communications (Remote I/O Communications Stopped) Communications cycle time = 2 (see note) + 0.11 x TB + 0.6 ms TB depends on the baud range as follows: 500 KB/...

  • マニュアル

    ...) <0> K (1)<2>, J (1)<4> K (2)<3>, J (2)<5> PT100 (2) <1> E (1)<7>, L (1)<8> T (2)<6>, U (2)<9> 4 to 20 mA <15> 1 to 5 V <17> N (1)<10>, W (1)<14> R (2)<11>, S (2)<12> 0 to 20 mA <16> 0 to 5 V <18> B (2)<13> 0 to 10 V <19> p390.1 p160.1 1t53.1 2t22.1 a 20.1 1V 5.1 2V10.1 p 20.1 p 40.1 1t-6.1 2t-6.1 a 1V 1....

  • マニュアル

    ...ON MODE Output mode Output time Input signal width Function setting mode NPN/PNP input colr Display color Set value *1 up, *2 a, a-1, a-2, a-3, b, b-1, d, e, f, , s *2 hold/0.01 to 99.99 Comments ----Only modes a-2, b, e, and can be selected for H5CX-L8E@. (If the output time is set to 0.00, hold is displayed.) Displayed for modes a, a-1, a-2, a-3, b, b-1 and s only. Unit: second , *2 Displayed only for models other than H5CX-L8E@. npn, pnp *2...

  • マニュアル

    ...H5CZ-L8/-L8D Present value OFF Set value Change to "Twin Timer" using the U Key. 0V otim Set value *1 up, down *2 a, a-1, a-2, a-3, b, b-1, d, e, f, z, s *2 hold/0.01 to 99.99 MODE + Function setting mode Display Parameter name timr Time range timm UP/DOWN mode outm Output modes Timer U1 Timer/Twin selection mode Reset Signal Power ON 3 s min. Mode Key (Changes modes and setting items) Reset Key (Resets present value and output) Up Keys 1 to 4 Down Keys 1 to 4...

  • マニュアル

    ...H5CZ-L8/-L8D Present value OFF Set value Change to "Twin Timer" using the U Key. 0V otim Set value *1 up, down *2 a, a-1, a-2, a-3, b, b-1, d, e, f, z, s *2 hold/0.01 to 99.99 MODE + Function setting mode Display Parameter name timr Time range timm UP/DOWN mode outm Output modes Timer U1 Timer/Twin selection mode Reset Signal Power ON 3 s min. Mode Key (Changes modes and setting items) Reset Key (Resets present value and output) Up Keys 1 to 4 Down Keys 1 to 4...

  • マニュアル

    ...表示のみ。 設定ではありま ON 回数モニタ値せん。 ×1000 設定値 ※1 up, down ※2 a, a-1, a-2, a-3, b, b-1, d, e, f, z, s ※2 hold/0.01∼99.99 ※接点ONで動作 ※トランジスタONで動作 キープロテクトスイッチの設定キープロテクトスイッチ 「ON」時は、 下表のキープロ...

  • マニュアル

    ... value (display value) ≥ Comparison value 1 ON condition for output 2: CP2 present value (display value) ≥ Comparison value 2 1 2 3 4 5 6 7 8 ON 0.01 to 0.1 s (AMD-S@1), 0.1 to 1 s (AMD-S@2), 1 to 10 s (AMD-S@3) Output 2 Comparison value 1 Setting range (0.0 s) Set value (99.9 s) Note: The characters displayed in reverse video are the default settings. OMRON ELECTRONICS LLC (U.S.A.) Tel: (1) 847-843-7900/Fax: (1) 847-843-7787 OMRON ASIA PACIFIC PTE. LTD. (...

  • マニュアル

    ... setting errors according to the key-protection levels shown in the following table. ※ Key-protection levels are set in Function Setting mode. OFF ※ All measurement range is possible to Measure- 0.1 to 1s be measured with [10kHz] setting. ment (Model AMD-...

  • マニュアル

    ... setting errors according to the key-protection levels shown in the following table. ※ Key-protection levels are set in Function Setting mode. OFF ※ All measurement range is possible to Measure- 0.1 to 1s be measured with [10kHz] setting. ment (Model AMD-...

  • マニュアル

    ...5・1PTotectivcandDiagnosticFunctions... 5-2Treubleshooting 5・3 ●`●● 5-2-lOControllerReceivesNoisewhcnlnvcrterisStarte〔1.,_...。 .,,、, 5・2-11AMRadioReceivesNoisewhenInvesterisStarted..........,.,, 5-2-12GroundFaultEnterrupterisActuatedwhenInverterisStarted.◆、‥ 5・2・13MechanicalSys(emMakesNoise..、..,,.,...,..,,.......,,,, MaintenanceandInspection......,,............_,.. 5・2-1 5・2・2 5-2-3 5・24 5-2-5 ...

  • マニュアル

    ...↑ UE Section5・7 ●Settingthemotorrevolutionspeedandjogoperation. 6.MechanicalIoadandconnectMty(refertotheappropriateproductoperatienmanual) 7.Autotuning HAILA UT UE Section5・8 eCarryingoutautotuningaccordingtomechanicalrigidity. 8.Testrun(refertoapPropriateproductoperationmanual) 9.Graphdisplay HAILA UT UE Section5・10 ●Checkingrunnhgconditionvebcityandtorqueraph. 10.Run(refertoapPropriateproductoperationmanual) END ...