全 41926 件が検索されました。(1221 - 1240件を表示)

  • マニュアル

    ... with the 3G3MV are performed in byte units. Select 1 Byte and BIN. Select No for reading data because there is no data to be read. Address Set the addresses of the Slaves. Note In this example, the Slave addresses are set in ...

  • マニュアル

    ... with the 3G3JV are performed in byte units. Select 1 Byte and BIN. Select No for reading data because there is no data to be read. Address Set the addresses of the Slaves. Note In this example, the Slave addresses are set in ...

  • マニュアル

    ...D S: Beginning Command Storage Word Specify the beginning word address for the command data transferred to the DeviceNet Master Unit. Preset the data to be transferred in consecutive words as shown in the following table. Bits Word address S S+1 ...

  • マニュアル

    ... after power loss ridethrough. Sets the time to approximately 0.7 times the motor secondary 0.1 to 5.0 circuit time constant. If an overcurrent or undercurrent occurs when starting a speed search or DC injection braking, increase the set values. 0.1 ...

  • マニュアル

    .... Word Bits 15 to 8 S 7 to 0 Command code (Set Explicit Message FINS command 2801.) S+1 Node address of slave or master to which message is to be sent: 0 to 3F Hex (0 to 63) S+2 Class ID code (Sets the DeviceNet class code for the function.) S+3 Instance ID code (Sets the DeviceNet instance code for the function.) S+4 Attribute ID code (Sets the DeviceNet attribute code for the function.) --- Attached data (for write) 6-68 Explicit Message service code Write: 10; Read: 0E Attached data (for write) 6.8 Communications ...

  • マニュアル

    ...C ● S: Beginning Command Storage Word Specify the beginning word address for the command data transferred to the DeviceNet Master Unit. Preset the data to be transferred in consecutive words as shown in the following table. Word address S S+1 ...

  • マニュアル

    ...All communications with the 3G3RV are performed in byte units. Select 1 Byte and BIN. Select No for reading data because there is no data to be read. Address Set the addresses of the Slaves. In this example, the Slave addresses are set in ...

  • マニュアル

    ...S Bit No. 15 to 8 7 to Command code (Set the FINS Explicit Message command (2801).) S+1 Node address of the Slave/Master to which the Explicit Message is sent: 0 to 3F hex (0 to 63) S+2 Class ID code (Set the DeviceNet Class code of the target function.)*1 Explicit Message service codes Write: 10, Read: 0E S+3 Instance ID code (Set the DeviceNet Instance code of the target function.) S+4 Attribute ID code (Set the DeviceNet Attribute code of the target function.) … 0 Attachment data (in case of a write request etc.)...

  • マニュアル

    ...Bit No. 15 to 8 7 to 0 Command code (Set the FINS Explicit Message command (2802).) S+1 Node address of the Slave/Master to which the Explicit Message is sent: 0 to 3F hex (0 to 63) S+2 Explicit Message service codes Write: 10, Read: 0E S+3 Class ID code (Set the CompoNet Class code of the target function.)*1 S+4 Instance ID code (Set the CompoNet Instance ID code of the target function.) S+5 Attribute ID code (Set the CompoNet Attribute ID code of the target function.) … Attachment data (in case of a ...

  • マニュアル

    ...-13 2 Specifications Safety Stop Type Reset Type E-STOP buttons on sides of AMR Emergency Stop • E-STOP button Safety Function on Operator Panel • E-STOP button on Pendant Emergency stop connection(s)*2...

  • マニュアル

    ... Point A Vertical Groove Lube Point B Top View Looking Down Vertical Groove Lube Point C Section A-A Figure 7-6. Lubricating Joint 3 Quill Replacing the Encoder Battery Pack Every 2 to 4 years, or if the robot'...

  • マニュアル

    ...リチウム電池 停電補償用電池コネクタ 各種スイッチ電源LED等電 源 監 視 中 通信 中 エ ラ ー RY 1 RY 2 RS-232C R S -2 3 2 C S D RD 7 8 T ES T R E SE T メ ン テ ナン ス 時 計 O N O N 入 力 入力LED 1 2 3 4 5 AC 10 0 V 6 コネクタ FG ~ AC電源端子 N ...

  • マニュアル

    ... the data that come after the whether remote I/O communication is executed or not.  Only message communication is executed (Remote I/O communication under suspension) Communication cycle time = 2 Note + 0.11 x TB + 0.6 [ms] When TB is 500 k bits/...

  • マニュアル

    .... 五 8 SW28 w置旧EIE旧8i 1 andcorrection・●valueinput. 鍾 8§ AIJTOSW2 S1ト「itchbetweenAUTOandTEST. presentposition indiCatiOnOUtpUt, 1 ◎,` Achangeover Thisconnectoτ ilncludesconnectio!〕 冑iththeHP6, UN4/ 一 SW1,...

  • マニュアル

    .... (physical port) Communications port (internal logical port): 0 to 7 Hex D Send Data Word Allocations (Third Operand of PMCR Instruction) Word No. S+0 Data format No. of send data words (4-digit Hex) S+1 Reserved ...

  • マニュアル

    ... the DM Area. CTBL(882) with High-speed Analog Sampling Function CTBL P M S S P: Port specifier (#0003) M: Register target value comparison table and start comparison. S: Target value comparison table Target value S+1 ...

  • マニュアル

    ... reflected in the Arithmetic Flags. Control the desired output or right-hand instruction with a branch from the same input condition that controls CMP(020), as shown in the following diagram. In this case, the Equals Flag and output A will be turned ON when S1 = ...

  • マニュアル

    ... input method (×1, ×2, or ×4). When the multiplier is disabled, the counter 1 input method (×1, ×2, or ×4) is used. CTBL(882) Settings for the High-speed Analog Sampling Function CTBL P M S S S+1 S+2 S+3 P: Port specifier (#0003) M: Register target value comparison table and start comparison. S: Target value comparison table Target value 8-digit hex First word of data sample storage area 0000 to 7FFF hex (DM Area address) Number of data samples 0001 to 8000 hex 295 Section 7-9 Analog Input Functions Example CTBL #3 #0...

  • マニュアル

    ...430 Output Required 432 Output Required 433 S Signed binary data (16 bits) Converts the specified double-precision floating-point data (64 bits) to 32bit signed binary data and outputs the result to the destination words. S+3 ...

  • マニュアル

    ... the minimum value range (excluding 0) Positive numbers: Fixed to the maximum velocity. Negative numbers: Fixed to the -maximum velocity. Positive numbers: 1 pulse/s Negative numbers: -1 Maximum Acceleration/ Positive numbers: Fixed to Deceleration*4 pulse/...