全 1430 件が検索されました。(1021 - 1040件を表示)
- マニュアル
... reset or output malfunctions may occur. Make sure that the Temperature Controller has 30 minutes or more to warm up after turning ON the power before starting actual control operations to ensure the correct temperature display. When using self-tuning, turn ON power for the load (...
- マニュアル
... to press the ESC Key several times. When ZERO SET is entered, the display will change to a confirmation display. Press the OK Button again to enable changing the setting. Note: The display on the left indicates that the current setting is INVALID, i....
- マニュアル
... scaling setting, and 1 EU becomes the minimum scaling unit. xvii How to Read Display Symbols The following tables show the correspondence between the symbols displayed on the displays and alphabet characters. The default is for 11-segment displays. a b c d ...
- マニュアル
... ........................................ 2-17 Echoback Test..................................................... 2-18 Operation Command ........................................... 2-19 Response Code List ................................................... 2-26 2-1 SECTION 2 CompoWay/F Communications Procedures 2.1 Data Format Hexadecimal values are expressed by adding the prefix H’ before the number, ...
- マニュアル
... of specifications for ambient temperature and humidity. The service life will decrease due to increased internal temperature if multiple Digital Controllers are mounted closely side by side or one on top of the other. If this type of mounting is used, use forced cooling, ...
- マニュアル
... high temperatures, may result in deterioration to internal parts, such as an electrolytic capacitor. 15) Internal circuit voltage (12 V) is output to the no-voltage input terminals, which may cause some connected devices to malfunction or fail. Check the specifications of the input device (...
- マニュアル
... time (min.) Reset time following power application: 0.05 sec 0.02 sec reset signal width (min.) ON residual voltage: 2 V max. * Contact and transistor signal input use common terminal. Connecting Sockets Socket Surface mounting Flush mounting P2CF-08(-...
- マニュアル
...h5cx-a_-n_-l_-n_inst-1148541-8c.pdf (51) Surface Mounting H5CX-A11@-N Y92S-29 (order separately) Waterproof Packing Panel H5CX -A11@-N 100.9 103.2* (51) P2CF-11(-E) Front-connecting sockets (order separately) H5CX-L8@-N 48 1. The thickness of a mounting panel should be 1 to 5 mm. 2. It is possible to mount Timers side by side by mounting Adapters. (But only towards the non-hook side.) 89.9 Y92S-29 (order separately) Waterproof Packing Panel H5CX -L8@-N 57.5 Y92F-30 (order separately) Flush Mounting Adapter P3GA-11 (order separately)...
- マニュアル
...Panel Adapter Panel-cutout Dimensions Diagram (Units: mm) Panel cutouts are as shown below. (according to DIN43700) To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i....
- マニュアル
... output terminals, and between input and output terminals. When double insulation or reinforced insulation is required, apply double insulation or reinforced insulation as defined in IEC 60664 that is suitable for the maximum operating voltage with clearances or solid insulation. Package Contents P2CF-08(-...
- マニュアル
... output terminals, and between input and output terminals. When double insulation or reinforced insulation is required, apply double insulation or reinforced insulation as defined in IEC 60664 that is suitable for the maximum operating voltage with clearances or solid insulation. Package Contents P2CF-08(-...
- マニュアル
...ステム・機械・装置水道、 電気の供給システムや24 時間連続運転システムなど高い信頼性が必 d) ガス、 要な設備 e) その他、上記 a)∼ d)に準ずる、高度な安全性が必要とされる用途 *上記は適合用途の条件の一部です。 当社のベスト、総合カタログ、...
- マニュアル
... fine metallic shavings or filings from installation to enter the product. Doing so many occasionally result in electric shock, fire, or malfunction. ‘n’ counters CP1 CP2 RESET R3 A A=(n–1)X72+70 UP/DOWN SW1: ...
- マニュアル
... shown in the right figure. Sensor n Units mounted side-by-side A 2 3 4 (DO NOT USE) Power supply 5 6 (DO NOT USE) Power supply Power supply SW2: 6 or E Q H7AN-R6D H7AN-R6DM H7AN-RW6D H7AN-RW6DM H7AN-RT6 H7AN-RT6M 8 H7AN-R8D H7AN-R8DM – – – H7AN-RT8M Table 2. SWITCHES SW1 SW2 SW3 SW4 SW2 ○ ○ ○ ○ ○ ○ ○ ○ ○ ○ – – SW3-1 SW3-1 SW3-1 SW3-1 SW3-1 SW3-1 SW3-2 SW3-2 SW3-2 SW3-2 SW3-2 SW3-2 – SW3-3 – SW3-3 – SW3-3 – SW4-1 – SW4-1 SW4-1 SW4-...
- マニュアル
...-1 SW3-1 – SW3-1 – SW3-1 SW3-1 SW3-1 SW3-1 – SW3-2 – SW3-2 SW3-2 SW3-2 – SW3-2 1 0 9999 – SW2: 6 or E 30 Hz C P 1 C P 2 • CP1, CP2 count input Maximum calculation speed 4 56 4 56 8 6 7 9A CP2 Digital display 1 Digital display Digital display CP2 1 1 n–2 㧙 n–1 n–2 Reset 㧙 1 2 n+1 n+2 0 9999 9998 t n–1 n–2 1 n 㧗 㧗 n–1 n 9999 㧗 㧗 n+1...
- マニュアル
...Flush mounting Y92F-30 48 P3G-08 @44.8 Model H7CN Model H7CN + Adapter 106 103.7 48 14.2 7 2 .5 (10.9) 97.6 10.9 P2CF-08(-E) ■ PANEL CUTOUT [mm] Standard panel cutout is as shown in the right figure. (conforms to DIN43700) 95.1 • Model H7CN-@@NM (with memory backup) Surface mounting 60 min. R0.5 max. Flush mounting 45㧗0.6 㧙0 Y92F-30 45㧗0.6 㧙0 Note 1.The thickness of mounting panel should be 1 to 5 mm. Note 2.It is possible to mount the ...
- マニュアル
... temperature of 23°C) External power supply 12 VDC, 100 mA Degree of protection IEC IP66, UL508 Type 4X* Voltage input • Accessories (Order Separately) P2CF-11 Track Mounting/Front Connecting Socket 11-pin 11-pin, finger-safe type P2CF-11-...
- マニュアル
...Y92F-30 (order separately) Flush Mounting Adapter 2. Key Protect Indicator (orange) 3. Control Output Indicator (orange) 4. Comparison Value 1, 2 Stage Indicator 5. Present Value (Main Display) Character height: 10 mm (red) 48 P2CF-11(-...
- マニュアル
... water or oil. • Do not use this equipment in dusty environments or expose it to corrosive gases or direct sunlight. • Wire signal lines and power lines separately to reduce the influence of noise. • Do not install the H7CX close to sources of excessive static electricity (...
- マニュアル
... water or oil. • Do not use this equipment in dusty environments or expose it to corrosive gases or direct sunlight. • Wire signal lines and power lines separately to reduce the influence of noise. • Do not install the H7CX close to sources of excessive static electricity (...