全 1430 件が検索されました。(1041 - 1060件を表示)

  • マニュアル

    ... power supply is not sufficient, the Counter may not start. Be sure to use a power supply with sufficient capacity. 3) Maintain voltage fluctuations in the power supply within the specified operating voltage range. 4) To allow for the startup time of peripheral devices (...

  • マニュアル

    ...るシステム・機械・装置 d) ガス、水道、電気の供給システムや24時間連続運転システムなど高い信頼性が必要な設備 e) その他、上記 a)∼ d)に準ずる、 高度な安全性が必要とされる用途 *上記は適合用途の条件の一部です。 当社のベスト、総合カタ...

  • マニュアル

    ... Motor with incremental encoder: R88M-Ujjj30H-j/V-jS1 S Servo Motor with absolute encoder: R88M-Ujjj30T-j/V-jS1 Items to Check After Unpacking Check the following items after removing the product from the package: S Has the correct product been delivered (i....

  • マニュアル

    ... even with the power turned off.) 5. Specifications and functions may be changed without notice in order to improve product performance. Items to Check when Unpacking Check the following items when removing the product from the package: Has the correct product been delivered (i....

  • マニュアル

    ... product to systems, machines, or equipment that may have a serious influence on human life and property if they are used improperly. Items to Check After Unpacking Check the following items after removing the product from the package: S Has the correct product been delivered (i....

  • マニュアル

    ..., appropriate for the operating conditions. 8. Specifications and functions may be changed without notice in order to improve product performance. Items to Check Before Unpacking Check the following items before removing the product from the package: S Has the correct product been delivered (i....

  • マニュアル

    .... S Servomotors with incremental encoders: R88M-WjH-j/-WjL-j S Servomotors with absolute encoders: R88M-WjT-j/-WjS-j Items to Check After Unpacking Check the following items after removing the product from the package: S Has the correct product been delivered (i....

  • マニュアル

    ...There is warning information on the Inverter in the position shown in the following illustration. Always heed the warnings. Warning information position Warning information position Illustration shows the 3G3RV-B2220 Illustration shows the 3G3RV-A2004 Warning Information For Europe (-...

  • マニュアル

    ... systems, machines, and equipment that may have a serious influence on lives and property if used improperly, consult your OMRON representative. Items to Check Before Unpacking 1. Check the following items before removing the product from the package: • Has the correct product been delivered (i....

  • マニュアル

    ... for the operating conditions. 8.Specifications and functions may be changed without notice in order to improve product performance. Items to Check Before Unpacking Check the following items before removing the product from the package: • • • • Has the correct product been delivered (i....

  • マニュアル

    ..., and follow the relevant specifications. • Servomotors with incremental encoders: R88M-W@H-@ • Servomotors with absolute encoders: R88M-W@T-@ Items to Check After Unpacking 1.Check the following items after removing the product from the package: • Has the correct product been delivered (i....

  • マニュアル

    ... effort has been made to provide detailed specifications, information on functions, and interrelationships between them. Assume that anything not described in this manual cannot be performed. • This manual is intended for the following personnel, who are assumed to have sufficient knowledge of electrical systems (i....

  • マニュアル

    ... effort has been made to provide detailed specifications, information on functions, and interrelationships between them. Assume that anything not described in this manual cannot be performed. • This manual is intended for the following personnel, who are assumed to have sufficient knowledge of electrical systems (i....

  • マニュアル

    ... warning information on the Inverter in the position shown in the following illustration. Always heed the warnings. Warning information position Warning information position Illustration shows the 3G3RV-B2220-V1 Illustration shows the 3G3RV-A2004-V1 Warning Information For Europe (-...

  • マニュアル

    ... turn OFF the power supply before setting the rotary switch. (The switch is factory-set to 0.) Setting 0 1 2 3 4 5 6 7 8 9 A B C D E F 1-4 Command pulse resolution 1000 2500 5000 10000 1000 2500 5000 10000 1000 2500 5000 10000 1000 2500 5000 10000 Command pulse connection method Open collector or line driver Command pulse type CW+CCW, positive logic CW Line driver CCW Open collector or line driver CW+CCW, negative logic CW Line driver CCW Open collector or line driver Sign + pulse string, positive logic PULS...

  • マニュアル

    .... !WARNING Do not touch the inside of the Servo Driver. Doing so may result in electric shock. !WARNING Turn OFF the emergency stop input (STOP) whenever turning OFF the main circuit power supply. Even if the main circuit power supply is turned OFF, ...

  • マニュアル

    ...007 015 022 037 055 075 0.2 kW 0.4 kW 0.75 kW 1.5 kW 2.2 kW 3.7 kW 5.5 kW 7.5 kW Voltage class 2 E 4 3-phase 200 V AC (200-V class) 1/3-phase 200 V AC (200-V class) 3-phase 400 V AC (400-V class) Enclosure rating A Panel-mounting (IP10 min.) or closed wall-mounting models „Checking the Accessories Note that this manual is the only accessory included with the 3G3JX model. Mounting screws and other necessary parts must be provided by the user....

  • マニュアル

    ...007 015 022 037 055 075 0.2 kW 0.4 kW 0.75 kW 1.5 kW 2.2 kW 3.7 kW 5.5 kW 7.5 kW Voltage class 2 E 4 3-phase 200 V AC (200-V class) 1/3-phase 200 V AC (200-V class) 3-phase 400 V AC (400-V class) Enclosure rating A Panel-mounting (IP10 min.) or closed wall-mounting models „Checking the Accessories Note that this manual is the only accessory included with the 3G3MX model. Mounting screws and other necessary parts must be provided by the user....

  • マニュアル

    ... directly without operating software. Built-in Braking Circuit (up to 22 kW) The Inverter models with 22 kW or lower capacity incorporate a braking transistor, enabling spacesaving configuration for applications that need rapid acceleration and stop. Restart Speed Search Function For a free-running motor (...

  • マニュアル

    ...When turning OFF the main circuit power supply, turn OFF the RUN Command Input (RUN) at the same time. Residual voltage may cause the Servomotor to continue rotating and result in injury or equipment damage even if the main circuit power supply is turned OFF externally, ...