全 129 件が検索されました。(81 - 100件を表示)
- マニュアル
... Current of Slave Unit with DC Inputs and Sensor Control Output (Load Current) IOUT (min) ≤ ION ≤ IOUT (max.) IOUT: Sensor control output (load current) ION: ON current of Input Slave Unit with DC inputs ION is calculated as follows: ION = (VCC − VR − ...
- マニュアル
... after temperature and pressure correction > Y1 = X1 Description 1.246X2+0.2524 0.4247X3+0.7735 X1 : Flowrate (Variable area flowmeter) signal The flow rate of the variable area flowmeter is represented by the following formula: Q=A*α [2/p]*[...
- マニュアル
...-2 Relation between ON Current of a Unit with DC Inputs and Sensor Control Output IOUT (min) ≤ ION ≤ IOUT (max) IOUT: Sensor control output (load current) ION: ON current of a Unit with DC inputs ION is calculated as follows: ION = (VCC - VR - ...
- マニュアル
... User's Manual for Visual Feedback Alignment Library (W608) 4-1 4 4 Individual Specifications of FB/FUN Structure The structure of the alignment library is as follows. XYθ Position (sPOSITION) Stores the XYθ coordinates. Variable name Data type OmronLib\...
...EIP002_IOLink_port0_1_IN[32] IO-Link 0 0 0 0 0 0 DC IOL EIP002_IOLink_port0_1_IN[33] port 0 SC 0 0 0 0 PDI DF VF EIP002_IOLink_port0_1_IN[34]~[35] Vendor ID EIP002_IOLink_port0_1_IN[36]~[38] Device ID EIP002_IOLink_port0_1_IN[39]~[41] Event 1 EIP002_IOLink_port0_1_IN[42]~[44] Event 2 EIP002_IOLink_port0_1_IN[45]~[47] Event 3 EIP002_IOLink_port0_1_IN[48]~[79] IO-Link port 1 input data EIP002_IOLink_port0_1_IN[80] 0 0 0 0...
...-Link port 0 近接センサの Process Data を格納 Byte0 (PD0)を格納 Byte1 (PD1)を格納 IO-Link port 0 input process data IOL (Port in IO-Link mode) DC (Device connected) 0 (Reserved) VF (Validation failed) DF (Data storage validation failed) PDI (Process data invalid) 0 (Reserved) SC (IO-Link short circuit) Vendor ID Device ID Event 1 Event 2 Event 3 データ種別「IO-Link port 0」と同様。 IO-Link port 1 0~15 0~15 データ種別「IO-Link port ...
...D10395 0 to 15 D10220 D10221 D10222 D10223 D10224 D10225 D10226 Data allocation IO-Link port 0 IO-Link port 0 input process data IOL (Port in IO-Link mode) DC (Device connected) 0(Reserved) VF (Validation failed) DF (Data storage validation failed) PDI (Process data invalid) 0(Reserved) SC (IO-Link short circuit) Vendor ID Device ID Event 1 Event 2 Event 3 Same functions as for the data allocation "IO-Link port 0" IO-Link port 1 Same functions as for the data allocation "IO-Link port 0" IO-Link port 2 Same functions as for the data...
...IO-Link port 0 input data IO-Link port 0 EIP002_IOLink_port0_1_IN[33] 0 0 0 0 0 0 DC IOL SC 0 0 0 0 PDI DF VF EIP002_IOLink_port0_1_IN[34] to [35] Vendor ID EIP002_IOLink_port0_1_IN[36] to [38] Device ID EIP002_IOLink_port0_1_IN[39] to [41] Event 1 EIP002_IOLink_port0_1_IN[42] to [44] Event 2 EIP002_IOLink_port0_1_IN[45] to [47] Event 3 EIP002_IOLink_port0_1_IN[48] to [79] IO-Link port 1 input data EIP002_IOLink_port0_1_...
- カタログ
...≦4≦5≦6≦7となるようにしてください。 詳細情報は www.fa.omron.co.jp 69 インバータ選定の概要 b105 オプション Vf自由設定 b101 高機能型汎用インバータ 3G3RX パラメータNo. その他 70 機能名称 b046 逆転防止選択 b050 瞬停ノンストップ選択 b051 瞬停ノンス...
- カタログ
...≦4≦5≦6≦7となるようにしてください。 詳細情報は www.fa.omron.co.jp 69 インバータ選定の概要 b105 オプション Vf自由設定 b101 高機能型汎用インバータ 3G3RX パラメータNo. その他 70 機能名称 b046 逆転防止選択 b050 瞬停ノンストップ選択 b051 瞬停ノンス...
- マニュアル
...Constantpower outputarea Frequency SetthethirddigitofNe.46to"1."ThelnverterwiHautomatically Iowertheoperatingleveltoensurestableoperationintheconstant poweroutputarea, 51 ---------------------[End of Page 9968]--------------------- 170% ρρ5cr∫tiOttofl"u'tctionsandCoJistants Section2-8 TheoperationIevelisloweredaccordingtothefo】lowingcalculation. OP1=・OP2xVF/OF OP1;Stallpreventiolloperationlevelduringaccelerationinthe constantpoweroutputarea OP2:Stallpreventionoperationlevelduringacceleration(No・30) ...
- マニュアル
...0.0 to 800.0 0.0 No No V 3 4-23 * 2nd/3rd control is displayed when "SET(08)/SET3(17)" is allocated to one of multi-function inputs from C001 to C008. 3-38 Operation Vf free setting Normal b031 = 10 3-7 Parameter List Parameter No. Function name Monitor or data range Default setting Changes during operation Unit Page Normal b031 = 10 Others Operation 3 b120 Brake control selection 00: Disabled 01: Enabled 00 No Yes ⎯ b121 Brake wait time for release 0.00 to 5.00 0.00 No Yes s b122 Brake wait time ...
- マニュアル
... Automatic torque boost (IM) on AA121(Control mode selection, 1st-motor). Re-confirmation is required for setting. A043 5 Hb142 0 Re-confirmation is required for setting. A044 0: Constant torque characteristics (VC) AA121 0: ...
- マニュアル
...FALSE or TRUE Outputs whether Outputs exists or not when an M code is received. The element numbers (0..7) in the array correspond to the arguments (VA..VH) in the M code. 0=VA, 1=VB, 2=VC, 3=VD, 4=VE, 5=...
- マニュアル
... acceleration/deceleration 2 Programming Example N01 N02 N03 N04 N05 N06 N07 N08 N09 N10 N11 N12 N13 N14 N15 G500, G501 Multi-block Acceleration/Deceleration Programming Example Feedrate VF: Velocity specified by F code ...
- マニュアル
...ォーマット〕〔オフセット〕 VFH〔オフセット〕.ファイル名 説 明 l ベリファイ対象はコマンドにより指定します。 VR VF • :ターミナル接続ポート :PC本体メモリカード フォーマットは、ベリファイ対象がターミナルの場合には、Sフォーマット、 HEXフォ...
- マニュアル
...ユニットが識別できます。 SK20側では、特殊補助リレー{030⑪}で通信異常の有無が判定できます。 圏卜r声一ト1'。 ユニvF例ヤタイプ)ユーザーズマニュアル」{SBcc・413) ●親局側の特殊補助リレー [C120/C500の場合ユ特蛛補助リレーsgCH ビットユ5∼8: 1514131211110-9呂75...
- マニュアル
...170 凡例 Q: 体積流量(Nm3/h) A: すきま断面積 Af:フロート 断面積 α: 流量係数 ρ: 流体密度 ρf:フロート 密度 Vf:フロート 体積 温度圧力補正(面積式流量計) 171 恒温槽の平均温度制御(入出力にバイアスがかかった場合) 恒温槽の平均温度制御(入出力...
- マニュアル
...力(負荷電流) ION : トランジスタ入力タイプのスレーブの ON 電流 ION は、以下のように求めることができます。 ION=(VCC−VR−VF)/RIN VF : トランジスタ入力タイプのスレーブの内部残留電圧 RIN : トランジスタ入力タイプのスレーブの入力インピーダンス...
- マニュアル
...の制御出力(負荷電流) ION : トランジスタ入力ユニットの ON 電流 ION は、以下のように求めることができます。 ION=(VCC−VR−VF)/RIN VF:トランジスタ入力ユニットの内部残留電圧(マルチプル I/O ターミナルでは、1.5V) RIN:トランジスタ入力ユニットの入...