全 1430 件が検索されました。(781 - 800件を表示)
- マニュアル
... in the wavelength range from 400 nm to 700 nm, protection is afforded by aversion responses including the blink reflex. For other wavelengths the hazard to the unaided eye is no greater than for Class 1. Direct intrabeam viewing of Class 3A lasers with optical aides (...
- マニュアル
... of its proper functions and performance. Read this information carefully and follow the cautions. If the product is used incorrectly, data or the equipment itself could be destroyed. Editor’s Note Visual Aids Indicates summaries of points of particular importance relating to product performance, ...
- マニュアル
... explode if mishandled. Do not disassemble the Data Carrier, or subject it to high pressure or high temperatures (of 100 °C or more), or dispose of it by incineration. xiv Operating Environment Precautions 4 !WARNING Provide safety measures in external circuits, i....
- マニュアル
... or surges. When using a noise filter, check the voltage and current and install it as close to the product as possible. (11) For a safety disconnection of the power-line in the application the equipment shall be provided with disconnecting devices suitable for isolation (...
- マニュアル
... to ensure that the product is capable of its proper functions and performance. Read this information carefully and follow the cautions. If the product is used incorrectly, data or the equipment itself could be destroyed. Indicates summaries of points of particular importance relating to product performance, ...
- マニュアル
... sensors or programmable controllers. The power indicator lights when the Sensor is powered ON. The Zero Reset indicator lights when the zero reset function is enabled. The ENABLE indicator lights when the sensor is ready for measurement. It goes off when measurement is not possible (...
- マニュアル
...0 0 0 0 1 1 1 1 8 0 0 0 0 1 0 0 1 0 0003H 0 0 0 0002H 1 3 E 7 • Settings to not write-protect any addresses: Address 0000H 0001H 0002H 0003H Bit 7 6 5 4 3 2 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 The write protection function is a function of the V680-CA5D...
- マニュアル
... for command processing is displayed. The end code is displayed in 2-digit hexadecimal, as shown below. Hexadecimal 0 1 2 3 4 5 6 7 8 9 A B C D E F Display SECTION 1 Part Names and Functions The display is lit for normal and warning responses and flashes for error responses. The error code “15” will be displayed if the operation conditions have not been set and operation is switched to Self-execution Mode. Maintenance Mode (SW5 ON) In Maintenance Mode, the measurement results for each measurement mode is displayed in 2-digit decimal....
- マニュアル
...0 0 0 0 1 1 1 1 8 0 0 0 0 1 0 0 1 0 0003H 0 0 0 0002H 1 3 E 7 • Settings to not write-protect any addresses: Address 0000H 0001H 0002H 0003H Bit 7 6 5 4 3 2 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 The write protection function is a function of the V680-CA5D@@-V@ ...
- マニュアル
...0 8 0 0 0002H 0 8 0 0 0 0 0 1 0003H 1 Section 2 RF Tags 0001H 0 3 1 0 0 1 E 7 • Settings to not write-protect any addresses: Address 0000H 0001H 0002H 0003H Bit 7 6 0 0 5 4 3 2 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 The write protection function is a function of the V680-CA5D-V Controller and the C1W-...
- マニュアル
... FG terminal is grounded. • If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. • Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...
- マニュアル
...Description I/O 1 S Signal line --- 2 GND Analog ground --- Node Address Switches The node address switches set the FL Remote Node Address. This node address is used as the rightmost part of the IP address (...
- マニュアル
... Displays in the Mode Selection Menu When the S8AS is switched to the Mode Selection Menu from Run Mode, the seven-segment display will show “RUN.” r u n 1 2 3 4 5 6 V A Yrs °C s s e t 1 2 3 4 5 6 V A Yrs °C s t s t 1 2 3 4 5 6 V A Yrs °C s If the Key is pressed, SET will be displayed. If the Key is pressed at this point, the S8AS will enter Setting Mode. Refer to 4-4 Switching to Setting Mode ...
- マニュアル
...CS1W-V680C11 CS1W-V680C12 CJ1W-V680C11 CJ1W-V680C12 P ER H ER D2 A HE T/R RR 1 C1 80 V6 RUN C ER 1 AD HE /R T /E RM NO P ER H ER D2 A HE T/R RR 2 C1 80 V6 RUN C ER 1 AD HE /R T /E RM NO R R /ER /ER RM RM NO NO ST ST TE TE ON ON 1 AD AD HE HE 2 AD HE V 24 DC UT P IN + - Man. No.: Z271-E1-07 Introduction Thank you for purchasing an ID Sensor Unit ...
- マニュアル
...-V680C11 CS1W-V680C12 CJ1W-V680C11 CJ1W-V680C12 P ER H ER D2 A HE T/R RR 1 C1 80 V6 RUN C ER 1 AD HE /R T M/E R NO P ER H ER D2 A HE T/R RR 2 C1 80 V6 RUN C ER 1 AD HE /R T /E RM NO R R /ER /ER RM RM NO NO ST ST TE TE ON ON AD 1 AD HE HE 2 AD HE V 24 DC UT P IN + - Man. No.: Z271-E1-08 Introduction Thank you for purchasing an ID Sensor ...
- マニュアル
...25±0.2 M3 pan-head screw Mounting Hole Dimensions Marked side Two, M3 If the RF Tag is mounted to metallic material, use the Section 4 Installing RF Tags separately sold Special Attachment (V600-A86) or a non-metallic spacer (...
- マニュアル
...side Tag is to be used mounted to metallic material, use the Section 4 Installing RF Tags on the back of the V680-D1KP66T RF Tag. If the RF Two, M3 separately sold special attachment (V600-A86) or a non-metallic spacer (...
- マニュアル
... sensor Continuous proportional current output (phase control or optimum cycle control) G3PW Power Controller Heater Just as with a solid state relay (SSR), ON/OFF control can be executed by inputting a time-proportional output or 5 V DC ON/OFF output (i....
- マニュアル
... FG terminal is grounded. - If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. - Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...
- マニュアル
... FG terminal is grounded. • If surge currents are present in the power lines, connect surge absorbers that suit the operating environment. • Before turning ON the power after the product is connected, make sure that the power supply voltage is correct, there are no incorrect connections (...