全 53645 件が検索されました。(6201 - 6220件を表示)
- マニュアル
...circuit D Size Load 4 Blue NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(...
- マニュアル
...Contact: www.ia.omron.com Regional Headquarters OMRON EUROPE B.V. Wegalaan 67-69, 2132 JD Hoofddorp The Netherlands Tel: (31)2356-81-300/Fax: (31)2356-81-388 OMRON ELECTRONICS LLC 2895 Greenspoint Parkway, Suite 200 Hoffman Estates, IL 60169 U....
- マニュアル
...Mode1,Mode3の場合、過接近判定距離と検出物体の材質の組合せで過接近検出することが可能です。 When diagnosis mode is selected mode1 or mode3, it’ s possible by a combination of the excessive proximity judgement distance and the material of the sensing object to check over approach. 诊断模式为Mode1、Mode3时,可结合过接近判断距离和检测物体的材质执行过接...
- マニュアル
... the sensor has passed for 300 msec after turning on, please use in the stable state. (6) The sensor is adjusted with a high degree of accuracy, so do not use in the environment with sudden temperature change. (7) The operation has been confirmed on OMRON'...
- マニュアル
... may cause radio interference, in which case the user may be required to take adequate measures. Suitability for Use Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’ ...
- マニュアル
...于下表所示距离以上范围使用。 E C D B A (水平动作) B A 检出物体 请必须在设定距离内通过。 S :检出距离 Sa :设定距离 Sa=0~0.8S (水平动作的情况,请确认样本上的检出领域图。 ) A E2FX1R5 □□ 20 B 15 型号尺寸 (单位:mm) E2F- E2F- E2F- E2F- E2F- E2FX10 X5M X10M X18M X2 X5 □□ □□ □□ □□ □□ □□ 200 300 30(20) 50(...
- マニュアル
... mm or more. (9)Mutual interference (10)Sensitivity adjustment (8)Influence from surrounding object Suitability for Use Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
... may be required to take adequate measures. (9)Influence by nearby metal PRECAUTIONS FOR SAFE USE Suitability for Use Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
...・センサ部の調整や脱着をおこなう場合は、必ず電源を切ってから作業をしてください。 2 9.5 *形式の末尾に (-S) がつくものは、保護スパイラルチューブ (SUS304,φ7,2m) ・センサヘッドを金属中に埋め込む場合は、 下表のように座ぐりを設けてく...
- マニュアル
... 時に点灯します。 *1 19.2 © OMRON Corporation 2017 All Rights Reserved. 26 光通信部 39.3 感度設定しきい値の微調整 【UP/DOWN】ボタン 【S.TUNE】ボタンチューニングを実行します。 緑デジタルのしきい値が変わります。 DINレール(PFP-□N)別売り < 通信コネクタタイプ > ( ) 内の寸法は関連部...
- マニュアル
... the power indicator and detecting indicator in a desired direction. (front sensing only) ■Terminal Arrangements Suitability for Use Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...
- マニュアル
....com Regional Headquarters OMRON EUROPE B.V. Sensor Business Unit Carl-Benz-Str. 4, D-71154 Nufringen, Germany Tel: (49) 7032-811-0/Fax: (49) 7032-811-199 OMRON ELECTRONICS LLC 2895 Greenspoint Parkway, Suite 200 Hoffman Estates, IL 60169 U....
- マニュアル
....com Regional Headquarters OMRON EUROPE B.V. Sensor Business Unit Carl-Benz-Str. 4, D-71154 Nufringen, Germany Tel: (49) 7032-811-0/Fax: (49) 7032-811-199 OMRON ELECTRONICS LLC 2895 Greenspoint Parkway, Suite 200 Hoffman Estates, IL 60169 U....
- マニュアル
...wires or power lines may result in incorrect operation and damage due to induction. Wire the Sensor using a separate conduit or independent conduit. (4) The following conditions shall be observed if you use the product under an environment using cutting oil that may affect product’...
- マニュアル
...装着してください。 真空側 2-4 大気側ファイバのフランジへの締め付けも真空と アンプ 形E3X-NM11 形E3X-DA□-N/-S 1.フランジの大気側ロックボタンがロック解除状態で コ−ル等で洗浄してお使いください。 あることを確認してください。 2.有...
- マニュアル
...取引先、 または貴社担当オムロン営業員にご相談ください。 34±0.4 A q 2009年10月 74.5±0.4 ■SPPECIFICATION Detection model Retroreflective model (M.S.R function is provided) Model Model E32-R16 ltem E32-R16 Detecting distance OPTICAL FIBER MODEL PHOTOELECTRIC SWITCH Amplifer unit E39-R1 E3X-A□ E3X-F□ E3X-NH□ E3X-NT□ 0.15 to 1.5m 50 to 700mm E3X-DA□ E3X-NM□ 0.15 to 1.5m Operating temperature −25 to 55℃ Storage temperature −40 ...
- マニュアル
.... Make 1 set of fiber interrupted, then turn the sensitivity adjustor slowly clockwise until find point B 1 Where the light becomes incident. Find point B 2, B 3, B 4 in the same way. ● Fiber unit ・Set the light source and receiver'...
- マニュアル
...-precision Contact Type) Operation Manual Smart Sensors High-precision Contact Type ZX-T Series This manual not printed Operation Manual Cat. No. E346-E1-06 Terms and Conditions Agreement Warranty, Limitations of Liability Warranties Exclusive Warranty Omron’...
- マニュアル
... the type of the sensor and mounting bracket. Suitability for Use NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(...
- マニュアル
...E3AS-HF for 2 hours each in X, Y and Z directions Air injection Air discharge Suitability for Use OMRON Corporation shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...