全 53645 件が検索されました。(6281 - 6300件を表示)

  • マニュアル

    ...なります。 ) 2. 位置決めしたい場所に検出体を置いて ボタンを3秒以上長押しします。 (緑デジタルは[ 2pnt ]→[ p%s ]となります。 ) 受光量設定 :2のときの受光量をパワーチューニングレベルの半分に調整します。 しきい値設定:2のときの受光量と...

  • マニュアル

    ... oli for cleaning. · Please dispose the product with on the case in accordance with relevant regulations (laws and regulations) · The mutual interference prevention function does not work when in combination with series other than E3X-ZV/E3X-MZV series. · The Communication Unit E3X-DRT21-...

  • マニュアル

    ... oli for cleaning. · Please dispose the product with on the case in accordance with relevant regulations (laws and regulations) · The mutual interference prevention function does not work when in combination with series other than E3X-ZV/E3X-MZV series. · The Communication Unit E3X-DRT21-...

  • マニュアル

    ...)表示になる 2. 位置決めしたい場所に検出体を置いて ボタンを3秒以上長押しします。 (緑デジタルは[ 2pnt ]→[ p%s ]となります。 ) hs 100 (受光量例) HS 高速モード stnd 100 g ga 800 DPC機能を使うことにより、受光量表示が安定します。 *3 スマートチューニ...

  • マニュアル

    ...ムmaxがIO-Link設定値1023となります。 設定値とモニタ出力の関係性は、 「6.モニタ出力-距離特性」をご確認ください。 Sensor's sensitivity can be changed in a range of 0-1023. The minimum and maximum values of the potentiometer correspond to IO-Link settings of 0 and 1023, respectively. For the relation between the setting and monitor output, refer to section 6 "Monitor output - Sensing Distance." *6 筐体の感度ボ...

  • マニュアル

    ...Green Orange the IO-Link communications. blinking at approx. 0.3s intervals Execute the system command to "Restore the factory settings" to initialize the settings. Refer to index 2 of servie data. ■Sensitivity adjustment Suitability for Use Sensor'...

  • マニュアル

    ...用。 (9)废弃时,请作为工业废弃物处理。 18 15.5 型 ③延长导线必须使用截面积0.3mm2以上、长度100m以下导线。 将韩国S-mark认证机种作为认证品使用时请不要超过10m。 ④对导线部施加的力小于以下值。 拉伸80N以下、扭矩0.1N·m以下、按压20N以下、弯曲3kg以下 ⑤安...

  • マニュアル

    ...お使いください。 (5)電源リセット時間について電 源を入れてから光 電スイッチが検 出 可 能になる時 間は1 0 0 m sですので、電 源 投 入 後 1 0 0 m s 以 降にてご使 用ください 。 負 荷と光 電スイッチが別 電 源に接 続されている場 合は必...

  • マニュアル

    ...:4.7KΩ 60V:100KΩ Suitability for Use MOUNTING TYPE① 20 52 62 15 *8.5 Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’...

  • マニュアル

    ... arrangement THE PRODUCTS CONTAINED IN THIS SHEET ARE NOT SAFETY RATED. THEY ARE NOT DESIGNED OR RATED FOR ENSURING SAFETY OF PERSONS, AND SHOULD NOT BE RELIED UPON AS A SAFETY COMPONENT OR PROTECTIVE DEVICE FOR SUCH PURPOSES. Please refer to separate catalogs for OMRON'...

  • マニュアル

    ...ムmaxがIO-Link設定値1023となります。 設定値とモニタ出力の関係性は、 「6.モニタ出力-距離特性」をご確認ください。 Sensor's sensitivity can be changed in a range of 0-1023. The minimum and maximum values of the potentiometer correspond to IO-Link settings of 0 and 1023, respectively. For the relation between the setting and monitor output, refer to section 6 "Monitor output - Sensing Distance." *6 筐体の感度ボ...

  • マニュアル

    ...Not Present ON 1 OFF 0 ON 1 OFF 0 Inconsistency has occurred on the settings (service data) written in by Green Orange the IO-Link communications. blinking at approx. 0.3s intervals Sensor's sensitivity can be adjusted using the potentiometer or using the IO-Link communications. The value which is set newer either using the potentiometer or sensitivity The sensitivity levels adjusted through IO-Link communications do not correspond to the levels the potentiometer indicates. Setup range T Contact: www.ia.omron.com max Single rotation to 270° T T NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING...

  • マニュアル

    ...100mA max. Black Load 3 Blue 0V NEVER USE THE PRODUCT FOR AN APPLICATION INVOLVING SERIOUS RISK TO LIFE OR PROPERTY WITHOUT ENSURING THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(...

  • マニュアル

    ... FDA, and it has already been registered with the CDRH (Center for Devices and Radiological Health). Ask your OMRON representative for details. Laser Labels Technical standards have been provided with the product. When using a device equipped with the product in the U....

  • マニュアル

    ... FDA, and it has already been registered with the CDRH (Center for Devices and Radiological Health). Ask your OMRON representative for details. Laser Labels Technical standards have been provided with the product. When using a device equipped with the product in the U....

  • マニュアル

    ... the safety precautions below for added safety. (1)Do not use the sensor under the environment with explosive or ignition gas. (2)Never disassemble, repair nor tamper with the product. (3)The maximum power supply voltage is 26.4 VDC. Before turning on the product'...

  • マニュアル

    ...Type E39-L104 EUROPE OMRON EUROPE B.V. Sensor Business Unit Carl-Benz Str.4, D-71154 Nufringen Germany Phone:49-7032-811-0 Fax: 49-7032-811-199 NORTH AMERICA OMRON ELECTRONICS LLC One Commerce Drive Schaumburg,IL 60173-5302 U....

  • マニュアル

    ...ールドコードの使用を原則としてください。 コードの延長は0.3mm2以上の線を用い、 100m以下としてください。 韓国S-ma r k認定機種を認定品として使用される場合は10m未満としてください。 コード部に加わる力は下記の値以下としてく...

  • マニュアル

    ...,请作参考 2种5 2种11 W1种1 W1种2 W2种1 Velo成ite 击o.3 D后phne成财t 问一-3绝D 动粘度 (mm2络s取后t4绝℃ 2.绝2 1绝以 5绝以 分财shiron Oil 击o.2后成分财shiroken EC5绝送-3 分shiron L财bi成HWC6该致riton 17绝绝D 分财shiroken 一5绝击 国H 10以 7~详.5...

  • マニュアル

    ...シローケンEC50T-3 W1種1号ユシロンルビックHWC68 W1種2号 グライトン1700D W2種1号 ユシローケンS50N 働粘度 (mm2/s) at40℃ 2.02 10以上50未満 負荷 0V E3Z-□□□Kご使用上の注意点 7∼9.5 7∼9.9 7∼9.2 7∼9.8 注1.上表の油にて、240H滴下試験し、絶縁抵抗100MΩ以...