全 53645 件が検索されました。(6301 - 6320件を表示)

  • マニュアル

    ... follow the safety precautions below for added safety. (1)Do not use the sensor under the environment with explosive or ignition gas. (2)Never disassemble, repair nor tamper with the product. (3)The maximum power supply voltage is 26.4 VDC. Before turning on the product'...

  • マニュアル

    ...シールドコードの使用を原則としてください。 コードの延長は0.3mm2以上の線を用い、100m以下としてください。 韓国S-mark認定機種を認定品として使用される場合は10m未満としてください。 コード部に加わる力は下記の値以下としてくだ...

  • マニュアル

    ... a light source of Separate type, BGS reflective type, and fixed type does not have it. Suitability for Use Omron Companies shall not be responsible for conformity with any standards, codes or regulations which apply to the combination of the Product in the Buyer’ ...

  • マニュアル

    ... fourni avec une fonction de protection contre les courts-circuits de charge. Cependant, ne jamais court-circuiter la charge. Ne pas utiliser un courant qui dépasse les valeurs nominales dans la sortie de contrôle. La sortie de contrôle est coupée lorsque cette fonction ...

  • マニュアル

    ... a clamp face. ⑦Plug in or out the connector after surly turning off a power supply. Cleaning Do not use thinner such as alcohol and benzine because it may melt a surface of a product. Do not apply high-pressure washing water directly to the sensor'...

  • マニュアル

    ...THE PRODUCTS CONTAINED IN THIS SHEET ARE NOT SAFETY RATED. THEY ARE NOT DESIGNED OR RATED FOR ENSURING SAFETY OF PERSONS, AND SHOULD NOT BE RELIED UPON AS A SAFETY COMPONENT OR PROTECTIVE DEVICE FOR SUCH PURPOSES. Please refer to separate catalogs for OMRON'...

  • マニュアル

    ...。 2-M3 乙烯圆形绝缘导线φ4,投光器:3芯,受光器:4芯 φ (导体截面积:0.2mm /绝缘体径 1.1mm) 标准长度2m ・将 E 3 Z S 连 接 在 F 3 S X 上 使 用 时 , 满 足 安 全 种 类 2 (EN954-1)的必要条件。 ・E3ZS不连接在F3SX上使用时,是安全种类1(EN954-1)。 ・关 于 F 3 ...

  • マニュアル

    ...shown in the table below No-load voltage (V peak) Maximum current rating (A) 0 to 20 5.0 More than 20, up to 30 100 Peak voltage value The E3ZS does not offer protection to the operator’s body from projectiles existing the hazardous area. Proper means of mechanical guarding must be provided to ensure protection from these potentially hazardous projectiles. Wiring must be done while the power is turned OFF. Doing it with the power ON may cause an electric shock. Do not connect the E3ZS to an AC or DC power supply with higher voltage than nominal ...

  • マニュアル

    ... having equivalent knowledge) and also being qualified for one of the following: • Introducing FA equipment • Designing FA systems • Managing FA sites E3NW-ECT EtherCAT Digital Sensor Communication Unit Operation Manual (E429) 1 How to Read the Manual Page Structure This manual'...

  • マニュアル

    ...設定となっています。 CX-Thermoなどの設定ツールの通信条件を以下のように設定してください。 設定値 01 38.4(kbit/s) 7(bit) 2(bit) 偶数 1. パソコンとUSB-赤外線変換ケーブルの接続 パソコンのUSBポートにUSB-赤外線変換ケーブルを接続します。 2. ド...

  • マニュアル

    .... Doing so will cause malfunction or failure. 4) Allow as much space as possible between the controller and devices that generate a powerful high-frequency or surge. 5) Use this product within the rated load and power supply. 6) Make sure that the device'...

  • マニュアル

    .... Doing so will cause malfunction or failure. 4) Allow as much space as possible between the controller and devices that generate a powerful high-frequency or surge. 5) Use this product within the rated load and power supply. 6) Make sure that the device'...

  • マニュアル

    ...communications. Doing so will cause malfunction or failure. 4) Allow as much space as possible between the controller and devices that generate a powerful high-frequency or surge. 5) Use this product within the rated load and power supply. 6) Make sure that the device'...

  • マニュアル

    ...communications. Doing so will cause malfunction or failure. 4) Allow as much space as possible between the controller and devices that generate a powerful high-frequency or surge. 5) Use this product within the rated load and power supply. 6) Make sure that the device'...

  • マニュアル

    ... manual de instrucciones vinculado. • 请参阅链接的使用说明书。 • 링크된 취급 설명서참조하십시오. © OMRON Corporation 2025 All Rights Reserved. Refer to the E5D-H Digital Controllers User’s Manual (Cat. No. H239) for detailed application procedures. ● Key to Warning Symbols CAUTION Indicates a potentially hazardous situation which, if not avoided, is likely to result in minor or moderate injury or property damage. Read this manual carefully before using the product. ● Warning Symbols CAUTION Minor injury due to electric shock may occasionally ...

  • マニュアル

    ... outputs, resulting in property damage. To maintain safety in the event of malfunction of the Digital Controller, take appropriate safety measures, such as installing a monitoring device on a separate line. OMRON Corporation ©All Rights Reserved Refer to the E5@C-T Digital Controllers User’...

  • マニュアル

    ...4 5 6 铂电阻温度计 Pt100 JPt100 热电偶 K J 温度输入 E L U 模拟量输入类型 T N R S B W PL II 10~70°C 60~120°C 115~165°C 140~260°C 4~20 mA 0~20 mA 1~5 V 0~5 V 0~10 V 红外温度传感器 ES1B 电流输入电压输入 运行停止。 设定范围 设定 0 1 2 3 4 5 6 7 8...

  • マニュアル

    ... outputs, resulting in property damage. To maintain safety in the event of malfunction of the Digital Controller, take appropriate safety measures, such as installing a monitoring device on a separate line. OMRON Corporation ©All Rights Reserved Refer to the E5 @C-T Digital Controllers User’...

  • マニュアル

    ...alarm outputs, resulting in property damage. To maintain safety in the event of malfunction of the Digital Controller, take appropriate safety measures, such as installing a monitoring device on a separate line. OMRON Corporation ©All Rights Reserved Refer to the E5□C Digital Controllers User’...

  • マニュアル

    ...作菜单铂电阻温度计 输入 Pt100 JPt100 热电偶 K J 温度输入 E L U 模拟量输入类型 T N R S B W PL II 10~70°C 60~120°C 115~165°C 140~260°C 4~20 mA 0~20 mA 1~5 V 0~5 V 0~10 V 红外温度传感器 ES1B 电流输入电压输入 °F -300~1500 -199.9~900.0 0.0~210.0 -199.9~900.0 0.0~...