全 2268 件が検索されました。(561 - 580件を表示)

  • マニュアル

    ...Model 020), 2-Position ON/OFF (Block Model 001), 3-Position ON/OFF (Block Model 002), Indication and Setting (Block Model 031), Indication and Operation (Block Model 032), Ratio Setting (Block Model 033), Indicator (Block Model 034), and 4-Point Warning Indicator (Block Model 110). ...

  • マニュアル

    ...% 0% 0% Low temperature SV High temperature Forward operation SV Low temperature High temperature Reverse operation For example, when heating control is being performed and the present temperature (PV) is lower than the target temperature (...

  • マニュアル

    ... read and write CPU Unit I/O memory. Connect ES100X Controllers Externally (CS1W-LCB01/05 Only) ES100X Controllers can be connected to the RS-232C port on the Loop Controller and ES100X External Controller Terminal function blocks can be used to monitor ES100X parameters, such as the ...

  • マニュアル

    ...2, etc.) • Data collection cycle: 1 s • Log count: 533 records • Log period: Logging is performed while data log object is displayed only. (It is cleared when screens are switched.) • Log address: (Refer to information on individual function blocks for details on logging the ...

  • マニュアル

    ... Ethernet. The CX-Process Monitor Plus is used together with the CX-Process Tool to create function blocks for Loop Control Units/Boards. You can also perform the following four functions. Monitoring Function Blocks in a Loop Control Unit/Board Monitor PV, ...

  • マニュアル

    ...” 7,”DVMODEL” Data type Note The parameter contents for device types are classified as follows: “PC” or “PLC”: Programmable Controller “NC” or “CNC”: Computerized numeric controllers “RC” or “ROBOT”: Robot controllers “COMPUTER”: Personal computers, panel computers, workstations, display devices, and other computers. “...

  • マニュアル

    ...Write Set Point Starts control for the specified loop. Stops control for the specified loop. Executes autotuning for the specified loop. Cancels autotuning for the specified loop. Reads the status of the specified loop. Reads a process value (PV). Reads the set point (...

  • マニュアル

    ..., LINT, UINT, UDINT, or ULINT), or equations that return integer values can be specified in the initial_value, final_value_equation, and increment_equation. Example 1: The iteration is performed when the iteration variable n = 0 to 50 in increments of 5, and the array variable ...

  • マニュアル

    ... outputs, 4 inputs, 4 outputs, 1 input/ 1 output, or 2 inputs/2 outputs. These enable bit-level distribution of Slave Units. At the same time, unused Slave Unit I/O can be suppressed. IP54 Dust-tight, Splashproof Units (Bit Slaves) The CRT1B-@D@@...

  • マニュアル

    ..., the Set Point and PID constant values must be set, and PV monitored using HMI software or a PT (Programmable Termnal). Loop Controller Personal computer CX-Process Tool: Create function block data. Analog Output Unit CPU Unit HMI software: For example, set ...

  • マニュアル

    ...The ASCII text is stored in D and subsequent words in the following order: leftmost byte of D, rightmost byte of D, leftmost byte of D+1, rightmost byte of D+1, etc. Decimal notation (C=0 hex) -1.23456 Conversion to ASCII text (...

  • マニュアル

    ...0% 0% Low temperature SV High temperature Forward operation SV Low temperature High temperature Reverse operation For example, when heating control is being performed and the process value (PV) is lower than the set point (...

  • マニュアル

    ... for normal read ON for no-read OFF Polygon mode (ASCII 1 character) 41 ('A'): 42 ('B'): Normal (continuous rotating) In-zone startup +6 JAN NW7 NORMAL NW7 SMALL NW7 HEX CODE39 NORMAL CODE39 ST/SP OUTPUT 2 of 5 (ITF) CODE128 CODE93 2 of 5 (3BAR) 2 of 5 (5BAR) No-check Modulus 10 (all bar codes) Modulus 11 (except JAN) Modulus 16 (NW7 only) Modulus 43 (CODE39 only) Modulus 47 (CODE93 only) Modulus 103 (CODE128 only) Note Selecting the values marked with asterisks is required for this protocol. Receive Data Word Allocation (4th Operand of PMCR(260))...

  • マニュアル

    ... := LREAL#100.0; Vel_Acc := LREAL#0.0; Vel_Dec := LREAL#0.0; Vel_Dir := _eMC_DIRECTION#_mcPositiveDirection; // The input parameters for the MC_CamIn (Start Cam Operation) instruction are se t. Camin_Em := TRUE; Camin_Sm := _eMC_START_MODE#_mcRelativePosition; Camin_...

  • マニュアル

    ... is followed. Sysmac Library User’s Manual for Temperature Control Library (W551) 35 DirectPowerControl Function The DirectPowerControl function block is used with the PIDAT or PIDAT_HeatCool instruction to greatly improve the following performance by directly controlling the MV (manipulated variable) to follow the ...

  • マニュアル

    ... := LREAL#100.0; Vel_Acc := LREAL#0.0; Vel_Dec := LREAL#0.0; Vel_Dir := _eMC_DIRECTION#_mcPositiveDirection; // The input parameters for the MC_CamIn (Start Cam Operation) instruction are se t. Camin_Em := TRUE; Camin_Sm := _eMC_START_MODE#_mcRelativePosition; Camin_...

  • マニュアル

    ... programming execution flag input from touch panel PTIn_M anCtl BOOL FALSE --- TRUE Input Manual/auto control flag input from touch panel --- --- TRUE Input Set point input from touch panel PTIn_SP REAL BOOL FALSE --- TRUE Input Autotuning execution flag input from touch panel PTIn_InitParam _sINIT_SE T_PARAMS (SampTime :=T#100ms,R ngLowLmt := 0.0, RngUpLmt := 100.0, DirOpr := FALSE) --- TRUE Input Initial setting parameter input from touch panel PTIn_InitSetOpr_Sa mpTime LINT 100 --- TRUE Input PID sampling period input from touch panel (unit: ms) (MVLowLmt := 0, MVUpLmt := 100, ManResetVal := 0.0, MVTrackSw := FALSE, MVTrackVal := 0....

  • マニュアル

    ................................... 22 Servo Press Library ............................................................................................... 25 What Is the Servo Press Library? .............................................................................................................. 26 Servo Press Library Functionality .............................................................................................................. 27 Common Specifications of Function Blocks ....................................................... 33 Common Variables .................................................................................................................................... 34 Precautions................................................................................................................................................ 40 Individual Specifications of Function Blocks ...................................................... 41 ...

  • マニュアル

    ... to control the stage axis. Also, output of path time (only when fifth order trajectory is enabled), In-Position Judgment of measurement position and reference position is performed. Axis travel distance Stage position Axis velocity calculation Generate PV PV (Current value) ...

  • マニュアル

    ...) 30000 (7530 hex) Y axis (CW) Pulse output 1 5000 (1388 hex) Origin 2. Move to position A. Speed 50 KHz 3. Move to other positions. A 5000 (1388 hex) 8 eed Sp B D 25000 (61A8 hex) Speed 80 KHz C 1. Origin search Hz 0K Speed 80 KHz 35000 (88B8 hex) X axis (CW) Pulse output 0 CP2E CPU Unit Software User’s Manual(W614) 12-53 12 Pulse Outputs z Operation 1 An origin search of X axis (pulse output 0) and Y axis (pulse output 1) is performed using the Origin Search Start Switch (CIO ...